Part Number: AM5728
Other Parts Discussed in Thread: DRA752, TMP102
Hi,
i have this kernel up and running, except for mmc1, connected to a microsd slot.
At mmc2 there is emmc and it works perfectly.
As from dra7-l4.dtsi, the driver used actually seems to be sdhci-omap.c and not hsmmc.
Attaching dts and boot log. Card seems detected, but there is no partition table processed.
Also, removing and reinserting, seems no detection happen.
I checked power supply (3,3), CD pin active low, all seems correct.
&mmc1 { /* 0x4809c000 */
pinctrl-names = "default", "hs";
pinctrl-0 = <&mmc1_pins_default>;
pinctrl-1 = <&mmc1_pins_hs>;
vmmc-supply = <&vdd_3v3>;
vqmmc-supply = <&ldo1_reg>;
bus-width = <4>;
cd-gpios = <&gpio6 27 GPIO_ACTIVE_LOW>;
max-frequency = <96000000>;
status = "okay";
};
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.10.65-00008-g98d45358edb2-dirty (angelo@dfj) (arm-linux-gnueabihf-gcc (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36)) 8.3.0, GNU ld (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36)) 2.32.0.20190321) #170 SMP PREEMPT Mon Feb 28 21:30:32 CET 2022
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM5728
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x95800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x99000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x9f000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0xfe400000
[ 0.000000] OMAP4: Map 0xafe00000 to (ptrval) for dram barrier
[ 0.000000] Zone ranges:
[ 0.000000] Normal [mem 0x0000000080000000-0x00000000afdfffff]
[ 0.000000] HighMem [mem 0x00000000afe00000-0x00000000ffffefff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000afdfffff]
[ 0.000000] node 0: [mem 0x00000000b0000000-0x00000000ffffefff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffefff]
[ 0.000000] DRA752 ES2.0
[ 0.000000] percpu: Embedded 16 pages/cpu s33688 r8192 d23656 u65536
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 522051
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk1p4 rw rootwait earlyprintk nologlevel rw
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1872200K/2095100K available (9099K kernel code, 719K rwdata, 1968K rodata, 1024K init, 230K bss, 34484K reserved, 188416K cma-reserved, 1286140K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] random: get_random_bytes called from 0xc0d00b6c with crng_init=0
[ 0.000000] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000000] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.001434] TI gptimer clockevent: always-on 32786 Hz at /ocp/interconnect@4ae00000/segment@10000/target-module@8000
[ 0.002014] TI gptimer percpu-dmtimer: 20000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@34000
[ 0.002197] TI gptimer percpu-dmtimer: 20000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@36000
[ 0.004089] Console: colour dummy device 80x30
[ 0.004119] Calibrating delay loop... 2052.09 BogoMIPS (lpj=1026048)
[ 0.011138] pid_max: default: 32768 minimum: 301
[ 0.011230] LSM: Security Framework initializing
[ 0.011291] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.011291] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.011962] CPU: Testing write buffer coherency: ok
[ 0.011993] CPU0: Spectre v2: using ICIALLU workaround
[ 0.012207] /cpus/cpu@0 missing clock-frequency property
[ 0.012237] /cpus/cpu@1 missing clock-frequency property
[ 0.012268] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.012847] Setting up static identity map for 0x80100000 - 0x80100078
[ 0.012969] rcu: Hierarchical SRCU implementation.
[ 0.013641] EFI services will not be available.
[ 0.014251] smp: Bringing up secondary CPUs ...
[ 0.021423] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.021423] CPU1: Spectre v2: using ICIALLU workaround
[ 0.021575] smp: Brought up 1 node, 2 CPUs
[ 0.021575] SMP: Total of 2 processors activated (4124.67 BogoMIPS).
[ 0.021575] CPU: All CPU(s) started in SVC mode.
[ 0.022064] devtmpfs: initialized
[ 0.046630] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.046813] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275000 ns
[ 0.046844] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.050170] pinctrl core: initialized pinctrl subsystem
[ 0.050811] DMI not present or invalid.
[ 0.051116] NET: Registered protocol family 16
[ 0.052368] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.055267] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.075683] thermal_sys: Registered thermal governor 'step_wise'
[ 0.076629] cpuidle: using governor menu
[ 0.269409] random: fast init done
[ 3.066619] platform 48970000.vip: Cannot lookup hwmod 'vip1'
[ 3.478790] iommu: Default domain type: Translated
[ 3.482788] mc: Linux media interface: v0.10
[ 3.482849] videodev: Linux video capture interface: v2.00
[ 3.482940] pps_core: LinuxPPS API ver. 1 registered
[ 3.482940] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 3.482971] PTP clock support registered
[ 3.483001] EDAC MC: Ver: 3.0.0
[ 3.483734] Advanced Linux Sound Architecture Driver Initialized.
[ 3.484161] Bluetooth: Core ver 2.22
[ 3.484222] NET: Registered protocol family 31
[ 3.484222] Bluetooth: HCI device and connection manager initialized
[ 3.484252] Bluetooth: HCI socket layer initialized
[ 3.484283] Bluetooth: L2CAP socket layer initialized
[ 3.484283] Bluetooth: SCO socket layer initialized
[ 3.484802] clocksource: Switched to clocksource 32k_counter
[ 3.493896] NET: Registered protocol family 2
[ 3.494049] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 3.495086] tcp_listen_portaddr_hash hash table entries: 512 (order: 1, 12288 bytes, linear)
[ 3.495178] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 3.495269] TCP bind hash table entries: 8192 (order: 5, 163840 bytes, linear)
[ 3.495422] TCP: Hash tables configured (established 8192 bind 8192)
[ 3.495513] UDP hash table entries: 512 (order: 2, 24576 bytes, linear)
[ 3.495574] UDP-Lite hash table entries: 512 (order: 2, 24576 bytes, linear)
[ 3.495697] NET: Registered protocol family 1
[ 3.496215] RPC: Registered named UNIX socket transport module.
[ 3.496246] RPC: Registered udp transport module.
[ 3.496246] RPC: Registered tcp transport module.
[ 3.496246] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 3.496276] PCI: CLS 0 bytes, default 64
[ 3.497406] Initialise system trusted keyrings
[ 3.497558] workingset: timestamp_bits=14 max_order=19 bucket_order=5
[ 3.501739] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 3.502349] NFS: Registering the id_resolver key type
[ 3.502410] Key type id_resolver registered
[ 3.502410] Key type id_legacy registered
[ 3.502441] ntfs: driver 2.1.32 [Flags: R/O].
[ 3.502960] jitterentropy: Initialization failed with host not compliant with requirements: 2
[ 3.502990] Key type asymmetric registered
[ 3.502990] Asymmetric key parser 'x509' registered
[ 3.503051] bounce: pool size: 64 pages
[ 3.503082] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 3.503112] io scheduler mq-deadline registered
[ 3.503112] io scheduler kyber registered
[ 4.193054] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 4.594696] OMAP GPIO hardware version 0.1
[ 4.823730] palmas 0-0058: Irq flag is 0x00000008
[ 4.839355] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[ 4.852416] smps12: supplied by regulator-dummy
[ 4.854522] smps3: supplied by regulator-dummy
[ 4.856597] smps45: supplied by regulator-dummy
[ 4.858856] smps6: supplied by regulator-dummy
[ 4.861145] SMPS7: supplied by regulator-dummy
[ 4.862213] smps8: supplied by regulator-dummy
[ 4.864074] smps9: Bringing 0uV into 1100000-1100000uV
[ 4.864959] smps9: supplied by regulator-dummy
[ 4.866210] ldo1: supplied by regulator-dummy
[ 4.868469] ldo2: supplied by regulator-dummy
[ 4.870513] ldo3: supplied by regulator-dummy
[ 4.872589] ldo4: supplied by regulator-dummy
[ 4.875183] LDO5: supplied by regulator-dummy
[ 4.875946] LDO6: supplied by regulator-dummy
[ 4.876708] LDO7: supplied by regulator-dummy
[ 4.877502] LDO8: supplied by regulator-dummy
[ 4.877960] ldo9: supplied by regulator-dummy
[ 4.880249] ldoln: supplied by regulator-dummy
[ 4.882293] ldousb: supplied by regulator-dummy
[ 4.886138] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 4.929199] edma 43300000.dma: memcpy is disabled
[ 4.932891] edma 43300000.dma: TI EDMA DMA engine driver
[ 4.944671] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 4.950439] pwm-backlight backlight: supply power not found, using dummy regulator
[ 4.956665] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 4.959411] printk: console [ttyS2] disabled
[ 4.959564] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 110, base_baud = 3000000) is a 8250
[ 5.873168] printk: console [ttyS2] enabled
[ 5.880828] omap_rng 48090000.rng: Random Number Generator ver. 20
[ 5.887207] random: crng init done
[ 5.900512] panel-simple display: supply power not found, using dummy regulator
[ 5.912261] display-connector connector@0: HDMI connector with no type
[ 5.918853] display-connector: probe of connector@0 failed with error -22
[ 5.933288] loop: module loaded
[ 5.938812] libphy: Fixed MDIO Bus: probed
[ 5.943756] tun: Universal TUN/TAP device driver, 1.6
[ 5.949005] CAN device driver interface
[ 5.954162] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=4493e337, irq=109)
[ 5.964050] c_can_platform 48480000.can: c_can_platform device registered (regs=7934cefc, irq=137)
[ 5.974822] PPP generic driver version 2.4.2
[ 5.979278] PPP BSD Compression module registered
[ 5.984008] PPP Deflate Compression module registered
[ 5.989135] PPP MPPE Compression module registered
[ 5.993957] NET: Registered protocol family 24
[ 5.998718] mousedev: PS/2 mouse device common for all mice
[ 6.004547] -->tsc2013_init
[ 6.007385] tsc2013_init-->i2c_add_driver
[ 6.013153] bq32k 0-0068: registered as rtc0
[ 6.017822] bq32k 0-0068: setting system clock to 2022-01-30T19:51:29 UTC (1643572289)
[ 6.026275] i2c /dev entries driver
[ 6.034057] Bluetooth: HCI UART driver ver 2.3
[ 6.038543] Bluetooth: HCI UART protocol H4 registered
[ 6.043731] Bluetooth: HCI UART protocol BCSP registered
[ 6.050445] cpu cpu0: dev_pm_opp_set_regulators: no regulator (vdd) found: -19
[ 6.058532] sdhci: Secure Digital Host Controller Interface driver
[ 6.064758] sdhci: Copyright(c) Pierre Ossman
[ 6.070220] sdhci-pltfm: SDHCI platform and OF driver helper
[ 6.077392] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 6.086273] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 6.086303] ledtrig-cpu: registered to indicate activity on CPUs
[ 6.097625] vdd_3v3: supplied by regen1
[ 6.102386] sdhci-omap 480b4000.mmc: no pinctrl state for ddr_1_8v mode
[ 6.109588] sdhci-omap 480d1000.mmc: supply vqmmc not found, using dummy regulator
[ 6.110565] sdhci-omap 480b4000.mmc: no pinctrl state for ddr_3_3v mode
[ 6.124816] sdhci-omap 480b4000.mmc: no pinctrl state for hs mode
[ 6.128326] ti-eqep-cnt 48442000.epwmss:eqep@0x48442180: invalid resource
[ 6.130981] sdhci-omap 480b4000.mmc: no pinctrl state for hs mode
[ 6.137847] ti-eqep-cnt: probe of 48442000.epwmss:eqep@0x48442180 failed with error -22
[ 6.153625] aic_dvdd_fixed: supplied by vdd_3v3
[ 6.160217] davinci-mcasp 4846c000.mcasp: IRQ common not found
[ 6.167907] NET: Registered protocol family 10
[ 6.169586] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA
[ 6.173156] Segment Routing with IPv6
[ 6.179504] sdhci-omap 480b4000.mmc: probe ok
[ 6.183319] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 6.194061] NET: Registered protocol family 17
[ 6.198577] can: controller area network core
[ 6.203033] NET: Registered protocol family 29
[ 6.207519] can: raw protocol
[ 6.210510] can: broadcast manager protocol
[ 6.214721] can: netlink gateway - max_hops=1
[ 6.219329] Bluetooth: RFCOMM TTY layer initialized
[ 6.224273] Bluetooth: RFCOMM socket layer initialized
[ 6.229522] Bluetooth: RFCOMM ver 1.11
[ 6.233306] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 6.238677] Bluetooth: BNEP filters: protocol multicast
[ 6.243957] Bluetooth: BNEP socket layer initialized
[ 6.248992] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 6.254974] Bluetooth: HIDP socket layer initialized
[ 6.260253] Key type dns_resolver registered
[ 6.264709] Registering SWP/SWPB emulation handler
[ 6.269561] omap_voltage_late_init: Voltage driver support not added
[ 6.275970] Power Management for TI OMAP4+ devices.
[ 6.281311] Loading compiled-in X.509 certificates
[ 6.287170] Key type encrypted registered
[ 6.291259] evm: Initialising EVM extended attributes:
[ 6.296447] evm: security.capability
[ 6.300048] evm: HMAC attrs: 0x1
[ 6.323577] mmc1: new MMC card at address 0001
[ 6.328704] mmcblk1: mmc1:0001 P1XXXX 7.20 GiB
[ 6.333557] mmcblk1boot0: mmc1:0001 P1XXXX partition 1 16.0 MiB
[ 6.339843] mmcblk1boot1: mmc1:0001 P1XXXX partition 2 16.0 MiB
[ 6.346038] mmcblk1rpmb: mmc1:0001 P1XXXX partition 3 128 KiB, chardev (244:0)
[ 6.346069] dmm 4e000000.dmm: workaround for errata i878 in use
[ 6.358764] mmcblk1: p1 p2 p3 p4 p5 p6 p7
[ 6.367065] dmm 4e000000.dmm: initialized all PAT entries
[ 6.375579] omap_i2c 48060000.i2c: bus 2 rev0.12 at 100 kHz
[ 6.381652] pca953x 0-0021: supply vcc not found, using dummy regulator
[ 6.388458] pca953x 0-0021: using no AI
[ 6.407653] tmp102 3-0048: initialized
[ 6.412292] -->tsc2013_probe
[ 6.415283] tsc2013 3-004b: GPIO not specified in DT (of_get_gpio returned -2)
[ 6.422546] tsc2013_probe-->tsc2013_hw_init
[ 6.426788] -->tsc2013_hw_init
[ 6.429870] tsc2013_probe-->tsc2013_sw_init
[ 6.434234] tsc2013_i2c_write_register : CFG[62] = 0xa58c
[ 6.439849] tsc2013_i2c_write_register : CFG[6a] = 0x0
[ 6.445190] tsc2013_i2c_write_register : CFG[72] = 0xb81c
[ 6.450866] input: tsc2013_ts as /devices/virtual/input/input0
[ 6.457641] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 6.466766] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 6.475128] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 6.481658] platform 40800000.dsp: Adding to iommu group 0
[ 6.488708] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 6.494842] platform 58820000.ipu: Adding to iommu group 1
[ 6.502105] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 6.508209] platform 55020000.ipu: Adding to iommu group 2
[ 6.515319] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 6.522796] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 6.529083] platform 41000000.dsp: Adding to iommu group 3
[ 6.535186] pwm-backlight backlight: supply power not found, using dummy regulator
[ 6.544036] DSS: OMAP DSS rev 6.1
[ 6.549530] omapdss_dss 58000000.dss: bound 58001000.dispc (ops 0xc0a43968)
[ 6.563812] [drm] Enabling DMM ywrap scrolling
[ 6.629333] Console: switching to colour frame buffer device 100x30
[ 6.652160] omapdrm omapdrm.0: [drm] fb0: omapdrmdrmfb frame buffer device
[ 6.660034] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 6.668731] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 6.678924] sdhci-omap 480d1000.mmc: supply vqmmc not found, using dummy regulator
[ 6.680664] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 6.687164] sdhci-omap 480d1000.mmc: no pinctrl state for sdr104 mode
[ 6.697753] sdhci-omap 480d1000.mmc: no pinctrl state for ddr50 mode
[ 6.704223] sdhci-omap 480d1000.mmc: no pinctrl state for sdr50 mode
[ 6.710662] sdhci-omap 480d1000.mmc: no pinctrl state for sdr25 mode
[ 6.717071] sdhci-omap 480d1000.mmc: no pinctrl state for sdr12 mode
[ 6.717071] sdhci-omap 480d1000.mmc: no pinctrl state for hs mode
[ 6.729614] sdhci-omap 480d1000.mmc: no pinctrl state for hs mode
[ 6.729888] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[ 6.735748] sdhci-omap 480d1000.mmc: no pinctrl state for hs200_1_8v mode
[ 6.749450] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 6.750885] ALSA device list:
[ 6.758300] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 6.761291] #0: mysb
[ 6.771362] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 6.780242] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 6.868225] mmc2: SDHCI controller on 480d1000.mmc [480d1000.mmc] using PIO
[ 6.875274] sdhci-omap 480d1000.mmc: probe ok
[ 6.881439] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 6.885009] sdhci-omap 480d1000.mmc: card claims to support voltages below defined range
[ 6.890319] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 6.931243] mmc2: new SDIO card at address 0001
[ 7.017913] EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: (null)
[ 7.026092] VFS: Mounted root (ext4 filesystem) on device 179:4.
[ 7.032897] devtmpfs: mounted
[ 7.036560] Freeing unused kernel memory: 1024K
[ 7.041290] Run /sbin/init as init process
[ 7.362091] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 7.384338] systemd[1]: Detected architecture arm.
Welcome to Arago 2021.09!
[ 7.411560] systemd[1]: Set hostname to <xxxxxx>.
[ 7.882385] systemd[1]: local-fs.target: Found ordering cycle on mnt-overlays.mount/start
[ 7.890686] systemd[1]: local-fs.target: Found dependency on mgc-system-init.service/start
...
Any hint very appreciated
thanks
angelo