Part Number: AM4377
Hello,
we have some issues with our own EtherCAT-Slave based on the AM4377. On TwinCAT everything works fine as it should. However, when using the Acontis EC-Engineer or the Acontis EC-Masterstack we most of the time get the error message "Line Crossed! At least one cable incorrectly connected (IN port and OUT port crossed)!". However we use the right ports and even EC-Engineer shows that the input and outputs are ok.
Due to availability issues of Ethernet Phys, we had to choose the DP83848, which is compliant with EtherCAT according to the Beckhoff "Application Note - PHY Selection Guide" page 8. To only thing to do is to "Use LED_LINK for link detection".
We set the link-polarity in tiescbsp.c:
Configured the eeprom to use enhanced link detection in tiesc_epprom.h:
Printing the values of the ESC registers 0x0140 & 0x0141:
0x0140: 80; 0x0141: 3e
This shows the enhanced link detection is enabled.
The schematics of the EtherCAT ports are shown in the attached PDF:
Can you please give us a hint, what might be the cause of the issues?
Thanks a lot for your help,
have a nice day,
Bernd