We are designing board OMAP3530/DM3730 based.
We want connected to MMC3 1.8V a WI2WI Wifi module SDIO 3.3V with voltage translator.
In BeagleBoard Refernce Manual, it is written :
8.26.2 MMC3 Signals
These signals can be used to provide an additional SD/MMC interface on an expansion
board. All of these signals are 1.8V, so if you plan to use the signals as an SD/MMC
interface, then a level shifter will be required.
But in http://processors.wiki.ti.com/index.php/SD-MMC_Usage_Notes_on_OMAP35x_and_AM37x :
MMC3 operates ONLY at 1.8V and cannot support external voltage translation
Our WI2WI module is SD1.1.
What is the chip reference of level shifter compatible with MMC3 port ?
Does anyone has already connected level shifter to MMC3 ?
Thanks in advance,
Seb