Hello,
I have a question regarding memory alignment requirements for the input data to TCP3e.
According to EDMA3 guide, when SAM=0 there are no limitations on source data alignment.
The TCP3e user's guide (SPRUGS1) describes the EDMA3 configuration for transferring the input data. Page 3-12 states:
"SRC (address) = User input data global start address (user input data must be 32-bit aligned)"
Since SAM=0,why is there a limitation that the input data to TCP3e must be aligned to 32 bits?
I would appreciate if this can be clarified.
Thanks
Ran