Other Parts Discussed in Thread: THS7303, PCA9543A
HI I have the leopard board dm365 with the MT9T031 I compile the kernel following this instructions
http://processors.wiki.ti.com/index.php/DMAI_GStreamer_Plug-In_Getting_Started_Guide
and base arago filesystem, this is my bootargs
setenv bootargs vpfe_capture.interface=1 mem=116M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,4M ip=192.168.0.122:eth:on
anyone knows why it does not detect the sensor? am I missing something else?
Linux video capture interface: v2.00
ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
dm365evm_enable_pca9543a
dm365evm_enable_pca9543a, status = -121
EVM: switch to HD imager video input
mt9t031 1-005d: No MT9T031 chip detected, register read ffffff87
vpfe-capture vpfe-capture: v4l2 sub device mt9t031 register fails
No sub devices registered
vpfe-capture: vpfe capture clocks disabled
vpfe_register_ccdc_device: DM365 ISIF
dm365_isif: probe of dm365_isif failed with error -22
af major#: 252, minor# 0
AF Driver initialized
aew major#: 251, minor# 0
AEW Driver initialized