Other Parts Discussed in Thread: TMS320DM8168
Hi all
- I am using board DM8168 (1GB DDRAM 2)
- I use syslink 02.00.00.67
- I wrote a sample:
- Load and start core DSP C674 from A8 (linux host) => success
- Call 'ProcMgr_read" function ==> have error code ProcMgr_E_TRANSLATE
- parameters for 'ProcMgr_read" function: ProcMgr_read(procMgrHandle,0xAB000000, &iNumByte,(Ptr) &value);
- Config memory for board
config ti.platforms.generic.Platform.Instance CPU =
ti.platforms.generic.Platform.create("CPU", {
clockRate: 800.0,
catalogName: "ti.catalog.c6000",
deviceName: "TMS320DM8168",
externalMemoryMap:
[
["DDR2",
{
base: 0xA0000000,
space: "code/data",
name: "DDR2",
len: 0x20000000,
access: "RWX",
}
],
["SR0",
{
base: 0x90000000,
space: "data",
name: "SR0",
len: 0x00100000,
access: "RWX",
}
],
["SR1",
{
base: 0x90100000,
space: "data",
name: "SR1",
len: 0x00100000,
access: "RWX",
}
],
["EXT_RAM",
{
base: 0x80000000,
space: "code/data",
name: "EXT_RAM",
len: 0x10000000,
access: "RWX",
}
],
],
l1DMode:"32k",
l1PMode:"32k",
l2Mode:"32k",
});
Any advice? Thanks