Hi,
I would like to know the list of examples available for C6678.
In the processor SDK, the steps to create CCS PDK examples for C6678 are more generic for the series of processors.
Please provide the steps, particularly for C6678.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know the list of examples available for C6678.
In the processor SDK, the steps to create CCS PDK examples for C6678 are more generic for the series of processors.
Please provide the steps, particularly for C6678.
How to generate the CCS PDK examples for C6678?
Pre-requisite
Steps to generate the PDK examples.
Once the processor_sdk_rtos_c667x_6_03_00_106 is installed, observe the PDK package, "pdk_c667x_2_0_16" under C:\ti

| cppi_evmc6678_c66BiosExampleProject |
| cppi_evmc6678_C66BiosTestProject |
| GPIO_LedBlink_C6678_EVM_c66xTestProject |
| hyplnk_evmc6678_C66BiosExampleProject |
| hyplnk_evmc6678_C66DevLibBiosExampleProject |
| I2C_BasicExample_C6678_Evm_c66xTestProject |
| I2C_BasicExample_C6678H_Evm_c66xExampleProject |
| NIMU_emacClientExample_EVMC6678C66BiosExampleProject |
| NIMU_emacExample_EVMC6678C66BiosExampleProject |
| nwalUnitTestC6678_C66TestProject |
| nwalUnitTestSaC6678_C66TestProject |
| PA_emacExample_evmc6678_C66BiosExampleProject |
| PA_multicoreExample_evmc6678_C66BiosExampleProject |
| PA_UnitTest_evmc6678_C66BiosTestProject |
| PCIE_evmc6678_wSoCFile_C66BiosExampleProject |
| PCIE_evmc6678_wSoCLib_C66BiosExampleProject |
| qmAcc_evmc6678_C66BiosTestProject |
| qmDCfg_evmc6678_C66BiosTestProject |
| qmDesc_evmc6678_C66BiosTestProject |
| qmInfra_evmc6678_C66BiosExampleProject |
| qmInfraMC_evmc6678_C66BiosExampleProject |
| qmInsRegion_evmc6678_C66BiosTestProject |
| qmQAlloc_evmc6678_C66BiosTestProject |
| qmQosFwCModel_evmc6678_C66BiosTestProject |
| qmQosSched_evmc6678_C66BiosTestProject |
| qmQosSchedCModel_evmc6678_C66BiosTestProject |
| qmQosSchedDropSched_evmc6678_C66BiosTestProject |
| qmQosSchedWide_evmc6678_C66BiosTestProject |
| qmQosTest_evmc6678_C66BiosTestProject |
| qmSCfg_evmc6678_C66BiosTestProject |
| qmSrioContext_evmc6678_C66BiosTestProject |
| qmSrioRtr_evmc6678_C66BiosTestProject |
| rm_evmc6678_C66BiosTestProject |
| rm_evmc6678_C66DspMtBiosTestProject |
| rmShared_evmc6678_C66BiosTestProject |
| SA_BasicExample_evmc6678_C66BiosExampleProject |
| SA_BasicExample_w3gpp_evmc6678_C66BiosExampleProject |
| SA_MultiCoreExample_evmc6678_C66BiosExampleProject |
| SA_MultiCoreExample_w3gpp_evmc6678_C66BiosExampleProject |
| SA_UnitTest_evmc6678_C66BiosTestProject |
| SA_UnitTest_w3gpp_evmc6678_C66BiosTestProject |
| SPI_BasicExample_C6678_c66xExampleProject |
| SPI_BasicExample_C6678_c66xTestProject |
| SRIO_Loopback_evmc6678_C66BiosTestProject |
| SRIO_LpbkDioIsr_evmc6678_C66BiosExampleProject |
| SRIO_MulticoreLpbk_evmc6678_C66BiosExampleProject |
| SRIO_TputBenchmarking_evmc6678_C66TestProject |
| transportQmssBenchmarkC6678C66ExampleProject |
| transportSrioBenchmarkC6678C66ExampleProject |
| transportSrioMultiBoardConsumerC6678C66ExampleProject |
| transportSrioMultiBoardProducerC6678C66ExampleProject |
| TSIP_evmc6678_c66exampleProject |
| TSIP_evmc6678_c66testProject |
| UART_BasicExample_C6678_c66xDMATestProject |
| UART_BasicExample_C6678_c66xExampleProject |
| UART_BasicExample_C6678_c66xTestProject |
Regards
Shankari G