Part Number: TDA3XEVM
Hi team,
Here's an issue from the customer may need your help;
The customer use the version of PROCESSOR_SDK_RADAR_03_08_00_00 for radar algorithm processing. And the tda3x used is self-designed.
PROCESSOR_SDK_RADAR_03_08_00_00\vision_sdk\build\Rules.make setting
MAKECONFIG=tda3xx_alps_bios_radar
MAKEAPPNAME=apps
The BSL can start normally, but appimage does not work, the log is as follows:

Trace the code and find the program is running to:
ipu1Core0EntryFuncPtr = (EntryFuncPtr_t) (sblEntryPoints.entryPoint[ SBLLIB_CORE_ID_IPU1_CPU0]);
ipu1Core0EntryFuncPtr();// Is this the entry address for APPimage?
Where is the entry address of this appimage configured?
They added debug information at main_ipu1_0.c main(), the console also doesn't log out. This main() calls main_common_ipu1_0.c main_comm0n(), then start Chains_main(). Restart radar use case.
Could you help check this case? Thanks.
Best Regards,
Cherry