Other Parts Discussed in Thread: AM1808
Hello All,
I think DM9621 can be used to connect to the USB2.0 OTG port we have on AM1808 to convert it to Ethernet interface. Some questions:
1. Has this DM9621 been used with AM1808
2. As far as I could find out, the bit rate should not impact if USB 2.0 full mode can be used, as it is ~60MBps practically 25MBps. Wheras Ethernet is only 12.5MBps. Is this conclusion correct?
3. Is any USB Hub needed in addition to DM9621?
4. What is the approx cost of this DM9621 part?
5. Any metrics on the it possible bit-rate reduction/side effects/known issues using the USB 2.0 OTG to USB-Ethernet convertor from Davicom?
6. Any other alterrnative devices we could have like used in Dlinks’?
7. Will using an Ethernet hub be a cheaper (fully TI) option, if data rates can be compromised to 50% full EMAC?
Please let me know
Best Regards,
Feroz