Part Number: AM3352
Other Parts Discussed in Thread: PCA9554, TPS65217, OMAP3530, DAC7512, LM3533, TPS65010, TPS65910, TPS65912, TWL6040, TPS65090, LP3971, LP3972, TPS51632, TPS62360, TPS65023
Hello,
So first a bit of a back story. I have got a media player which was discontinued by a company serveral years ago because the mother company pulled the plug. I managed to use Debian on it for serveral years after flashing this rootfs. Now, the problem is the Kernel is version 3.8.13 which is getting less and less useable with the time. I'am missing some old features. So I'am trying to make a new kernel.
This is what I have got:
- original uImage
- the dts:
/dts-v1/;
/ {
model = "Simple Audio AM335x Roomplayer";
interrupt-parent = <0x01>;
compatible = "sa,am335x-sa-roomplayer\0ti,am33xx";
#size-cells = <0x01>;
#address-cells = <0x01>;
__symbols__ {
vmmcsd_fixed = "/fixedregulator@0";
mcasp1 = "/ocp/mcasp@4803C000";
mcasp0 = "/ocp/mcasp@48038000";
aes = "/ocp/aes@53500000";
sham = "/ocp/sham@53100000";
ehrpwm2 = "/ocp/epwmss@48304000/ehrpwm@48304200";
ecap2 = "/ocp/epwmss@48304000/ecap@48304100";
epwmss2 = "/ocp/epwmss@48304000";
ehrpwm1 = "/ocp/epwmss@48302000/ehrpwm@48302200";
ecap1 = "/ocp/epwmss@48302000/ecap@48302100";
epwmss1 = "/ocp/epwmss@48302000";
ehrpwm0 = "/ocp/epwmss@48300000/ehrpwm@48300200";
ecap0 = "/ocp/epwmss@48300000/ecap@48300100";
epwmss0 = "/ocp/epwmss@48300000";
lcdc = "/ocp/lcdc@4830e000";
tscadc = "/ocp/tscadc@44e0d000";
cpsw_emac1 = "/ocp/ethernet@4a100000/slave@4a100300";
cpsw_emac0 = "/ocp/ethernet@4a100000/slave@4a100200";
davinci_mdio = "/ocp/ethernet@4a100000/mdio@4a101000";
mac = "/ocp/ethernet@4a100000";
usb_otg_hs = "/ocp/usb@47400000";
gpmc = "/ocp/gpmc@50000000";
spi1 = "/ocp/spi@481a0000";
flash = "/ocp/spi@48030000/m25p80@0";
spi0 = "/ocp/spi@48030000";
pruss = "/ocp/pruss@4a300000";
timer7 = "/ocp/timer@4804a000";
timer6 = "/ocp/timer@48048000";
timer5 = "/ocp/timer@48046000";
timer4 = "/ocp/timer@48044000";
timer3 = "/ocp/timer@48042000";
timer2 = "/ocp/timer@48040000";
timer1 = "/ocp/timer@44e31000";
dcan1 = "/ocp/d_can@481d0000";
dcan0 = "/ocp/d_can@481cc000";
wdt2 = "/ocp/wdt@44e35000";
mmc3 = "/ocp/mmc@47810000";
mmc2 = "/ocp/mmc@481d8000";
mmc1 = "/ocp/mmc@48060000";
i2c2 = "/ocp/i2c@4819c000";
i2c1 = "/ocp/i2c@4802a000";
wm8776 = "/ocp/i2c@44e0b000/wm8776@1b";
ldo4_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@6";
ldo3_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@5";
ldo2_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@4";
ldo1_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@3";
dcdc3_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@2";
dcdc2_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@1";
dcdc1_reg = "/ocp/i2c@44e0b000/tps@24/regulators/regulator@0";
tps = "/ocp/i2c@44e0b000/tps@24";
pca9554_2 = "/ocp/i2c@44e0b000/pca9554@23";
pca9554_1 = "/ocp/i2c@44e0b000/pca9554@22";
pca9554_0 = "/ocp/i2c@44e0b000/pca9554@20";
i2c0 = "/ocp/i2c@44e0b000";
uart6 = "/ocp/serial@481aa000";
uart5 = "/ocp/serial@481a8000";
uart4 = "/ocp/serial@481a6000";
uart3 = "/ocp/serial@48024000";
uart2 = "/ocp/serial@48022000";
uart1 = "/ocp/serial@44e09000";
rstctl = "/ocp/rstctl@0";
gpio4 = "/ocp/gpio@481ae000";
gpio3 = "/ocp/gpio@481ac000";
gpio2 = "/ocp/gpio@4804c000";
gpio1 = "/ocp/gpio@44e07000";
edma = "/ocp/edma@49000000";
intc = "/ocp/interrupt-controller@48200000";
ocp = "/ocp";
mcasp0_pins = "/pinmux@44e10800/pinmux_mcasp0_pins";
emmc2_pins = "/pinmux@44e10800/pinmux_emmc2_pins";
rstctl_pins = "/pinmux@44e10800/pinmux_rstctl_pins";
uart2_pins = "/pinmux@44e10800/pinmux_uart2_pins";
i2c0_pins = "/pinmux@44e10800/pinmux_i2c0_pins";
am33xx_pinmux = "/pinmux@44e10800";
cpu = "/cpus/cpu@0";
};
fixedregulator@0 {
phandle = <0x08>;
linux,phandle = <0x08>;
regulator-max-microvolt = <0x325aa0>;
regulator-min-microvolt = <0x325aa0>;
regulator-name = "vmmcsd_fixed";
compatible = "regulator-fixed";
};
ocp {
phandle = <0x12>;
linux,phandle = <0x12>;
ti,hwmods = "l3_main";
ranges;
#size-cells = <0x01>;
#address-cells = <0x01>;
compatible = "simple-bus";
sound {
sa,codec-clock-rate-48000 = <0x1770000>;
sa,codec-clock-rate-44100 = <0xac4400>;
sa,mcasp-controller = <0x0f>;
sa,audio-codec = <0x0e>;
sa,model = "Simple Audio AM335x Roomplayer";
compatible = "sa,am335x-sa-roomplayer-audio";
};
mcasp@4803C000 {
phandle = <0x4b>;
linux,phandle = <0x4b>;
dma-names = "tx\0rx";
dmas = <0x07 0x0a 0x07 0x0b>;
rx-dma-offset = <0x46400000>;
tx-dma-offset = <0x46400000>;
asp-chan-q = <0x02>;
status = "disabled";
interrupts = <0x52 0x53>;
reg = <0x4803c000 0x2000>;
ti,hwmods = "mcasp1";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap2-mcasp-audio";
};
mcasp@48038000 {
phandle = <0x0f>;
linux,phandle = <0x0f>;
rx-num-evt = <0x01>;
tx-num-evt = <0x01>;
serial-dir = <0x01 0x02 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00>;
num-serializer = <0x10>;
tdm-slots = <0x02>;
op-mode = <0x00>;
pinctrl-0 = <0x0d>;
pinctrl-names = "default";
dma-names = "tx\0rx";
dmas = <0x07 0x08 0x07 0x09>;
rx-dma-offset = <0x46000000>;
tx-dma-offset = <0x46000000>;
asp-chan-q = <0x02>;
status = "okay";
interrupts = <0x50 0x51>;
reg = <0x48038000 0x2000>;
ti,hwmods = "mcasp0";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap2-mcasp-audio";
};
aes@53500000 {
phandle = <0x4a>;
linux,phandle = <0x4a>;
status = "okay";
dma-names = "tx\0rx";
dmas = <0x07 0x06 0x07 0x05>;
interrupts = <0x66>;
interrupt-parent = <0x01>;
reg = <0x53500000 0xa0>;
#size-cells = <0x00>;
#address-cells = <0x01>;
ti,hwmods = "aes";
compatible = "ti,omap4-aes";
};
sham@53100000 {
phandle = <0x49>;
linux,phandle = <0x49>;
status = "okay";
dma-names = "rx";
dmas = <0x07 0x24>;
interrupts = <0x6d>;
interrupt-parent = <0x01>;
reg = <0x53100000 0x200>;
#size-cells = <0x00>;
#address-cells = <0x01>;
ti,hwmods = "sham";
compatible = "ti,omap4-sham";
};
epwmss@48304000 {
phandle = <0x46>;
linux,phandle = <0x46>;
ranges = <0x48304100 0x48304100 0x80 0x48304180 0x48304180 0x80 0x48304200 0x48304200 0x80>;
status = "disabled";
#size-cells = <0x01>;
#address-cells = <0x01>;
ti,hwmods = "epwmss2";
reg = <0x48304000 0x10>;
compatible = "ti,am33xx-pwmss";
ehrpwm@48304200 {
phandle = <0x48>;
linux,phandle = <0x48>;
status = "disabled";
ti,hwmods = "ehrpwm2";
reg = <0x48304200 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ehrpwm";
};
ecap@48304100 {
phandle = <0x47>;
linux,phandle = <0x47>;
status = "disabled";
ti,hwmods = "ecap2";
reg = <0x48304100 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ecap";
};
};
epwmss@48302000 {
phandle = <0x43>;
linux,phandle = <0x43>;
ranges = <0x48302100 0x48302100 0x80 0x48302180 0x48302180 0x80 0x48302200 0x48302200 0x80>;
status = "disabled";
#size-cells = <0x01>;
#address-cells = <0x01>;
ti,hwmods = "epwmss1";
reg = <0x48302000 0x10>;
compatible = "ti,am33xx-pwmss";
ehrpwm@48302200 {
phandle = <0x45>;
linux,phandle = <0x45>;
status = "disabled";
ti,hwmods = "ehrpwm1";
reg = <0x48302200 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ehrpwm";
};
ecap@48302100 {
phandle = <0x44>;
linux,phandle = <0x44>;
status = "disabled";
ti,hwmods = "ecap1";
reg = <0x48302100 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ecap";
};
};
epwmss@48300000 {
phandle = <0x40>;
linux,phandle = <0x40>;
ranges = <0x48300100 0x48300100 0x80 0x48300180 0x48300180 0x80 0x48300200 0x48300200 0x80>;
status = "disabled";
#size-cells = <0x01>;
#address-cells = <0x01>;
ti,hwmods = "epwmss0";
reg = <0x48300000 0x10>;
compatible = "ti,am33xx-pwmss";
ehrpwm@48300200 {
phandle = <0x42>;
linux,phandle = <0x42>;
status = "disabled";
ti,hwmods = "ehrpwm0";
reg = <0x48300200 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ehrpwm";
};
ecap@48300100 {
phandle = <0x41>;
linux,phandle = <0x41>;
status = "disabled";
ti,hwmods = "ecap0";
reg = <0x48300100 0x80>;
#pwm-cells = <0x03>;
compatible = "ti,am33xx-ecap";
};
};
lcdc@4830e000 {
phandle = <0x3f>;
linux,phandle = <0x3f>;
ti,hwmods = "lcdc";
status = "disabled";
interrupts = <0x24>;
reg = <0x4830e000 0x1000>;
compatible = "ti,am3352-lcdc\0ti,da830-lcdc";
};
tscadc@44e0d000 {
phandle = <0x3e>;
linux,phandle = <0x3e>;
status = "disabled";
ti,hwmods = "adc_tsc";
interrupts = <0x10>;
interrupt-parent = <0x01>;
reg = <0x44e0d000 0x1000>;
compatible = "ti,ti-tscadc";
};
ethernet@4a100000 {
phandle = <0x3b>;
linux,phandle = <0x3b>;
disable-napi;
ranges;
interrupts = <0x28 0x29 0x2a 0x2b>;
interrupt-parent = <0x01>;
#size-cells = <0x01>;
#address-cells = <0x01>;
reg = <0x4a100000 0x800 0x4a101200 0x100>;
cpts_clock_shift = <0x1d>;
cpts_clock_mult = <0x80000000>;
cpts_active_slave = <0x00>;
slaves = <0x02>;
mac_control = <0x20>;
rx_descs = <0x40>;
no_bd_ram = <0x00>;
bd_ram_size = <0x2000>;
ale_entries = <0x400>;
cpdma_channels = <0x08>;
ti,hwmods = "cpgmac0";
compatible = "ti,cpsw";
slave@4a100300 {
phandle = <0x3d>;
linux,phandle = <0x3d>;
phy_id = <0x0c 0x01>;
mac-address = [d0 ff 50 01 21 04];
};
slave@4a100200 {
phandle = <0x3c>;
linux,phandle = <0x3c>;
phy_id = <0x0c 0x01>;
mac-address = [d0 ff 50 01 21 02];
};
mdio@4a101000 {
phandle = <0x0c>;
linux,phandle = <0x0c>;
reg = <0x4a101000 0x100>;
bus_freq = <0xf4240>;
ti,hwmods = "davinci_mdio";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,davinci_mdio";
};
};
usb@47400000 {
phandle = <0x3a>;
linux,phandle = <0x3a>;
interface_type = <0x01>;
status = "okay";
ti,hwmods = "usb_otg_hs";
power = <0xfa>;
port1-mode = <0x01>;
port0-mode = <0x01>;
ram-bits = <0x0c>;
num-eps = <0x10>;
multipoint = <0x01>;
interrupts = <0x11 0x12 0x13>;
reg = <0x47400000 0x1000 0x47401000 0x800 0x47401800 0x800>;
compatible = "ti,musb-am33xx";
};
nop-phy@1 {
compatible = "nop-xceiv-usb";
};
nop-phy@0 {
compatible = "nop-xceiv-usb";
};
gpmc@50000000 {
phandle = <0x39>;
linux,phandle = <0x39>;
status = "disabled";
#size-cells = <0x01>;
#address-cells = <0x02>;
gpmc,num-waitpins = <0x02>;
gpmc,num-cs = <0x07>;
interrupts = <0x64>;
reg = <0x50000000 0x1000000>;
ti,hwmods = "gpmc";
compatible = "ti,am3352-gpmc";
};
spi@481a0000 {
phandle = <0x38>;
linux,phandle = <0x38>;
status = "disabled";
dma-names = "tx0\0rx0\0tx1\0rx1";
dmas = <0x07 0x2a 0x07 0x2b 0x07 0x2c 0x07 0x2d>;
ti,hwmods = "spi1";
ti,spi-num-cs = <0x02>;
interrupt = <0x7d>;
reg = <0x481a0000 0x400>;
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap4-mcspi";
};
spi@48030000 {
phandle = <0x36>;
linux,phandle = <0x36>;
status = "okay";
dma-names = "tx0\0rx0\0tx1\0rx1";
dmas = <0x07 0x10 0x07 0x11 0x07 0x12 0x07 0x13>;
ti,hwmods = "spi0";
ti,spi-num-cs = <0x02>;
interrupt = <0x41>;
reg = <0x48030000 0x400>;
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap4-mcspi";
m25p80@0 {
phandle = <0x37>;
linux,phandle = <0x37>;
m25p,fast-read;
spi-max-frequency = <0x2625a00>;
reg = <0x00>;
compatible = "atmel,at25df641";
#size-cells = <0x01>;
#address-cells = <0x01>;
ethaddr@7F0000 {
reg = <0x7f0000 0x10000>;
label = "MAC Address";
};
uImage@100000 {
read-only;
reg = <0x100000 0x500000>;
label = "Linux Kernel";
};
ubootenv@F0000 {
reg = <0xf0000 0x10000>;
label = "U-Boot Environment";
};
uboot@80000 {
read-only;
reg = <0x80000 0x70000>;
label = "U-Boot";
};
spl@0 {
read-only;
reg = <0x00 0x80000>;
label = "U-Boot SPL";
};
};
};
rtc@44e3e000 {
ti,system-power-controller;
ti,hwmods = "rtc";
interrupts = <0x4b 0x4c>;
reg = <0x44e3e000 0x1000>;
compatible = "ti,da830-rtc";
};
pruss@4a300000 {
phandle = <0x35>;
linux,phandle = <0x35>;
interrupts = <0x14 0x15 0x16 0x17 0x18 0x19 0x1a 0x1b>;
status = "disabled";
interrupt-parent = <0x01>;
ti,pintc-offset = <0x20000>;
reg = <0x4a300000 0x80000>;
ti,deassert-hard-reset = "pruss\0pruss";
ti,hwmods = "pruss";
compatible = "ti,pruss-v2";
};
timer@4804a000 {
phandle = <0x34>;
linux,phandle = <0x34>;
ti,timer-pwm;
ti,hwmods = "timer7";
interrupts = <0x5f>;
reg = <0x4804a000 0x400>;
compatible = "ti,omap2-timer";
};
timer@48048000 {
phandle = <0x33>;
linux,phandle = <0x33>;
ti,timer-pwm;
ti,hwmods = "timer6";
interrupts = <0x5e>;
reg = <0x48048000 0x400>;
compatible = "ti,omap2-timer";
};
timer@48046000 {
phandle = <0x32>;
linux,phandle = <0x32>;
ti,timer-pwm;
ti,hwmods = "timer5";
interrupts = <0x5d>;
reg = <0x48046000 0x400>;
compatible = "ti,omap2-timer";
};
timer@48044000 {
phandle = <0x31>;
linux,phandle = <0x31>;
ti,timer-pwm;
ti,hwmods = "timer4";
interrupts = <0x5c>;
reg = <0x48044000 0x400>;
compatible = "ti,omap2-timer";
};
timer@48042000 {
phandle = <0x30>;
linux,phandle = <0x30>;
ti,hwmods = "timer3";
interrupts = <0x45>;
reg = <0x48042000 0x400>;
compatible = "ti,omap2-timer";
};
timer@48040000 {
status = "disabled";
phandle = <0x2f>;
linux,phandle = <0x2f>;
ti,hwmods = "timer2";
interrupts = <0x44>;
reg = <0x48040000 0x400>;
compatible = "ti,omap2-timer";
};
timer@44e31000 {
status = "disabled";
phandle = <0x2e>;
linux,phandle = <0x2e>;
ti,timer-alwon;
ti,hwmods = "timer1";
interrupts = <0x43>;
reg = <0x44e31000 0x400>;
compatible = "ti,omap2-timer";
};
d_can@481d0000 {
phandle = <0x2d>;
linux,phandle = <0x2d>;
status = "disabled";
interrupts = <0x37>;
reg = <0x481d0000 0x2000>;
ti,hwmods = "d_can1";
compatible = "bosch,d_can";
};
d_can@481cc000 {
phandle = <0x2c>;
linux,phandle = <0x2c>;
status = "disabled";
interrupts = <0x34>;
reg = <0x481cc000 0x2000>;
ti,hwmods = "d_can0";
compatible = "bosch,d_can";
};
wdt@44e35000 {
phandle = <0x2b>;
linux,phandle = <0x2b>;
interrupts = <0x5b>;
reg = <0x44e35000 0x1000>;
ti,hwmods = "wd_timer2";
compatible = "ti,omap3-wdt";
};
mmc@47810000 {
phandle = <0x2a>;
linux,phandle = <0x2a>;
status = "disabled";
ti,needs-special-hs-handling;
ti,needs-special-reset;
ti,hwmods = "mmc3";
compatible = "ti,omap3-hsmmc";
};
mmc@481d8000 {
phandle = <0x29>;
linux,phandle = <0x29>;
ti,vcc-aux-disable-is-sleep;
pinctrl-0 = <0x0b>;
pinctrl-names = "default";
reset-names = "eMMC_RSTn";
reset = <0x0a 0x00 0x00>;
ti,non-removable;
bus-width = <0x08>;
vmmc-supply = <0x09>;
status = "okay";
dma-names = "tx\0rx";
dmas = <0x07 0x02 0x07 0x03>;
ti,needs-special-hs-handling;
ti,needs-special-reset;
ti,hwmods = "mmc2";
compatible = "ti,omap3-hsmmc";
};
mmc@48060000 {
phandle = <0x28>;
linux,phandle = <0x28>;
ti,vcc-aux-disable-is-sleep;
vmmc-supply = <0x08>;
status = "okay";
dma-names = "tx\0rx";
dmas = <0x07 0x18 0x07 0x19>;
ti,needs-special-hs-handling;
ti,needs-special-reset;
ti,dual-volt;
ti,hwmods = "mmc1";
compatible = "ti,omap3-hsmmc";
};
i2c@4819c000 {
phandle = <0x27>;
linux,phandle = <0x27>;
status = "disabled";
interrupts = <0x1e>;
reg = <0x4819c000 0x1000>;
ti,hwmods = "i2c3";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap4-i2c";
};
i2c@4802a000 {
phandle = <0x26>;
linux,phandle = <0x26>;
status = "disabled";
interrupts = <0x47>;
reg = <0x4802a000 0x1000>;
ti,hwmods = "i2c2";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap4-i2c";
};
i2c@44e0b000 {
phandle = <0x1c>;
linux,phandle = <0x1c>;
pinctrl-0 = <0x06>;
pinctrl-names = "default";
clock-frequency = <0x186a0>;
status = "okay";
interrupts = <0x46>;
reg = <0x44e0b000 0x1000>;
ti,hwmods = "i2c1";
#size-cells = <0x00>;
#address-cells = <0x01>;
compatible = "ti,omap4-i2c";
wm8776@1b {
phandle = <0x0e>;
linux,phandle = <0x0e>;
reg = <0x1b>;
compatible = "wlf,wm8776";
};
tps@24 {
phandle = <0x20>;
linux,phandle = <0x20>;
interrupts = <0x07>;
interrupt-parent = <0x01>;
ti,pmic-shutdown-controller;
compatible = "ti,tps65217";
reg = <0x24>;
regulators {
#size-cells = <0x00>;
#address-cells = <0x01>;
regulator@6 {
phandle = <0x25>;
linux,phandle = <0x25>;
regulator-always-on;
regulator-compatible = "ldo4";
reg = <0x06>;
};
regulator@5 {
phandle = <0x09>;
linux,phandle = <0x09>;
regulator-always-on;
regulator-max-microvolt = <0x1b7740>;
regulator-min-microvolt = <0x1b7740>;
regulator-compatible = "ldo3";
reg = <0x05>;
};
regulator@4 {
phandle = <0x24>;
linux,phandle = <0x24>;
regulator-always-on;
regulator-compatible = "ldo2";
reg = <0x04>;
};
regulator@3 {
phandle = <0x23>;
linux,phandle = <0x23>;
regulator-always-on;
regulator-compatible = "ldo1";
reg = <0x03>;
};
regulator@2 {
phandle = <0x22>;
linux,phandle = <0x22>;
regulator-always-on;
regulator-boot-on;
regulator-max-microvolt = <0x118c30>;
regulator-min-microvolt = <0xe1d48>;
regulator-name = "vdd_core";
regulator-compatible = "dcdc3";
reg = <0x02>;
};
regulator@1 {
phandle = <0x02>;
linux,phandle = <0x02>;
regulator-always-on;
regulator-boot-on;
regulator-max-microvolt = <0x1437c8>;
regulator-min-microvolt = <0xe1d48>;
regulator-name = "vdd_mpu";
regulator-compatible = "dcdc2";
reg = <0x01>;
};
regulator@0 {
phandle = <0x21>;
linux,phandle = <0x21>;
regulator-always-on;
regulator-compatible = "dcdc1";
reg = <0x00>;
};
};
};
pca9554@23 {
phandle = <0x1f>;
linux,phandle = <0x1f>;
reg = <0x23>;
compatible = "nxp,pca9554";
};
pca9554@22 {
phandle = <0x1e>;
linux,phandle = <0x1e>;
reg = <0x22>;
compatible = "nxp,pca9554";
};
pca9554@20 {
phandle = <0x1d>;
linux,phandle = <0x1d>;
reg = <0x20>;
compatible = "nxp,pca9554";
};
};
serial@481aa000 {
phandle = <0x1b>;
linux,phandle = <0x1b>;
status = "disabled";
interrupts = <0x2e>;
reg = <0x481aa000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart6";
compatible = "ti,omap3-uart";
};
serial@481a8000 {
phandle = <0x1a>;
linux,phandle = <0x1a>;
status = "disabled";
interrupts = <0x2d>;
reg = <0x481a8000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart5";
compatible = "ti,omap3-uart";
};
serial@481a6000 {
phandle = <0x19>;
linux,phandle = <0x19>;
status = "disabled";
interrupts = <0x2c>;
reg = <0x481a6000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart4";
compatible = "ti,omap3-uart";
};
serial@48024000 {
phandle = <0x18>;
linux,phandle = <0x18>;
status = "disabled";
interrupts = <0x4a>;
reg = <0x48024000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart3";
compatible = "ti,omap3-uart";
};
serial@48022000 {
phandle = <0x17>;
linux,phandle = <0x17>;
pinctrl-0 = <0x05>;
pinctrl-names = "default";
status = "okay";
interrupts = <0x49>;
reg = <0x48022000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart2";
compatible = "ti,omap3-uart";
};
serial@44e09000 {
phandle = <0x16>;
linux,phandle = <0x16>;
status = "okay";
interrupts = <0x48>;
reg = <0x44e09000 0x2000>;
clock-frequency = <0x2dc6c00>;
ti,hwmods = "uart1";
compatible = "ti,omap3-uart";
};
rstctl@0 {
phandle = <0x0a>;
linux,phandle = <0x0a>;
gpio-names = "eMMC_RSTn";
gpios = <0x04 0x14 0x00>;
#reset-cells = <0x02>;
pinctrl-0 = <0x03>;
pinctrl-names = "default";
compatible = "gpio-rctrl";
status = "okay";
};
gpio@481ae000 {
phandle = <0x15>;
linux,phandle = <0x15>;
interrupts = <0x3e>;
reg = <0x481ae000 0x1000>;
#interrupt-cells = <0x01>;
interrupt-controller;
#gpio-cells = <0x02>;
gpio-controller;
ti,hwmods = "gpio4";
compatible = "ti,omap4-gpio";
};
gpio@481ac000 {
phandle = <0x14>;
linux,phandle = <0x14>;
interrupts = <0x20>;
reg = <0x481ac000 0x1000>;
#interrupt-cells = <0x01>;
interrupt-controller;
#gpio-cells = <0x02>;
gpio-controller;
ti,hwmods = "gpio3";
compatible = "ti,omap4-gpio";
};
gpio@4804c000 {
phandle = <0x04>;
linux,phandle = <0x04>;
interrupts = <0x62>;
reg = <0x4804c000 0x1000>;
#interrupt-cells = <0x01>;
interrupt-controller;
#gpio-cells = <0x02>;
gpio-controller;
ti,hwmods = "gpio2";
compatible = "ti,omap4-gpio";
};
gpio@44e07000 {
phandle = <0x13>;
linux,phandle = <0x13>;
interrupts = <0x60>;
reg = <0x44e07000 0x1000>;
#interrupt-cells = <0x01>;
interrupt-controller;
#gpio-cells = <0x02>;
gpio-controller;
ti,hwmods = "gpio1";
compatible = "ti,omap4-gpio";
};
edma@49000000 {
phandle = <0x07>;
linux,phandle = <0x07>;
ti,edma-xbar-event-map = <0x20 0x0c 0x1e 0x14>;
ti,edma-default-queue = <0x01>;
ti,edma-queue-priority-map = <0x00 0x00 0x01 0x01 0x02 0x02>;
ti,edma-queue-tc-map = <0x00 0x00 0x01 0x01 0x02 0x02>;
ti,edma-slots = <0x100>;
ti,edma-regions = <0x04>;
dma-channels = <0x40>;
#dma-cells = <0x01>;
interrupts = <0x0c 0x0d 0x0e>;
interrupt-parent = <0x01>;
reg = <0x49000000 0x10000 0x44e10f90 0x40>;
ti,hwmods = "tpcc\0tptc0\0tptc1\0tptc2";
compatible = "ti,edma3";
};
interrupt-controller@48200000 {
phandle = <0x01>;
linux,phandle = <0x01>;
reg = <0x48200000 0x1000>;
ti,intc-size = <0x80>;
#interrupt-cells = <0x01>;
interrupt-controller;
compatible = "ti,omap2-intc";
};
};
pinmux@44e10800 {
phandle = <0x11>;
linux,phandle = <0x11>;
pinctrl-single,function-mask = <0x7f>;
pinctrl-single,register-width = <0x20>;
#size-cells = <0x00>;
#address-cells = <0x01>;
reg = <0x44e10800 0x238>;
compatible = "pinctrl-single";
pinmux_mcasp0_pins {
phandle = <0x0d>;
linux,phandle = <0x0d>;
pinctrl-single,pins = <0x190 0x08 0x194 0x08 0x198 0x08 0x19c 0x28 0x1a0 0x08 0x1a4 0x08 0x1a8 0x28 0x1ac 0x28>;
};
pinmux_emmc2_pins {
phandle = <0x0b>;
linux,phandle = <0x0b>;
pinctrl-single,pins = <0x80 0x32 0x84 0x32 0x00 0x31 0x04 0x31 0x08 0x31 0x0c 0x31 0x10 0x31 0x14 0x31 0x18 0x31 0x1c 0x31>;
};
pinmux_rstctl_pins {
phandle = <0x03>;
linux,phandle = <0x03>;
pinctrl-single,pins = <0x50 0x17>;
};
pinmux_uart2_pins {
phandle = <0x05>;
linux,phandle = <0x05>;
pinctrl-single,pins = <0x180 0x30>;
};
pinmux_i2c0_pins {
phandle = <0x06>;
linux,phandle = <0x06>;
pinctrl-single,pins = <0x188 0x70 0x18c 0x70>;
};
};
soc {
compatible = "ti,omap-infra";
mpu {
ti,hwmods = "mpu";
compatible = "ti,omap3-mpu";
};
};
cpus {
cpu@0 {
phandle = <0x10>;
linux,phandle = <0x10>;
cpu0-supply = <0x02>;
clock-latency = <0x493e0>;
voltage-tolerance = <0x02>;
operating-points = <0xf4240 0x149970 0xc3500 0x13d620 0x927c0 0x10f7c0 0x493e0 0xec928>;
compatible = "arm,cortex-a8";
};
};
memory {
reg = <0x80000000 0x20000000>;
device_type = "memory";
};
aliases {
serial5 = "/ocp/serial@481aa000";
serial4 = "/ocp/serial@481a8000";
serial3 = "/ocp/serial@481a6000";
serial2 = "/ocp/serial@48024000";
serial1 = "/ocp/serial@48022000";
serial0 = "/ocp/serial@44e09000";
};
chosen {
bootargs = "console=ttyO0,115200n8 drm.debug=7 root=/dev/sda1 rw rootfstype=ext4 rootwait";
};
};
- config.gz/.config
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.8.13 Kernel Configuration
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_GENERIC_GPIO=y
CONFIG_HAVE_PROC_CPU=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_NEED_DMA_MAP_STATE=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_ARM_PATCH_PHYS_VIRT=y
CONFIG_GENERIC_BUG=y
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_HAVE_IRQ_WORK=y
CONFIG_IRQ_WORK=y
CONFIG_BUILDTIME_EXTABLE_SORT=y
#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_CROSS_COMPILE=""
CONFIG_LOCALVERSION=""
# CONFIG_LOCALVERSION_AUTO is not set
CONFIG_HAVE_KERNEL_GZIP=y
CONFIG_HAVE_KERNEL_LZMA=y
CONFIG_HAVE_KERNEL_XZ=y
CONFIG_HAVE_KERNEL_LZO=y
# CONFIG_KERNEL_GZIP is not set
# CONFIG_KERNEL_LZMA is not set
# CONFIG_KERNEL_XZ is not set
CONFIG_KERNEL_LZO=y
CONFIG_DEFAULT_HOSTNAME="(none)"
CONFIG_SWAP=y
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
CONFIG_POSIX_MQUEUE=y
CONFIG_POSIX_MQUEUE_SYSCTL=y
# CONFIG_FHANDLE is not set
# CONFIG_AUDIT is not set
CONFIG_HAVE_GENERIC_HARDIRQS=y
#
# IRQ subsystem
#
CONFIG_GENERIC_HARDIRQS=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_GENERIC_IRQ_SHOW=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_CHIP=y
CONFIG_IRQ_DOMAIN=y
# CONFIG_IRQ_DOMAIN_DEBUG is not set
CONFIG_SPARSE_IRQ=y
CONFIG_KTIME_SCALAR=y
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
#
# Timers subsystem
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
#
# CPU/Task time and stats accounting
#
CONFIG_TICK_CPU_ACCOUNTING=y
CONFIG_BSD_PROCESS_ACCT=y
CONFIG_BSD_PROCESS_ACCT_V3=y
CONFIG_TASKSTATS=y
CONFIG_TASK_DELAY_ACCT=y
CONFIG_TASK_XACCT=y
CONFIG_TASK_IO_ACCOUNTING=y
#
# RCU Subsystem
#
CONFIG_TINY_RCU=y
# CONFIG_PREEMPT_RCU is not set
# CONFIG_TREE_RCU_TRACE is not set
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=17
CONFIG_CGROUPS=y
# CONFIG_CGROUP_DEBUG is not set
# CONFIG_CGROUP_FREEZER is not set
# CONFIG_CGROUP_DEVICE is not set
# CONFIG_CPUSETS is not set
CONFIG_CGROUP_CPUACCT=y
CONFIG_RESOURCE_COUNTERS=y
CONFIG_MEMCG=y
# CONFIG_MEMCG_SWAP is not set
# CONFIG_MEMCG_KMEM is not set
# CONFIG_CGROUP_PERF is not set
CONFIG_CGROUP_SCHED=y
CONFIG_FAIR_GROUP_SCHED=y
# CONFIG_CFS_BANDWIDTH is not set
# CONFIG_RT_GROUP_SCHED is not set
CONFIG_BLK_CGROUP=y
# CONFIG_DEBUG_BLK_CGROUP is not set
# CONFIG_CHECKPOINT_RESTORE is not set
CONFIG_NAMESPACES=y
CONFIG_UTS_NS=y
CONFIG_IPC_NS=y
# CONFIG_USER_NS is not set
CONFIG_PID_NS=y
CONFIG_NET_NS=y
CONFIG_UIDGID_CONVERTED=y
# CONFIG_UIDGID_STRICT_TYPE_CHECKS is not set
CONFIG_SCHED_AUTOGROUP=y
CONFIG_MM_OWNER=y
# CONFIG_SYSFS_DEPRECATED is not set
# CONFIG_RELAY is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE="initramfs.cpio.gz"
CONFIG_INITRAMFS_ROOT_UID=0
CONFIG_INITRAMFS_ROOT_GID=0
CONFIG_RD_GZIP=y
# CONFIG_RD_BZIP2 is not set
# CONFIG_RD_LZMA is not set
# CONFIG_RD_XZ is not set
# CONFIG_RD_LZO is not set
CONFIG_INITRAMFS_COMPRESSION_NONE=y
# CONFIG_INITRAMFS_COMPRESSION_GZIP is not set
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
CONFIG_EXPERT=y
CONFIG_HAVE_UID16=y
CONFIG_UID16=y
# CONFIG_SYSCTL_SYSCALL is not set
CONFIG_KALLSYMS=y
CONFIG_KALLSYMS_ALL=y
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y
# CONFIG_EMBEDDED is not set
CONFIG_HAVE_PERF_EVENTS=y
CONFIG_PERF_USE_VMALLOC=y
#
# Kernel Performance Events And Counters
#
CONFIG_PERF_EVENTS=y
# CONFIG_DEBUG_PERF_USE_VMALLOC is not set
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_COMPAT_BRK=y
CONFIG_SLAB=y
# CONFIG_SLUB is not set
# CONFIG_SLOB is not set
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
# CONFIG_JUMP_LABEL is not set
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_ARCH_TRACEHOOK=y
CONFIG_HAVE_DMA_ATTRS=y
CONFIG_HAVE_DMA_CONTIGUOUS=y
CONFIG_GENERIC_SMP_IDLE_THREAD=y
CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
CONFIG_HAVE_CLK=y
CONFIG_HAVE_DMA_API_DEBUG=y
CONFIG_HAVE_HW_BREAKPOINT=y
CONFIG_HAVE_ARCH_JUMP_LABEL=y
CONFIG_ARCH_WANT_IPC_PARSE_VERSION=y
CONFIG_HAVE_ARCH_SECCOMP_FILTER=y
CONFIG_HAVE_MOD_ARCH_SPECIFIC=y
CONFIG_MODULES_USE_ELF_REL=y
CONFIG_CLONE_BACKWARDS=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
# CONFIG_MODULES is not set
CONFIG_BLOCK=y
CONFIG_LBDAF=y
CONFIG_BLK_DEV_BSG=y
# CONFIG_BLK_DEV_BSGLIB is not set
CONFIG_BLK_DEV_INTEGRITY=y
# CONFIG_BLK_DEV_THROTTLING is not set
#
# Partition Types
#
CONFIG_PARTITION_ADVANCED=y
# CONFIG_ACORN_PARTITION is not set
# CONFIG_OSF_PARTITION is not set
# CONFIG_AMIGA_PARTITION is not set
# CONFIG_ATARI_PARTITION is not set
CONFIG_MAC_PARTITION=y
CONFIG_MSDOS_PARTITION=y
# CONFIG_BSD_DISKLABEL is not set
# CONFIG_MINIX_SUBPARTITION is not set
# CONFIG_SOLARIS_X86_PARTITION is not set
# CONFIG_UNIXWARE_DISKLABEL is not set
# CONFIG_LDM_PARTITION is not set
# CONFIG_SGI_PARTITION is not set
# CONFIG_ULTRIX_PARTITION is not set
# CONFIG_SUN_PARTITION is not set
# CONFIG_KARMA_PARTITION is not set
CONFIG_EFI_PARTITION=y
# CONFIG_SYSV68_PARTITION is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_CFQ_GROUP_IOSCHED is not set
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
CONFIG_UNINLINE_SPIN_UNLOCK=y
# CONFIG_FREEZER is not set
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_MULTIPLATFORM is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_BCM2835 is not set
# CONFIG_ARCH_CNS3XXX is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_SIRF is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_MXS is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C24XX is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_EXYNOS is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_NOMADIK is not set
# CONFIG_PLAT_SPEAR is not set
# CONFIG_ARCH_DAVINCI is not set
CONFIG_ARCH_OMAP=y
# CONFIG_ARCH_VT8500_SINGLE is not set
CONFIG_GPIO_PCA953X=y
#
# TI OMAP Common Features
#
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# OMAP Feature Selections
#
CONFIG_OMAP_RESET_CLOCKS=y
CONFIG_OMAP_MUX=y
CONFIG_OMAP_MUX_DEBUG=y
CONFIG_OMAP_MUX_WARNINGS=y
CONFIG_OMAP_MBOX_FWK=y
CONFIG_OMAP_MBOX_KFIFO_SIZE=256
CONFIG_OMAP_32K_TIMER=y
# CONFIG_OMAP3_L2_AUX_SECURE_SAVE_RESTORE is not set
CONFIG_OMAP_32K_TIMER_HZ=512
CONFIG_OMAP_DM_TIMER=y
CONFIG_OMAP_PM_NOOP=y
CONFIG_MACH_OMAP_GENERIC=y
#
# TI OMAP2/3/4 Specific Features
#
CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
CONFIG_SOC_HAS_OMAP2_SDRC=y
# CONFIG_ARCH_OMAP2 is not set
CONFIG_ARCH_OMAP3=y
# CONFIG_ARCH_OMAP4 is not set
# CONFIG_SOC_OMAP5 is not set
CONFIG_SOC_OMAP3430=y
# CONFIG_SOC_TI81XX is not set
CONFIG_SOC_AM33XX=y
#
# OMAP Board Type
#
CONFIG_MACH_AM335XEVM=y
CONFIG_MACH_AM335XIAEVM=y
CONFIG_MACH_TAM335X=y
# CONFIG_MACH_OMAP3_BEAGLE is not set
# CONFIG_MACH_DEVKIT8000 is not set
# CONFIG_MACH_OMAP_LDP is not set
# CONFIG_MACH_OMAP3530_LV_SOM is not set
# CONFIG_MACH_OMAP3_TORPEDO is not set
# CONFIG_MACH_OVERO is not set
# CONFIG_MACH_OMAP3EVM is not set
# CONFIG_MACH_OMAP3517EVM is not set
# CONFIG_MACH_CRANEBOARD is not set
# CONFIG_MACH_OMAP3_PANDORA is not set
# CONFIG_MACH_TOUCHBOOK is not set
# CONFIG_MACH_OMAP_3430SDP is not set
# CONFIG_MACH_NOKIA_RM680 is not set
# CONFIG_MACH_NOKIA_RX51 is not set
# CONFIG_MACH_OMAP_ZOOM2 is not set
# CONFIG_MACH_OMAP_ZOOM3 is not set
# CONFIG_MACH_CM_T35 is not set
# CONFIG_MACH_CM_T3517 is not set
# CONFIG_MACH_IGEP0020 is not set
# CONFIG_MACH_IGEP0030 is not set
# CONFIG_MACH_SBC3530 is not set
# CONFIG_MACH_OMAP_3630SDP is not set
# CONFIG_OMAP3_EMU is not set
# CONFIG_OMAP3_SDRC_AC_TIMING is not set
# CONFIG_ARCH_VT8500 is not set
#
# Processor Type
#
CONFIG_CPU_V7=y
CONFIG_CPU_32v6K=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
# CONFIG_ARM_LPAE is not set
# CONFIG_ARCH_PHYS_ADDR_T_64BIT is not set
CONFIG_ARM_THUMB=y
CONFIG_ARM_THUMBEE=y
# CONFIG_ARM_VIRT_EXT is not set
CONFIG_SWP_EMULATE=y
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
# CONFIG_CACHE_L2X0 is not set
CONFIG_ARM_L1_CACHE_SHIFT_6=y
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_DMA_MEM_BUFFERABLE=y
CONFIG_ARM_NR_BANKS=8
CONFIG_MULTI_IRQ_HANDLER=y
CONFIG_ARM_ERRATA_430973=y
# CONFIG_ARM_ERRATA_458693 is not set
# CONFIG_ARM_ERRATA_460075 is not set
CONFIG_ARM_ERRATA_720789=y
# CONFIG_ARM_ERRATA_743622 is not set
# CONFIG_ARM_ERRATA_751472 is not set
# CONFIG_ARM_ERRATA_754322 is not set
# CONFIG_ARM_ERRATA_775420 is not set
CONFIG_TI_PRIV_EDMA=y
#
# Bus support
#
# CONFIG_PCI_SYSCALL is not set
# CONFIG_PCCARD is not set
#
# Kernel Features
#
# CONFIG_ARM_ARCH_TIMER is not set
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_ARCH_NR_GPIO=0
# CONFIG_PREEMPT_NONE is not set
CONFIG_PREEMPT_VOLUNTARY=y
# CONFIG_PREEMPT is not set
CONFIG_HZ=512
CONFIG_THUMB2_KERNEL=y
CONFIG_ARM_ASM_UNIFIED=y
CONFIG_AEABI=y
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
CONFIG_HAVE_ARCH_PFN_VALID=y
CONFIG_HIGHMEM=y
# CONFIG_HIGHPTE is not set
CONFIG_HW_PERF_EVENTS=y
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_HAVE_MEMBLOCK=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=999999
# CONFIG_COMPACTION is not set
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_BOUNCE=y
CONFIG_VIRT_TO_BUS=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
CONFIG_CROSS_MEMORY_ATTACH=y
CONFIG_NEED_PER_CPU_KM=y
# CONFIG_CLEANCACHE is not set
# CONFIG_FRONTSWAP is not set
CONFIG_FORCE_MAX_ZONEORDER=12
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
# CONFIG_SECCOMP is not set
# CONFIG_CC_STACKPROTECTOR is not set
# CONFIG_XEN is not set
#
# Boot options
#
CONFIG_USE_OF=y
CONFIG_ATAGS=y
# CONFIG_DEPRECATED_PARAM_STRUCT is not set
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
CONFIG_ARM_APPENDED_DTB=y
CONFIG_ARM_ATAG_DTB_COMPAT=y
CONFIG_ARM_ATAG_DTB_COMPAT_CMDLINE_FROM_BOOTLOADER=y
# CONFIG_ARM_ATAG_DTB_COMPAT_CMDLINE_EXTEND is not set
CONFIG_CMDLINE=" debug "
CONFIG_CMDLINE_FROM_BOOTLOADER=y
# CONFIG_CMDLINE_EXTEND is not set
# CONFIG_CMDLINE_FORCE is not set
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
# CONFIG_CRASH_DUMP is not set
# CONFIG_AUTO_ZRELADDR is not set
#
# CPU Power Management
#
#
# CPU Frequency scaling
#
# CONFIG_CPU_FREQ is not set
# CONFIG_CPU_IDLE is not set
# CONFIG_ARCH_NEEDS_CPU_IDLE_COUPLED is not set
#
# Floating point emulation
#
#
# At least one emulation must be selected
#
CONFIG_VFP=y
CONFIG_VFPv3=y
CONFIG_NEON=y
#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
CONFIG_ARCH_BINFMT_ELF_RANDOMIZE_PIE=y
CONFIG_HAVE_AOUT=y
# CONFIG_BINFMT_AOUT is not set
CONFIG_BINFMT_MISC=y
# CONFIG_COREDUMP is not set
#
# Power management options
#
# CONFIG_SUSPEND is not set
CONFIG_PM_RUNTIME=y
CONFIG_PM=y
# CONFIG_PM_DEBUG is not set
# CONFIG_APM_EMULATION is not set
CONFIG_ARCH_HAS_OPP=y
CONFIG_PM_OPP=y
CONFIG_PM_CLK=y
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_ARM_CPU_SUSPEND=y
CONFIG_NET=y
#
# Networking options
#
CONFIG_PACKET=y
# CONFIG_PACKET_DIAG is not set
CONFIG_UNIX=y
# CONFIG_UNIX_DIAG is not set
CONFIG_XFRM=y
CONFIG_XFRM_ALGO=y
CONFIG_XFRM_USER=y
# CONFIG_XFRM_SUB_POLICY is not set
CONFIG_XFRM_MIGRATE=y
# CONFIG_XFRM_STATISTICS is not set
CONFIG_NET_KEY=y
CONFIG_NET_KEY_MIGRATE=y
CONFIG_INET=y
# CONFIG_IP_MULTICAST is not set
# CONFIG_IP_ADVANCED_ROUTER is not set
CONFIG_IP_PNP=y
CONFIG_IP_PNP_DHCP=y
# CONFIG_IP_PNP_BOOTP is not set
# CONFIG_IP_PNP_RARP is not set
# CONFIG_NET_IPIP is not set
# CONFIG_NET_IPGRE_DEMUX is not set
# CONFIG_ARPD is not set
# CONFIG_SYN_COOKIES is not set
# CONFIG_INET_AH is not set
# CONFIG_INET_ESP is not set
# CONFIG_INET_IPCOMP is not set
# CONFIG_INET_XFRM_TUNNEL is not set
# CONFIG_INET_TUNNEL is not set
# CONFIG_INET_XFRM_MODE_TRANSPORT is not set
# CONFIG_INET_XFRM_MODE_TUNNEL is not set
# CONFIG_INET_XFRM_MODE_BEET is not set
# CONFIG_INET_LRO is not set
CONFIG_INET_DIAG=y
CONFIG_INET_TCP_DIAG=y
# CONFIG_INET_UDP_DIAG is not set
# CONFIG_TCP_CONG_ADVANCED is not set
CONFIG_TCP_CONG_CUBIC=y
CONFIG_DEFAULT_TCP_CONG="cubic"
# CONFIG_TCP_MD5SIG is not set
# CONFIG_IPV6 is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
# CONFIG_NETFILTER is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IP_SCTP is not set
# CONFIG_RDS is not set
# CONFIG_TIPC is not set
# CONFIG_ATM is not set
# CONFIG_L2TP is not set
# CONFIG_BRIDGE is not set
CONFIG_HAVE_NET_DSA=y
# CONFIG_VLAN_8021Q is not set
# CONFIG_DECNET is not set
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_WAN_ROUTER is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set
CONFIG_DNS_RESOLVER=y
# CONFIG_BATMAN_ADV is not set
# CONFIG_OPENVSWITCH is not set
# CONFIG_NETPRIO_CGROUP is not set
CONFIG_BQL=y
#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
# CONFIG_WIRELESS is not set
# CONFIG_WIMAX is not set
# CONFIG_RFKILL is not set
# CONFIG_RFKILL_REGULATOR is not set
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
# CONFIG_NFC is not set
CONFIG_HAVE_BPF_JIT=y
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH=""
CONFIG_DEVTMPFS=y
CONFIG_DEVTMPFS_MOUNT=y
CONFIG_STANDALONE=y
# CONFIG_PREVENT_FIRMWARE_BUILD is not set
CONFIG_FW_LOADER=y
CONFIG_FIRMWARE_IN_KERNEL=y
CONFIG_EXTRA_FIRMWARE="am335x-pm-firmware.bin"
CONFIG_EXTRA_FIRMWARE_DIR="firmware"
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_GENERIC_CPU_DEVICES is not set
CONFIG_REGMAP=y
CONFIG_REGMAP_I2C=y
# CONFIG_DMA_SHARED_BUFFER is not set
# CONFIG_CMA is not set
#
# Bus devices
#
CONFIG_OMAP_OCP2SCP=y
CONFIG_OMAP_INTERCONNECT=y
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_REDBOOT_PARTS is not set
CONFIG_MTD_CMDLINE_PARTS=y
# CONFIG_MTD_AFS_PARTS is not set
CONFIG_MTD_OF_PARTS=y
# CONFIG_MTD_AR7_PARTS is not set
#
# User Modules And Translation Layers
#
CONFIG_MTD_CHAR=y
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_SM_FTL is not set
# CONFIG_MTD_OOPS is not set
# CONFIG_MTD_SWAP is not set
#
# RAM/ROM/Flash chip drivers
#
CONFIG_MTD_CFI=y
# CONFIG_MTD_JEDECPROBE is not set
CONFIG_MTD_GEN_PROBE=y
# CONFIG_MTD_CFI_ADV_OPTIONS is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
CONFIG_MTD_CFI_INTELEXT=y
# CONFIG_MTD_CFI_AMDSTD is not set
# CONFIG_MTD_CFI_STAA is not set
CONFIG_MTD_CFI_UTIL=y
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set
#
# Mapping drivers for chip access
#
# CONFIG_MTD_COMPLEX_MAPPINGS is not set
# CONFIG_MTD_PHYSMAP is not set
# CONFIG_MTD_PHYSMAP_OF is not set
# CONFIG_MTD_PLATRAM is not set
#
# Self-contained MTD device drivers
#
# CONFIG_MTD_DATAFLASH is not set
CONFIG_MTD_M25P80=y
CONFIG_M25PXX_USE_FAST_READ=y
# CONFIG_MTD_SST25L is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set
#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOCG3 is not set
# CONFIG_MTD_NAND is not set
# CONFIG_MTD_ONENAND is not set
#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set
# CONFIG_MTD_UBI is not set
CONFIG_DTC=y
CONFIG_OF=y
#
# Device Tree and Open Firmware support
#
CONFIG_PROC_DEVICETREE=y
# CONFIG_OF_SELFTEST is not set
CONFIG_OF_FLATTREE=y
CONFIG_OF_EARLY_FLATTREE=y
CONFIG_OF_DYNAMIC=y
CONFIG_OF_ADDRESS=y
CONFIG_OF_IRQ=y
CONFIG_OF_DEVICE=y
CONFIG_OF_I2C=y
CONFIG_OF_NET=y
CONFIG_OF_MDIO=y
CONFIG_OF_MTD=y
CONFIG_OF_RESOLVE=y
CONFIG_OF_OVERLAY=y
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
CONFIG_BLK_DEV_LOOP_MIN_COUNT=8
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
# CONFIG_BLK_DEV_DRBD is not set
# CONFIG_BLK_DEV_NBD is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=16384
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
# CONFIG_BLK_DEV_RBD is not set
#
# Misc devices
#
# CONFIG_SENSORS_LIS3LV02D is not set
# CONFIG_AD525X_DPOT is not set
# CONFIG_ATMEL_PWM is not set
# CONFIG_ICS932S401 is not set
# CONFIG_ENCLOSURE_SERVICES is not set
# CONFIG_APDS9802ALS is not set
# CONFIG_ISL29003 is not set
# CONFIG_ISL29020 is not set
# CONFIG_SENSORS_TSL2550 is not set
# CONFIG_SENSORS_BH1780 is not set
# CONFIG_SENSORS_BH1770 is not set
# CONFIG_SENSORS_APDS990X is not set
# CONFIG_HMC6352 is not set
# CONFIG_DS1682 is not set
# CONFIG_TI_DAC7512 is not set
# CONFIG_BMP085_I2C is not set
# CONFIG_BMP085_SPI is not set
# CONFIG_USB_SWITCH_FSA9480 is not set
# CONFIG_GPEVT is not set
# CONFIG_GROVE_I2C is not set
# CONFIG_C2PORT is not set
#
# EEPROM support
#
CONFIG_EEPROM_AT24=y
# CONFIG_EEPROM_AT25 is not set
# CONFIG_EEPROM_LEGACY is not set
# CONFIG_EEPROM_MAX6875 is not set
CONFIG_EEPROM_93CX6=y
# CONFIG_EEPROM_93XX46 is not set
#
# Texas Instruments shared transport line discipline
#
# CONFIG_TI_ST is not set
# CONFIG_SENSORS_LIS3_SPI is not set
# CONFIG_SENSORS_LIS3_I2C is not set
#
# Altera FPGA firmware download module
#
# CONFIG_ALTERA_STAPL is not set
CONFIG_BEAGLEBONE_PINMUX_HELPER=y
CONFIG_CAPE_BEAGLEBONE=y
# CONFIG_CAPE_BEAGLEBONE_GEIGER is not set
# CONFIG_CAPE_BEAGLEBONE_NIXIE is not set
#
# SCSI device support
#
CONFIG_SCSI_MOD=y
# CONFIG_RAID_ATTRS is not set
# CONFIG_SCSI is not set
# CONFIG_SCSI_DMA is not set
# CONFIG_SCSI_NETLINK is not set
# CONFIG_ATA is not set
# CONFIG_MD is not set
CONFIG_NETDEVICES=y
CONFIG_NET_CORE=y
# CONFIG_BONDING is not set
# CONFIG_DUMMY is not set
# CONFIG_EQUALIZER is not set
CONFIG_MII=y
# CONFIG_NET_TEAM is not set
# CONFIG_MACVLAN is not set
# CONFIG_VXLAN is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
# CONFIG_TUN is not set
# CONFIG_VETH is not set
#
# CAIF transport drivers
#
#
# Distributed Switch Architecture drivers
#
# CONFIG_NET_DSA_MV88E6XXX is not set
# CONFIG_NET_DSA_MV88E6060 is not set
# CONFIG_NET_DSA_MV88E6XXX_NEED_PPU is not set
# CONFIG_NET_DSA_MV88E6131 is not set
# CONFIG_NET_DSA_MV88E6123_61_65 is not set
CONFIG_ETHERNET=y
# CONFIG_NET_CADENCE is not set
# CONFIG_NET_VENDOR_BROADCOM is not set
# CONFIG_NET_CALXEDA_XGMAC is not set
# CONFIG_NET_VENDOR_CIRRUS is not set
# CONFIG_DM9000 is not set
# CONFIG_DNET is not set
# CONFIG_NET_VENDOR_FARADAY is not set
# CONFIG_NET_VENDOR_INTEL is not set
# CONFIG_NET_VENDOR_MARVELL is not set
# CONFIG_NET_VENDOR_MICREL is not set
# CONFIG_NET_VENDOR_MICROCHIP is not set
# CONFIG_NET_VENDOR_NATSEMI is not set
# CONFIG_ETHOC is not set
# CONFIG_NET_VENDOR_SEEQ is not set
# CONFIG_NET_VENDOR_SMSC is not set
# CONFIG_NET_VENDOR_STMICRO is not set
CONFIG_NET_VENDOR_TI=y
CONFIG_TI_DAVINCI_EMAC=y
CONFIG_TI_DAVINCI_MDIO=y
CONFIG_TI_DAVINCI_CPDMA=y
CONFIG_TI_CPSW=y
# CONFIG_TI_CPTS is not set
# CONFIG_NET_VENDOR_WIZNET is not set
CONFIG_PHYLIB=y
#
# MII PHY device drivers
#
# CONFIG_AT803X_PHY is not set
# CONFIG_AMD_PHY is not set
# CONFIG_MARVELL_PHY is not set
# CONFIG_DAVICOM_PHY is not set
# CONFIG_QSEMI_PHY is not set
# CONFIG_LXT_PHY is not set
# CONFIG_CICADA_PHY is not set
# CONFIG_VITESSE_PHY is not set
CONFIG_SMSC_PHY=y
# CONFIG_BROADCOM_PHY is not set
# CONFIG_BCM87XX_PHY is not set
# CONFIG_ICPLUS_PHY is not set
# CONFIG_REALTEK_PHY is not set
# CONFIG_NATIONAL_PHY is not set
# CONFIG_STE10XP is not set
# CONFIG_LSI_ET1011C_PHY is not set
# CONFIG_MICREL_PHY is not set
# CONFIG_FIXED_PHY is not set
# CONFIG_MDIO_BITBANG is not set
# CONFIG_MDIO_BUS_MUX_GPIO is not set
# CONFIG_MDIO_BUS_MUX_MMIOREG is not set
# CONFIG_MICREL_KS8995MA is not set
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
# CONFIG_WLAN is not set
#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
# CONFIG_WAN is not set
# CONFIG_ISDN is not set
#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
# CONFIG_INPUT_POLLDEV is not set
# CONFIG_INPUT_SPARSEKMAP is not set
# CONFIG_INPUT_MATRIXKMAP is not set
#
# Userland interfaces
#
# CONFIG_INPUT_MOUSEDEV is not set
# CONFIG_INPUT_JOYDEV is not set
# CONFIG_INPUT_EVDEV is not set
# CONFIG_INPUT_EVBUG is not set
#
# Input Device Drivers
#
# CONFIG_INPUT_KEYBOARD is not set
# CONFIG_INPUT_MOUSE is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
# CONFIG_INPUT_TOUCHSCREEN is not set
# CONFIG_INPUT_MISC is not set
#
# Hardware I/O ports
#
# CONFIG_SERIO is not set
# CONFIG_GAMEPORT is not set
#
# Character devices
#
CONFIG_VT=y
CONFIG_CONSOLE_TRANSLATIONS=y
CONFIG_VT_CONSOLE=y
CONFIG_HW_CONSOLE=y
CONFIG_VT_HW_CONSOLE_BINDING=y
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
# CONFIG_LEGACY_PTYS is not set
# CONFIG_JHD629_I2C is not set
# CONFIG_SERIAL_NONSTANDARD is not set
# CONFIG_N_GSM is not set
# CONFIG_TRACE_SINK is not set
# CONFIG_DEVKMEM is not set
#
# Serial drivers
#
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_NR_UARTS=32
CONFIG_SERIAL_8250_RUNTIME_UARTS=4
CONFIG_SERIAL_8250_EXTENDED=y
CONFIG_SERIAL_8250_MANY_PORTS=y
CONFIG_SERIAL_8250_SHARE_IRQ=y
CONFIG_SERIAL_8250_DETECT_IRQ=y
CONFIG_SERIAL_8250_RSA=y
# CONFIG_SERIAL_8250_DW is not set
# CONFIG_SERIAL_8250_EM is not set
#
# Non-8250 serial port support
#
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_MAX310X is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
# CONFIG_SERIAL_OF_PLATFORM is not set
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
# CONFIG_SERIAL_SCCNXP is not set
# CONFIG_SERIAL_TIMBERDALE is not set
# CONFIG_SERIAL_ALTERA_JTAGUART is not set
# CONFIG_SERIAL_ALTERA_UART is not set
# CONFIG_SERIAL_IFX6X60 is not set
# CONFIG_SERIAL_XILINX_PS_UART is not set
# CONFIG_SERIAL_ARC is not set
# CONFIG_TTY_PRINTK is not set
# CONFIG_HVC_DCC is not set
# CONFIG_IPMI_HANDLER is not set
# CONFIG_HW_RANDOM is not set
# CONFIG_R3964 is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
CONFIG_I2C_COMPAT=y
CONFIG_I2C_CHARDEV=y
CONFIG_I2C_MUX=y
#
# Multiplexer I2C Chip support
#
CONFIG_I2C_MUX_GPIO=y
CONFIG_I2C_MUX_PCA9541=y
CONFIG_I2C_MUX_PCA954x=y
# CONFIG_I2C_MUX_PINCTRL is not set
CONFIG_I2C_HELPER_AUTO=y
#
# I2C Hardware Bus support
#
#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_CBUS_GPIO is not set
# CONFIG_I2C_DESIGNWARE_PLATFORM is not set
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_OCORES is not set
CONFIG_I2C_OMAP=y
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_PXA_PCI is not set
# CONFIG_I2C_SIMTEC is not set
# CONFIG_I2C_XILINX is not set
#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set
#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
#
# SPI Master Controller Drivers
#
# CONFIG_SPI_ALTERA is not set
# CONFIG_SPI_BITBANG is not set
# CONFIG_SPI_GPIO is not set
# CONFIG_SPI_OC_TINY is not set
CONFIG_SPI_OMAP24XX=y
# CONFIG_SPI_PXA2XX_PCI is not set
# CONFIG_SPI_SC18IS602 is not set
# CONFIG_SPI_XCOMM is not set
# CONFIG_SPI_XILINX is not set
# CONFIG_SPI_DESIGNWARE is not set
#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
# CONFIG_HSI is not set
#
# PPS support
#
# CONFIG_PPS is not set
#
# PPS generators support
#
#
# PTP clock support
#
# CONFIG_PTP_1588_CLOCK is not set
#
# Enable PHYLIB and NETWORK_PHY_TIMESTAMPING to see the additional clocks.
#
# CONFIG_PTP_1588_CLOCK_PCH is not set
CONFIG_PINCTRL=y
#
# Pin controllers
#
CONFIG_PINMUX=y
CONFIG_PINCONF=y
# CONFIG_DEBUG_PINCTRL is not set
CONFIG_PINCTRL_SINGLE=y
# CONFIG_PINCTRL_EXYNOS is not set
# CONFIG_PINCTRL_EXYNOS5440 is not set
CONFIG_ARCH_HAVE_CUSTOM_GPIO_H=y
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIOLIB=y
CONFIG_OF_GPIO=y
CONFIG_DEBUG_GPIO=y
CONFIG_GPIO_SYSFS=y
CONFIG_GPIO_OF_HELPER=y
#
# Memory mapped GPIO drivers:
#
# CONFIG_GPIO_GENERIC_PLATFORM is not set
# CONFIG_GPIO_EM is not set
# CONFIG_GPIO_TS5500 is not set
#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX7300 is not set
# CONFIG_GPIO_MAX732X is not set
CONFIG_GPIO_PCA953X_IRQ=y
CONFIG_GPIO_PCF857X=y
# CONFIG_GPIO_SX150X is not set
# CONFIG_GPIO_TWL4030 is not set
# CONFIG_GPIO_ADP5588 is not set
# CONFIG_GPIO_ADNP is not set
#
# PCI GPIO expanders:
#
#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_GPIO_MC33880 is not set
# CONFIG_GPIO_74X164 is not set
#
# AC97 GPIO expanders:
#
#
# MODULbus GPIO expanders:
#
#
# USB GPIO expanders:
#
# CONFIG_W1 is not set
# CONFIG_POWER_SUPPLY is not set
# CONFIG_POWER_AVS is not set
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
# CONFIG_WATCHDOG is not set
CONFIG_SSB_POSSIBLE=y
#
# Sonics Silicon Backplane
#
# CONFIG_SSB is not set
CONFIG_BCMA_POSSIBLE=y
#
# Broadcom specific AMBA
#
# CONFIG_BCMA is not set
#
# Multifunction device drivers
#
# CONFIG_MFD_CORE is not set
# CONFIG_MFD_88PM860X is not set
# CONFIG_MFD_88PM800 is not set
# CONFIG_MFD_88PM805 is not set
# CONFIG_MFD_SM501 is not set
# CONFIG_MFD_ASIC3 is not set
# CONFIG_MFD_TI_AM335X_TSCADC is not set
# CONFIG_HTC_EGPIO is not set
# CONFIG_HTC_PASIC3 is not set
# CONFIG_HTC_I2CPLD is not set
# CONFIG_MFD_LM3533 is not set
# CONFIG_TPS6105X is not set
# CONFIG_TPS65010 is not set
# CONFIG_TPS6507X is not set
# CONFIG_MFD_TPS65217 is not set
# CONFIG_MFD_TPS6586X is not set
# CONFIG_MFD_TPS65910 is not set
# CONFIG_MFD_TPS65912_I2C is not set
# CONFIG_MFD_TPS65912_SPI is not set
# CONFIG_MFD_TPS80031 is not set
CONFIG_TWL4030_CORE=y
# CONFIG_TWL4030_MADC is not set
CONFIG_TWL4030_POWER=y
# CONFIG_MFD_TWL4030_AUDIO is not set
# CONFIG_TWL6040_CORE is not set
# CONFIG_MFD_STMPE is not set
# CONFIG_MFD_TC3589X is not set
# CONFIG_MFD_TMIO is not set
# CONFIG_MFD_T7L66XB is not set
# CONFIG_MFD_SMSC is not set
# CONFIG_MFD_TC6387XB is not set
# CONFIG_MFD_TC6393XB is not set
# CONFIG_PMIC_DA903X is not set
# CONFIG_MFD_DA9052_SPI is not set
# CONFIG_MFD_DA9052_I2C is not set
# CONFIG_MFD_DA9055 is not set
# CONFIG_PMIC_ADP5520 is not set
# CONFIG_MFD_LP8788 is not set
# CONFIG_MFD_MAX77686 is not set
# CONFIG_MFD_MAX77693 is not set
# CONFIG_MFD_MAX8907 is not set
# CONFIG_MFD_MAX8925 is not set
# CONFIG_MFD_MAX8997 is not set
# CONFIG_MFD_MAX8998 is not set
# CONFIG_MFD_SEC_CORE is not set
# CONFIG_MFD_ARIZONA_I2C is not set
# CONFIG_MFD_ARIZONA_SPI is not set
# CONFIG_MFD_WM8400 is not set
# CONFIG_MFD_WM831X_I2C is not set
# CONFIG_MFD_WM831X_SPI is not set
# CONFIG_MFD_WM8350_I2C is not set
# CONFIG_MFD_WM8994 is not set
# CONFIG_MFD_PCF50633 is not set
# CONFIG_MFD_MC13XXX_SPI is not set
# CONFIG_MFD_MC13XXX_I2C is not set
# CONFIG_ABX500_CORE is not set
# CONFIG_EZX_PCAP is not set
# CONFIG_MFD_WL1273_CORE is not set
# CONFIG_MFD_TPS65090 is not set
# CONFIG_MFD_AAT2870_CORE is not set
# CONFIG_MFD_RC5T583 is not set
# CONFIG_MFD_SYSCON is not set
# CONFIG_MFD_PALMAS is not set
# CONFIG_MFD_RETU is not set
# CONFIG_MFD_AS3711 is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
CONFIG_REGULATOR_DUMMY=y
CONFIG_REGULATOR_FIXED_VOLTAGE=y
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
CONFIG_REGULATOR_GPIO=y
# CONFIG_REGULATOR_AD5398 is not set
# CONFIG_REGULATOR_FAN53555 is not set
# CONFIG_REGULATOR_ISL6271A is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_MAX8649 is not set
# CONFIG_REGULATOR_MAX8660 is not set
# CONFIG_REGULATOR_MAX8952 is not set
# CONFIG_REGULATOR_MAX8973 is not set
# CONFIG_REGULATOR_LP3971 is not set
# CONFIG_REGULATOR_LP3972 is not set
# CONFIG_REGULATOR_LP872X is not set
# CONFIG_REGULATOR_TPS51632 is not set
# CONFIG_REGULATOR_TPS62360 is not set
CONFIG_REGULATOR_TPS65023=y
CONFIG_REGULATOR_TPS6507X=y
# CONFIG_REGULATOR_TPS6524X is not set
CONFIG_REGULATOR_TWL4030=y
# CONFIG_MEDIA_SUPPORT is not set
#
# Graphics support
#
# CONFIG_DRM is not set
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
# CONFIG_OF_DISPLAY_TIMING is not set
# CONFIG_OF_VIDEOMODE is not set
# CONFIG_FB is not set
# CONFIG_OMAP2_DSS is not set
# CONFIG_EXYNOS_VIDEO is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set
#
# Console display driver support
#
CONFIG_DUMMY_CONSOLE=y
# CONFIG_SOUND is not set
#
# HID support
#
CONFIG_HID=y
# CONFIG_HIDRAW is not set
# CONFIG_UHID is not set
CONFIG_HID_GENERIC=y
#
# Special HID drivers
#
#
# I2C HID support
#
# CONFIG_I2C_HID is not set
CONFIG_USB_ARCH_HAS_OHCI=y
CONFIG_USB_ARCH_HAS_EHCI=y
# CONFIG_USB_ARCH_HAS_XHCI is not set
# CONFIG_USB_SUPPORT is not set
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
CONFIG_MMC_UNSAFE_RESUME=y
# CONFIG_MMC_CLKGATE is not set
#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_MINORS=8
CONFIG_MMC_BLOCK_BOUNCE=y
CONFIG_SDIO_UART=y
# CONFIG_MMC_TEST is not set
#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_SDHCI_PXAV3 is not set
# CONFIG_MMC_SDHCI_PXAV2 is not set
CONFIG_MMC_OMAP=y
CONFIG_MMC_OMAP_HS=y
# CONFIG_MMC_DW is not set
# CONFIG_MEMSTICK is not set
# CONFIG_NEW_LEDS is not set
# CONFIG_ACCESSIBILITY is not set
# CONFIG_EDAC is not set
CONFIG_RTC_LIB=y
# CONFIG_RTC_CLASS is not set
CONFIG_DMADEVICES=y
# CONFIG_DMADEVICES_DEBUG is not set
#
# DMA Devices
#
# CONFIG_DW_DMAC is not set
# CONFIG_TIMB_DMA is not set
CONFIG_TI_EDMA=y
# CONFIG_DMA_OMAP is not set
CONFIG_DMA_ENGINE=y
CONFIG_DMA_VIRTUAL_CHANNELS=y
#
# DMA Clients
#
# CONFIG_NET_DMA is not set
# CONFIG_ASYNC_TX_DMA is not set
# CONFIG_DMATEST is not set
# CONFIG_AUXDISPLAY is not set
# CONFIG_UIO is not set
#
# Virtio drivers
#
# CONFIG_VIRTIO_MMIO is not set
#
# Microsoft Hyper-V guest support
#
# CONFIG_STAGING is not set
CONFIG_CLKDEV_LOOKUP=y
CONFIG_HAVE_CLK_PREPARE=y
CONFIG_COMMON_CLK=y
#
# Common Clock Framework
#
# CONFIG_COMMON_CLK_DEBUG is not set
#
# Hardware Spinlock drivers
#
CONFIG_CLKSRC_MMIO=y
CONFIG_IOMMU_SUPPORT=y
CONFIG_OF_IOMMU=y
# CONFIG_OMAP_IOMMU is not set
#
# Remoteproc drivers (EXPERIMENTAL)
#
# CONFIG_STE_MODEM_RPROC is not set
# CONFIG_PRU_RPROC is not set
#
# Rpmsg drivers (EXPERIMENTAL)
#
# CONFIG_VIRT_DRIVERS is not set
# CONFIG_PM_DEVFREQ is not set
# CONFIG_EXTCON is not set
# CONFIG_MEMORY is not set
# CONFIG_IIO is not set
# CONFIG_PWM is not set
# CONFIG_IPACK_BUS is not set
CONFIG_RSTCTL=y
CONFIG_RSTCTL_GPIO=y
CONFIG_RSTCTL_TEST=y
CONFIG_RSTCTL_TEST_CONSUMER=y
#
# File systems
#
CONFIG_DCACHE_WORD_ACCESS=y
# CONFIG_EXT2_FS is not set
# CONFIG_EXT3_FS is not set
CONFIG_EXT4_FS=y
CONFIG_EXT4_USE_FOR_EXT23=y
# CONFIG_EXT4_FS_POSIX_ACL is not set
# CONFIG_EXT4_FS_SECURITY is not set
# CONFIG_EXT4_DEBUG is not set
CONFIG_JBD2=y
# CONFIG_JBD2_DEBUG is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
# CONFIG_XFS_FS is not set
# CONFIG_GFS2_FS is not set
# CONFIG_BTRFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_FS_POSIX_ACL=y
CONFIG_FILE_LOCKING=y
CONFIG_FSNOTIFY=y
CONFIG_DNOTIFY=y
CONFIG_INOTIFY_USER=y
CONFIG_FANOTIFY=y
CONFIG_QUOTA=y
# CONFIG_QUOTA_NETLINK_INTERFACE is not set
CONFIG_PRINT_QUOTA_WARNING=y
# CONFIG_QUOTA_DEBUG is not set
CONFIG_QUOTA_TREE=y
# CONFIG_QFMT_V1 is not set
CONFIG_QFMT_V2=y
CONFIG_QUOTACTL=y
# CONFIG_AUTOFS4_FS is not set
# CONFIG_FUSE_FS is not set
CONFIG_GENERIC_ACL=y
#
# Caches
#
# CONFIG_FSCACHE is not set
#
# CD-ROM/DVD Filesystems
#
# CONFIG_ISO9660_FS is not set
# CONFIG_UDF_FS is not set
#
# DOS/FAT/NT Filesystems
#
CONFIG_FAT_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_FAT_DEFAULT_CODEPAGE=437
CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
# CONFIG_NTFS_FS is not set
#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
CONFIG_TMPFS_POSIX_ACL=y
CONFIG_TMPFS_XATTR=y
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_ECRYPT_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
# CONFIG_JFFS2_FS is not set
# CONFIG_LOGFS is not set
# CONFIG_CRAMFS is not set
# CONFIG_SQUASHFS is not set
# CONFIG_VXFS_FS is not set
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_QNX6FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_PSTORE is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
CONFIG_F2FS_FS=y
CONFIG_F2FS_STAT_FS=y
CONFIG_F2FS_FS_XATTR=y
CONFIG_F2FS_FS_POSIX_ACL=y
# CONFIG_NETWORK_FILESYSTEMS is not set
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="iso8859-1"
CONFIG_NLS_CODEPAGE_437=y
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
# CONFIG_NLS_ASCII is not set
CONFIG_NLS_ISO8859_1=y
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
# CONFIG_NLS_MAC_ROMAN is not set
# CONFIG_NLS_MAC_CELTIC is not set
# CONFIG_NLS_MAC_CENTEURO is not set
# CONFIG_NLS_MAC_CROATIAN is not set
# CONFIG_NLS_MAC_CYRILLIC is not set
# CONFIG_NLS_MAC_GAELIC is not set
# CONFIG_NLS_MAC_GREEK is not set
# CONFIG_NLS_MAC_ICELAND is not set
# CONFIG_NLS_MAC_INUIT is not set
# CONFIG_NLS_MAC_ROMANIAN is not set
# CONFIG_NLS_MAC_TURKISH is not set
# CONFIG_NLS_UTF8 is not set
#
# Kernel hacking
#
CONFIG_PRINTK_TIME=y
CONFIG_DEFAULT_MESSAGE_LOGLEVEL=4
CONFIG_ENABLE_WARN_DEPRECATED=y
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
CONFIG_MAGIC_SYSRQ=y
# CONFIG_STRIP_ASM_SYMS is not set
# CONFIG_READABLE_ASM is not set
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
# CONFIG_DEBUG_SECTION_MISMATCH is not set
CONFIG_DEBUG_KERNEL=y
# CONFIG_DEBUG_SHIRQ is not set
CONFIG_LOCKUP_DETECTOR=y
CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC=y
CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC_VALUE=1
# CONFIG_PANIC_ON_OOPS is not set
CONFIG_PANIC_ON_OOPS_VALUE=0
CONFIG_DETECT_HUNG_TASK=y
CONFIG_DEFAULT_HUNG_TASK_TIMEOUT=60
CONFIG_BOOTPARAM_HUNG_TASK_PANIC=y
CONFIG_BOOTPARAM_HUNG_TASK_PANIC_VALUE=1
CONFIG_SCHED_DEBUG=y
CONFIG_SCHEDSTATS=y
CONFIG_TIMER_STATS=y
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_DEBUG_SLAB is not set
CONFIG_HAVE_DEBUG_KMEMLEAK=y
# CONFIG_DEBUG_KMEMLEAK is not set
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
CONFIG_DEBUG_SPINLOCK=y
CONFIG_DEBUG_MUTEXES=y
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_SPARSE_RCU_POINTER is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_ATOMIC_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
# CONFIG_DEBUG_STACK_USAGE is not set
# CONFIG_DEBUG_KOBJECT is not set
# CONFIG_DEBUG_HIGHMEM is not set
CONFIG_DEBUG_BUGVERBOSE=y
# CONFIG_DEBUG_INFO is not set
# CONFIG_DEBUG_VM is not set
# CONFIG_DEBUG_WRITECOUNT is not set
# CONFIG_DEBUG_MEMORY_INIT is not set
# CONFIG_DEBUG_LIST is not set
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_DEBUG_CREDENTIALS is not set
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_RCU_TRACE is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# CONFIG_LKDTM is not set
# CONFIG_NOTIFIER_ERROR_INJECTION is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
# CONFIG_DEBUG_PAGEALLOC is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
CONFIG_HAVE_SYSCALL_TRACEPOINTS=y
CONFIG_HAVE_C_RECORDMCOUNT=y
CONFIG_TRACING_SUPPORT=y
CONFIG_FTRACE=y
# CONFIG_FUNCTION_TRACER is not set
# CONFIG_IRQSOFF_TRACER is not set
# CONFIG_SCHED_TRACER is not set
# CONFIG_ENABLE_DEFAULT_TRACERS is not set
# CONFIG_FTRACE_SYSCALLS is not set
CONFIG_BRANCH_PROFILE_NONE=y
# CONFIG_PROFILE_ANNOTATED_BRANCHES is not set
# CONFIG_PROFILE_ALL_BRANCHES is not set
# CONFIG_STACK_TRACER is not set
# CONFIG_BLK_DEV_IO_TRACE is not set
# CONFIG_PROBE_EVENTS is not set
# CONFIG_DYNAMIC_DEBUG is not set
# CONFIG_DMA_API_DEBUG is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
# CONFIG_TEST_KSTRTOX is not set
# CONFIG_STRICT_DEVMEM is not set
CONFIG_ARM_UNWIND=y
# CONFIG_DEBUG_USER is not set
CONFIG_DEBUG_LL=y
CONFIG_DEBUG_LL_UART_NONE=y
# CONFIG_DEBUG_ICEDCC is not set
# CONFIG_DEBUG_SEMIHOSTING is not set
CONFIG_DEBUG_LL_INCLUDE="mach/debug-macro.S"
CONFIG_EARLY_PRINTK=y
# CONFIG_PID_IN_CONTEXTIDR is not set
#
# Security options
#
CONFIG_KEYS=y
# CONFIG_ENCRYPTED_KEYS is not set
# CONFIG_KEYS_DEBUG_PROC_KEYS is not set
# CONFIG_SECURITY_DMESG_RESTRICT is not set
# CONFIG_SECURITY is not set
# CONFIG_SECURITYFS is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
CONFIG_CRYPTO_ALGAPI=y
CONFIG_CRYPTO_ALGAPI2=y
CONFIG_CRYPTO_HASH=y
CONFIG_CRYPTO_HASH2=y
# CONFIG_CRYPTO_MANAGER is not set
# CONFIG_CRYPTO_MANAGER2 is not set
# CONFIG_CRYPTO_USER is not set
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set
#
# Block modes
#
# CONFIG_CRYPTO_CBC is not set
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
# CONFIG_CRYPTO_ECB is not set
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set
#
# Hash modes
#
# CONFIG_CRYPTO_HMAC is not set
# CONFIG_CRYPTO_XCBC is not set
# CONFIG_CRYPTO_VMAC is not set
#
# Digest
#
CONFIG_CRYPTO_CRC32C=y
# CONFIG_CRYPTO_GHASH is not set
# CONFIG_CRYPTO_MD4 is not set
# CONFIG_CRYPTO_MD5 is not set
# CONFIG_CRYPTO_MICHAEL_MIC is not set
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
# CONFIG_CRYPTO_SHA1 is not set
# CONFIG_CRYPTO_SHA1_ARM is not set
# CONFIG_CRYPTO_SHA256 is not set
# CONFIG_CRYPTO_SHA512 is not set
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set
#
# Ciphers
#
CONFIG_CRYPTO_AES=y
# CONFIG_CRYPTO_AES_ARM is not set
# CONFIG_CRYPTO_ANUBIS is not set
# CONFIG_CRYPTO_ARC4 is not set
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
# CONFIG_CRYPTO_DES is not set
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set
#
# Compression
#
# CONFIG_CRYPTO_DEFLATE is not set
# CONFIG_CRYPTO_ZLIB is not set
# CONFIG_CRYPTO_LZO is not set
#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
# CONFIG_CRYPTO_USER_API_HASH is not set
# CONFIG_CRYPTO_USER_API_SKCIPHER is not set
# CONFIG_CRYPTO_HW is not set
# CONFIG_ASYMMETRIC_KEY_TYPE is not set
# CONFIG_BINARY_PRINTF is not set
#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_STRNCPY_FROM_USER=y
CONFIG_GENERIC_STRNLEN_USER=y
CONFIG_GENERIC_PCI_IOMAP=y
CONFIG_GENERIC_IO=y
CONFIG_PERCPU_RWSEM=y
# CONFIG_CRC_CCITT is not set
CONFIG_CRC16=y
# CONFIG_CRC_T10DIF is not set
# CONFIG_CRC_ITU_T is not set
CONFIG_CRC32=y
# CONFIG_CRC32_SELFTEST is not set
CONFIG_CRC32_SLICEBY8=y
# CONFIG_CRC32_SLICEBY4 is not set
# CONFIG_CRC32_SARWATE is not set
# CONFIG_CRC32_BIT is not set
# CONFIG_CRC7 is not set
# CONFIG_LIBCRC32C is not set
# CONFIG_CRC8 is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_LZO_COMPRESS=y
CONFIG_LZO_DECOMPRESS=y
# CONFIG_XZ_DEC is not set
# CONFIG_XZ_DEC_BCJ is not set
CONFIG_DECOMPRESS_GZIP=y
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_DQL=y
CONFIG_NLATTR=y
CONFIG_ARCH_HAS_ATOMIC64_DEC_IF_POSITIVE=y
# CONFIG_AVERAGE is not set
# CONFIG_CORDIC is not set
# CONFIG_DDR is not set
What I have tried so far is serveral kernels for example: https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/latest/index_FDS.html with this .config 3.8.13 file and then do either:
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- olddefconfig
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- LOADADDR=0x80008000 uImage
OR
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- LOADADDR=0x80008000 uImage
Then answer all the questions with no or the default option. So far i have not been able to get past the "Starting kernel..." which probably means some uncompatability. Once i was able to boot further with a 4.1.6 kernel it then said "calibrating clock delay" and got stuck there before it said it couldn initilize the clock which of course makes this logical, maybe this is why it does not boot?
Does anyone have any pointers to what i should do, or try?
Regards,
Lars