This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: PRU Ethernet 10Mbps support

Part Number: AM3358

Hi,

We are using the AM335x with PRU Ethernets and are unable to get our link detected when plugged into a 10Mbps only device.  

The https://www.ti.com/product/AM3358 datasheet states the processor has  2-Port 10/100 PRU EMAC, which would suggest 10Mbps is supported 

However, the https://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components/PRU-ICSS/Linux_Drivers/PRU-ICSS_Ethernet.html website explaining the PRUs only ever mention 100Mbps. 
and looking around the forums there are some older posts for different processors using PRU Ethernet such as this https://e2e.ti.com/support/processors-group/processors/f/processors-forum/857940/am5728-pru-ethernet-10mbps-issue which states 10Mbps is not supported

can you please provide some clarity on if the 10Mbps speed (half-duplex) is supported on the AM335 and if so why the link would then not be detected? 

Thanks

Jon