This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: Get QT cross compile tool chain by Yocto but failed

Part Number: AM6548

Hi,

I've referenced this thread:

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1006420/am6548-how-to-build-the-qt-toolchain-sdk-for-am65x

And tried to get Qt cross compile tool chain by yocto build command:

MACHINE=am65xx-evm bitbake -k meta-toolchain-arago-tisdk

under downloaded SDK "ti-processor-sdk-linux-am65xx-evm-08_01_00_01".

Fetch and compile stage were fine, but failed as the following log.

Any idea or suggestion to fix this?

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:05
Sstate summary: Wanted 0 Found 0 Missed 0 Current 2100 (0% match, 100% complete)
NOTE: Executing Tasks
ERROR: meta-toolchain-arago-tisdk-1.0-r5.0 do_populate_sdk: Unable to install packages. Command '/build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/recipe-sysroot-native/usr/bin/opkg --volatile-cache -f /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/opkg.conf -t /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/temp/ipktemp/ -o /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/sdk/image/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/aarch64-linux --force_postinstall install packagegroup-arago-toolchain-tisdk-target' returned 1:
Collected errors:
* Solver encountered 1 problem(s):
* Problem 1/1:
* - nothing provides tensorflow-lite-staticdev needed by packagegroup-arago-tisdk-addons-sdk-target-1.0-r44.0.am65xx_evm
*
* Solution 1:
* - do not ask to install a package providing packagegroup-arago-toolchain-tisdk-target

* opkg_finalize_intercepts: Failed to open dir /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/temp/ipktemp//opkg-ZvZclY/opkg-intercept-IfyjCh: No such file or directory.
* rm_r: Failed to open dir /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/temp/ipktemp//opkg-ZvZclY/opkg-intercept-IfyjCh: No such file or directory.
* rm_r: Failed to open dir /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/temp/ipktemp//opkg-ZvZclY: No such file or directory.


ERROR: Logfile of failure stored in: /build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/build/arago-tmp-external-arm-glibc/work/aarch64-linux/meta-toolchain-arago-tisdk/1.0-r5.0/temp/log.do_populate_sdk.2516
ERROR: Task (/build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-arago/meta-arago-distro/recipes-core/meta/meta-toolchain-arago-tisdk.bb:do_populate_sdk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6109 tasks of which 6108 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Summary: 1 task failed:
/build/wayneshih/ti-processor-sdk-linux-am65xx-evm-08_01_00_01/yocto-build/sources/meta-arago/meta-arago-distro/recipes-core/meta/meta-toolchain-arago-tisdk.bb:do_populate_sdk
Summary: There were 6 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.