Part Number: TDA2E
Hi Sir,
1.
I have two projects and hope to use the same processor,
Two projects use different image sensor input interface, one is MIPI 2-Lane/4-lane and another one is Parallel (DVP) .
Could TDA2E support MIPI and DVP interface at the same time?
2.
Could TDA2E support USB3.0 to output Image Sensor RAW data and YUV data?
If TDA2E SDK can support UVC protocol throw USB3.0 connector that should be great.
Thanks
Ranny.