Part Number: TDA4VM
I want to mount the USB disk by USB0, but it doesn't work
Is the default configuration of EVM can mount USB disk by USB0?
NOTE: My SDK version is SDK8.0
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
I want to mount the USB disk by USB0, but it doesn't work
Is the default configuration of EVM can mount USB disk by USB0?
NOTE: My SDK version is SDK8.0
Hi,
Yes, The default configuration of the PSDK Linux rel 8.0 must support USB disk.
Please make sure the SW3 switch USBC_MODE_SEL pins SW 3.3 = 0 and SW 3.4 =1 so that it is in DRP (dual role).
Can you share the USB disk type being used and more detail on the issue by providing the full kernel debug log?
Thanks.