This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: Limit on the maximum capacity of eMMC when using Linux provided by TI

Guru 12050 points
Part Number: AM5748

Hi,

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/927908/am5716-max-emmc-size-supported-am5716?tisearch=e2e-sitesearch&keymatch=eMMC%20AM5716#

The E2E Thread above had the following answer:
 
ーーー
There is no limitation on size of eMMC supported, it would be limited by the Operating system and type of file system being used.32GB eMMC part is supported.
ーーー
[Question1]
Does the AM5748 eMMC support 64GB and 128GB as well?
 
[Question2]
It says "it would be limited by the Operating system and type of file system being used".
Is there a software limit on the maximum capacity of eMMC when using Linux provided by TI?
Thanks,
Koki