Hi Team,
I am trying to read 12 gpio pin i.e GPIO2_28, GPIO2_29,GPIO2_30, GPIO2_31,GPIO2_22,GPIO2_23,GPIO2_24,GPIO2_25, GPIO2_25, GPIO2_14,GPIO0_18, GPIO0_29 and GPIO3_13 pin of AM3359 processor.
From FPGA signal are coming to this above pins which is configured as input pin and mode is set as 7 for GPIO in dts file.
I am getting correct value(0x00000FFF),when i am reading FPGA register but when i am using below echo command i could not able to read GPIO value.
Please find the below logs for gpio read:
root@RCU:~# echo 86 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio86/direction
in /sys/class/gpio/gpio86/direction
root@RCU:~# cat /sys/class/gpio/gpio86/value
0
root@RCU:~#
root@RCU:~# echo 87 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio87/direction
in /sys/class/gpio/gpio87/direction
root@RCU:~# cat /sys/class/gpio/gpio87/value
0
root@RCU:~#
root@RCU:~# echo 88 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio88/direction
in /sys/class/gpio/gpio88/direction
root@RCU:~# cat /sys/class/gpio/gpio88/value
0
root@RCU:~#
root@RCU:~# echo 89 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio89/direction
in /sys/class/gpio/gpio89/direction
root@RCU:~# cat /sys/class/gpio/gpio89/value
0
root@RCU:~#
root@RCU:~# echo 78 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio78/direction
in /sys/class/gpio/gpio78/direction
root@RCU:~# cat /sys/class/gpio/gpio78/value
1
root@RCU:~#
root@RCU:~# echo 18 > /sys/class/gpio/export
root@RCU:~# echo "in" /sys/class/gpio/gpio18/direction
in /sys/class/gpio/gpio18/direction
root@RCU:~# cat /sys/class/gpio/gpio18/value
0
root@RCU:~#
root@RCU:~# echo 89 > /sys/class/gpio/export
sh: write error: Device or resource busy
root@RCU:~# echo "in" /sys/class/gpio/gpio89/direction
in /sys/class/gpio/gpio89/direction
root@RCU:~# cat /sys/class/gpio/gpio89/value
0
root@RCU:~#
why i could not able to read gpio value ?.
what are the other method to read 12 gpio pins at a time ?.
Please help me on this.
Regards,
Amit Kumar Keshri