This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where to put shared memory in the C6a816x?



I have the C6a816/AM389x Integra EVM and in considering both the memory map given by the EZSDK FAQ:

http://processors.wiki.ti.com/images/e/eb/Ez_sdk_memory_map.PNG

and that given by evmTI816x.platform in XDCTOOLS, I am wondering where to put  memory regions shared by both the ARM and the DSP.  The memory map diagram in the FAQ suggests using space after 0x90000000, requiring the definition of a new segment in evmTI816x.platform.  Is this correct?

Lee Holeva

 

  • Lee,

    We are looking into this and will get back with you as soon as we can.

    Regards,
    Marc

  • Lee,

           I hope you want to change the memory section SR1 as mentioned in the memory map diagram in FAQ, which is what is shared between ARM & DSP.

           To change you need to update the file (in case of c6accel application) ./soc/packages/ti/c6accel_unitservers/TI816X/serverplatforms.xs the below lines and all other sections appropriately.

               ["DDR3_SR1", {
                    comment: "DDR3 Memory reserved for use by SharedRegion 1",
                    name: "DDR3_SR1",
                    base: 0x8D000000,
                    len:  0x00C00000    /* 12 MB (Reserved)*/
                }],

     

            Could you also let us know your goal in this experiment, as i am not sure why you want to change this section but not others. 

    Best Regards

    Velan

  • Velan said:
    Could you also let us know your goal in this experiment, as i am not sure why you want to change this section but not others. 

     

    Actually, I may want to change all the sections to take advantage of the 1GB of DDR.  I'm still in getting-to-know mode and for now I'm using the Platform.xdc file that had been included with the Syslink samples:

    metaonly module Platform inherits xdc.platform.IPlatform {

        config ti.platforms.generic.Platform.Instance plat =
            ti.platforms.generic.Platform.create("plat", {
                clockRate:      800.0,
                catalogName:    "ti.catalog.c6000",
                deviceName:     "TMS320TI816X",
                externalMemoryMap: [
                    ["EXT_RAM",
                        {name: "EXT_RAM",     base: 0x80000000, len: 0x0A600000, space: "code/data",access: "RWX"}],
                    ["DDR2",
                        {name: "DDR2",        base: 0x8B000000, len: 0x02000000, space: "code/data",access: "RWX"}],
                    ["SHARED",
                        {name: "SHARED",      base: 0x8E000000, len: 0x01000000, space: "code/data",access: "RWX"}],
                    ["APPLICATION",
                        {name: "APPLICATION",  base: 0x8D000000, len: 0x00C00000, space: "code/data",access: "RWX"}],
                ],
                l1DMode:"32k",
                l1PMode:"32k",
                l2Mode:"256k",
        });

    instance :

        override config string codeMemory  = "DDR2";
        override config string dataMemory  = "DDR2";
        override config string stackMemory = "DDR2";

    }

    Lee Holeva