Part Number: TDA4VM-Q1
Hi,experts:
We are trying to debug a video sensor driver on a TDA4 board, but have encountered some problems.
Our existing software debugging environment is as follows:
1) TDA4 SDK version:
ti-processor-sdk-linux-j7-evm-08_01_00_07
ti-processor-sdk-rtos-j721e-evm-08_01_00_13
2) CCS debug emulator: XDS560v2
3) The video link is as follows:
[AR0233] --4-lane CSI-> [MAX9295] --GMSL2-> [MAX9296] --4-lane CSI-> [J721E]
4) Camera module parameters:
sensor resolution: 1920x1080@30fps
sensor data format: RAW12
5) Current debugging progress: I2C communication between TDA4 and MAX9295, MAX9296, AR0233 has been adjusted, and their registers can be read and written normally.
【Q1】: Which sample programs can be used under pdk to better configure and debug the registers of MAX9296, MAX9295 and AR0233?
【Q2】: Can you provide an example of the same type as MAX9295+MAX9296 for reference?
Thank you for your support, I will work hard to learn your products and keep improving.
Thanks!