Part Number: AM5718
Hi,
Customer encountered a problem when using the DSP core of AM5718 to test DeviceLoopback_ExampleProject. The clock line and synchronization line can output the corresponding waveform, but the AXR pin cannot output the waveform, the receive buffer cannot receive data, and the set callback function cannot be triggered. , check that the values of the TXSTAT and RXSTAT registers are 0x171 and 0x175 respectively.
/*
* bsp_mcasp.c
*
* Created on: 2022年3月10日
* Author: lhy0611
*/
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/Diags.h>
#include <xdc/runtime/Log.h>
#include <xdc/runtime/Assert.h>
#include <xdc/runtime/Registry.h>
#include <xdc/runtime/IHeap.h>
#include <xdc/runtime/Memory.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/heaps/HeapMem.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/ipc/Ipc.h>
#include <ti/ipc/MessageQ.h>
#include <ti/ipc/MultiProc.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <stdio.h>
#include <ti/csl/example/utils/common/inc/app_utils.h>
#include <ti/csl/soc.h>
#include <ti/csl/hw_types.h>
#include <ti/csl/csl_edma.h>
#include <ti/csl/csl_chip.h>
#include <ti/csl/arch/csl_arch.h>
/* TI-RTOS Header files */
#include <ti/drv/gpio/GPIO.h>
#include <ti/drv/gpio/soc/GPIO_soc.h>
#include <ti/drv/gpio/test/led_blink/src/GPIO_log.h>
#include <ti/drv/gpio/test/led_blink/src/GPIO_board.h>
#include <ti/board/board.h>
#include <ti/osal/osal.h>
#include <ti/osal/CacheP.h>
/* EDMA3 头文件 */
#include <ti/sdo/edma3/drv/edma3_drv.h>
#include <ti/sdo/edma3/rm/edma3_rm.h>
#include <ti/sdo/edma3/rm/sample/bios6_edma3_rm_sample.h>
#include <ti/drv/mcasp/mcasp_drv.h>
#include <ti/drv/mcasp/mcasp_osal.h>
#include <ti/drv/mcasp/soc/mcasp_soc.h>
#include <ti/csl/csl_mcasp.h>
#include <bsp_mcasp.h>
#include <mcasp_cfg.h>
#include <mcasp_drv.h>
#include <mcasp_tune.h>
void Configure_XBAR(void)
{
/* Mapping the DMA crossbar for McASP DMA_DREQ_(128-120) in to EDMA3_DREQ_0-15.
* The EDMA3_DREQ_0-15 correspond to (CSL_EDMA3_CHA_MCASP'n'_RX) which are
* used inside mcasp_soc.c to register EDMA. Please note that the API below takes
* the mapped DMAReq with 1 as the base, whereas CSL_EDMA3_CHA_MCASP'n'
* are with base 0 */
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 128,
1 + CSL_EDMA3_CHA_MCASP0_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 129,
1 + CSL_EDMA3_CHA_MCASP0_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 130,
1 + CSL_EDMA3_CHA_MCASP1_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 131,
1 + CSL_EDMA3_CHA_MCASP1_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 132,
1 + CSL_EDMA3_CHA_MCASP2_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 133,
1 + CSL_EDMA3_CHA_MCASP2_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 134,
1 + CSL_EDMA3_CHA_MCASP3_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 135,
1 + CSL_EDMA3_CHA_MCASP3_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 136,
1 + CSL_EDMA3_CHA_MCASP4_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 137,
1 + CSL_EDMA3_CHA_MCASP4_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 138,
1 + CSL_EDMA3_CHA_MCASP5_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 139,
1 + CSL_EDMA3_CHA_MCASP5_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 140,
1 + CSL_EDMA3_CHA_MCASP6_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 141,
1 + CSL_EDMA3_CHA_MCASP6_TX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 142,
1 + CSL_EDMA3_CHA_MCASP7_RX);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_EDMA, 143,
1 + CSL_EDMA3_CHA_MCASP7_RX);
}
void configMcASP_SocHwInfo(void)
{
/* Configure the interrupts for the McASP Instance MCASP_NUM */
/* ON Keystone, it involves CIC programming as well.
* The McASP does that internally, if configured with the correct parameters.
* Such as muxNum, muxInEvent, muxOutEvent,
* cpuInEventNum, cpuIntNum
*/
Mcasp_HwInfo hwInfo;
Mcasp_socGetInitCfg(MCASP_NUM, &hwInfo);
if ((hwInfo.rxMuxOutEvent == MCASP_UNASSIGNED_MUX_EVENTNUM)
|| (hwInfo.txMuxOutEvent == MCASP_UNASSIGNED_MUX_EVENTNUM))
{
#ifdef _TMS320C6X
/* Choosing a free Crossbar Instance number from Table 17-3. DSP1_INTC Default Interrupt Mapping
* in the AM572x TRM . Please note that this is fore Core 0 , i.e DSP1 only*/
/* Freely available cross bar instance numbers for DSP1 */
hwInfo.txMuxOutEvent = CSL_XBAR_INST_DSP1_IRQ_74;
hwInfo.rxMuxOutEvent = CSL_XBAR_INST_DSP1_IRQ_75;
/* The CPU event numbers corresponding to the above */
hwInfo.cpuTxEventNumber = 74;
hwInfo.cpuRxEventNumber = 75;
#endif
}
/* Write back */
Mcasp_socSetInitCfg(MCASP_NUM, &hwInfo);
}
extern EDMA3_DRV_GblConfigParams sampleEdma3GblCfgParams[];
static void enableEDMAHwEvent(uint32_t edmaNum, uint32_t eventNo)
{
sampleEdma3GblCfgParams[edmaNum].dmaChannelHwEvtMap[eventNo / 32] |= (1
<< (eventNo % 32));
}
EDMA3_DRV_Handle McaspApp_edmaInit(Mcasp_HwInfo *cfg)
{
EDMA3_DRV_Handle hEdma;
EDMA3_DRV_Result edmaResult = 0;
enableEDMAHwEvent(EDMACC_NUM, CSL_EDMA3_CHA_MCASP2_RX);
enableEDMAHwEvent(EDMACC_NUM, CSL_EDMA3_CHA_MCASP2_TX);
hEdma = edma3init(EDMACC_NUM, &edmaResult);
if (edmaResult != EDMA3_DRV_SOK)
{
/* Report EDMA Error
*/
System_printf("\nEDMA driver initialization unsuccessful\n");
}
else
{
System_printf("\nEDMA driver initialization successful.\n");
}
return hEdma;
}
void mcaspAppCallback(void *arg, MCASP_Packet *ioBuf)
{
System_printf("\nmcaspAppCallback.\n");
if (ioBuf->cmd == MCASP_READ)
{
}
else if (ioBuf->cmd == MCASP_WRITE)
{
}
else
{
}
}
Mcasp_HwSetupData mcaspRcvSetup = {
/* .rmask = */0xFFFFFFFF,
/* All the data bits are to be used */
/* .rfmt = */0x000080b0,
/* 0 bit delay from framsync
* MSB first
* No extra bit padding
* Padding bit (ignore)
* slot Size is 24
* Reads from DMA port
* NO rotation
*/
/* .afsrctl = */0x00000193, /* 3-slot TDM mode,
* Frame sync is one word
* Internally generated frame sync
* Falling edge is start of frame
*/
/* I2S MODE*/
/* .rtdm = */0x00000007, /* 3 slots are active
* */
/* .rintctl = */0x000000b3, /* sync error and overrun error */
/* .rstat = */0x000001FF, /* reset any existing status bits */
/* .revtctl = */0x00000000, /* DMA request is enabled or disabled */
{ //25Mhz
/* I2S MODE*/
/* .aclkrctl = */0x00000023, /* Div (4), Internal Source, rising edge */
/* .ahclkrctl = */0x00008003, /* Div (4), Internal AUX_CLK Source */
/* .rclkchk = */0x00000000 } };
Mcasp_HwSetupData mcaspXmtSetup = {
/* .xmask = */0xFFFFFFFF, /* All the data bits are to be used */
/* I2S MODE*/
/* .xfmt = */0x000080b0, //0x4846 80A8
/*
* 0 bit delay from framsync
* MSB first
* No extra bit padding
* Padding bit (ignore)
* slot Size is 24
* Reads from DMA port
* 0-bit rotation
*/
/*I2S MODE*/
/* .afsxctl = */0x00000193, /* 3-slot TDM mode,//0x4846 80AC
* Frame sync is one word
* internally generated frame sync
* Falling edge is start of frame
*/
/* .xtdm = */0x00000007, /* 3 slots are active */ // 0x4846 80B8
/* .xintctl = */0x000000b7, /* sync error,overrun error,clK error */ //0x4846 80BC
/* .xstat = */0x000001FF, /* reset any existing status bits */ //0x4846 80C0
/* .xevtctl = */0x00000000, /* DMA request is enabled or disabled */ //0x4846 80CC
{ //25Mhz
/* I2S MODE*/ // 0x4846 80B0
/* .aclkxctl = */0x00000023, /* Div (4), Internal Source, SYNC, Falling edge */
/* .ahclkxctl = */0x00008003, /* Div (4), Internal AUX_CLK Source */
/* .xclkchk = */0x00000000 },
};
/* The below variables are used to quit the frame processing loop if an error occurs */
int gblErrFlagXmt = 0;
int gblErrFlagRcv = 0;
/* The below variables are used to analyze the errors if an error interrupt happens */
Mcasp_errCbStatus errCbStatusXmt;
Mcasp_errCbStatus errCbStatusRcv;
/* Error handler for Transmit side */
void GblErrXmt(Mcasp_errCbStatus errCbStat)
{
gblErrFlagXmt = 1;
errCbStatusXmt = errCbStat;
System_printf("GblErrXmt\n");
}
/* Error handler for Rcv side */
void GblErrRcv(Mcasp_errCbStatus errCbStat)
{
gblErrFlagRcv = 1;
errCbStatusRcv = errCbStat;
System_printf("GblErrRcv\n");
}
Mcasp_Params mcaspParams;
Ptr hMcaspDev;
/* McAsp channel parameters */
Mcasp_ChanParams mcasp_txchanparam = { //
.noOfSerRequested = TX_NUM_SERIALIZER, //1
.indexOfSersRequested = { Mcasp_SerializerNum_0 }, //
.mcaspSetup = &mcaspXmtSetup, //
.isDmaDriven = TRUE, .channelMode = Mcasp_OpMode_TDM, //
.wordWidth = Mcasp_WordLength_24, //
.userLoopJobBuffer = NULL, .userLoopJobLength = 0, //
.edmaHandle = NULL, //
.gblCbk = (Mcasp_GblCallback) &GblErrXmt, //
.noOfChannels = 1, //
.dataFormat = Mcasp_BufferFormat_1SER_MULTISLOT_NON_INTERLEAVED, //
.enableHwFifo = TRUE, //
.hwFifoEventDMARatio = TX_FIFO_EVENT_DMA_RATIO, //
.isDataPacked = TRUE, //
.wordBitsSelect = Mcasp_WordBitsSelect_LSB //
};
Mcasp_ChanParams mcasp_rxchanparam = { //
.noOfSerRequested = RX_NUM_SERIALIZER, //1
.indexOfSersRequested = { Mcasp_SerializerNum_1 }, //
.mcaspSetup = &mcaspRcvSetup, //
.isDmaDriven = TRUE, //
.channelMode = Mcasp_OpMode_TDM, //
.wordWidth = Mcasp_WordLength_24, //
.userLoopJobBuffer = NULL, //
.userLoopJobLength = 0, //
.edmaHandle = NULL, //
.gblCbk = (Mcasp_GblCallback) &GblErrRcv, //
.noOfChannels = 1, //
.dataFormat = Mcasp_BufferFormat_1SER_MULTISLOT_NON_INTERLEAVED, //
.enableHwFifo = TRUE, //
.hwFifoEventDMARatio = RX_FIFO_EVENT_DMA_RATIO, //
.isDataPacked = TRUE, //
.wordBitsSelect = Mcasp_WordBitsSelect_LSB //
};
/* Channel Handles */
Ptr hMcaspTxChan;
Ptr hMcaspRxChan;
/**************************************************************************************/
/* FUNCTION DESCRIPTION: This utility function converts local GEM L2 address in to global
memory addresses used by the EDMA inside McASP
*/
/**************************************************************************************/
static uintptr_t getGlobalAddr(uintptr_t addr)
{
if ((addr >= 0x800000) && (addr < 0x1000000))
{
#ifdef _TMS320C6X
uint32_t coreNum;
/* Get the core number. */
coreNum = CSL_chipReadReg(CSL_CHIP_DNUM);
#if defined(SOC_AM572x) || defined(SOC_AM571x)
/* Compute the global address. */
return ((1 << 30) | (coreNum << 24) | (addr & 0x00ffffff));
#else
/* Compute the global address. */
return ((1 << 28) | (coreNum << 24) | (addr & 0x00ffffff));
#endif
#else
return addr;
#endif
}
else
{
/* non-L2 address range */
return addr;
}
}
/*
* ======== prime ========
*/
MCASP_Packet rxFrame;
MCASP_Packet txFrame;
#pragma DATA_SECTION (rxbuf,".l2sram")
#pragma DATA_ALIGN (rxbuf,128)
uint8_t rxbuf[100];
#pragma DATA_SECTION (txbuf,".l2sram")
#pragma DATA_ALIGN (txbuf,128)
uint8_t txbuf[100];
Void mcasp_test_Task(void)
{
Mcasp_HwInfo hwInfo;
volatile int32_t i32Count, status = 0;
int32_t count = 0;
Mcasp_socGetInitCfg(MCASP_NUM, &hwInfo);
hwInfo.dmaHandle = McaspApp_edmaInit(&hwInfo);
Mcasp_socSetInitCfg(MCASP_NUM, &hwInfo);
mcaspParams = Mcasp_PARAMS;
mcaspParams.mcaspHwSetup.glb.dlbMode = (CSL_MCASP_DLBCTL_DLBEN_ENABLE
| ( CSL_MCASP_DLBCTL_ORD_XMTEVEN << CSL_MCASP_DLBCTL_ORD_SHIFT)
| ( CSL_MCASP_DLBCTL_MODE_XMTCLK << CSL_MCASP_DLBCTL_MODE_SHIFT));
status = mcaspBindDev(&hMcaspDev, MCASP_NUM, &mcaspParams);
if ((status != MCASP_COMPLETED) || (hMcaspDev == NULL))
{
System_printf("mcaspBindDev for McASP Failed\n");
// abort();
}
else
{
System_printf("mcaspBindDev for McASP success\n");
}
/* Create Mcasp channel for Tx */
status = mcaspCreateChan(&hMcaspTxChan, hMcaspDev, MCASP_OUTPUT,
&mcasp_txchanparam, mcaspAppCallback, NULL);
if ((status != MCASP_COMPLETED) || (hMcaspTxChan == NULL))
{
System_printf("mcaspCreateChan for McASP3 Tx Failed %d\n", status);
// BIOS_exit(0);
}
else
{
System_printf("mcaspCreateChan for McASP3 Tx success\n");
}
/* Create Mcasp channel for Rx */
status = mcaspCreateChan(&hMcaspRxChan, hMcaspDev, MCASP_INPUT,
&mcasp_rxchanparam, mcaspAppCallback, NULL);
if ((status != MCASP_COMPLETED) || (hMcaspRxChan == NULL))
{
System_printf("mcaspCreateChan for McASP3 Rx Failed\n");
// BIOS_exit(0);
}
else
{
System_printf("mcaspCreateChan for McASP3 Rx success\n");
}
uint32_t tx_bytes_per_sample = (mcasp_txchanparam.wordWidth / 8);
uint32_t rx_bytes_per_sample = (mcasp_rxchanparam.wordWidth / 8);
uint32_t tx_frame_size = mcasp_txchanparam.noOfSerRequested
* tx_bytes_per_sample;
uint32_t rx_frame_size = mcasp_rxchanparam.noOfSerRequested
* rx_bytes_per_sample;
System_printf("rx_frame_size:%d,tx_frame_size:%d\n", rx_frame_size,
tx_frame_size);
// rxbuf = malloc(rx_frame_size);
// txbuf = malloc(tx_frame_size);
memset(rxbuf, 0, rx_frame_size);
memset(txbuf, 3, tx_frame_size);
rxFrame.cmd = MCASP_READ;
rxFrame.addr = rxbuf; //(void*)(getGlobalAddr((uintptr_t) rxbuf));
rxFrame.size = rx_frame_size;
rxFrame.arg = (uintptr_t) hMcaspRxChan;
rxFrame.status = 0;
rxFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcaspSubmitChan(hMcaspRxChan, &rxFrame);
if ((status != MCASP_PENDING))
{
System_printf(
"Debug: Error McASP3 RX : Prime buffer #%d submission FAILED\n",
status);
}
else
{
System_printf(
"Debug: McASP3 RX : Prime buffer #%d submission Success\n",
status);
}
txFrame.cmd = MCASP_WRITE;
txFrame.addr = txbuf; //(void*) (getGlobalAddr((uintptr_t) txbuf));
txFrame.size = tx_frame_size;
txFrame.arg = (uintptr_t) hMcaspTxChan;
txFrame.status = 0;
txFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcaspSubmitChan(hMcaspTxChan, &txFrame);
if ((status != MCASP_PENDING))
{
System_printf(
"Debug: Error McASP3 TX : Prime buffer #%d submission FAILED\n",
status);
}
else
{
System_printf(
"Debug: McASP3 TX : Prime buffer #%d submission Success\n",
status);
}
Task_sleep(1000);
int cnt = 0;
for (cnt = 0; cnt < tx_frame_size; cnt++)
{
System_printf("txbuf[%d]:%d,rxbuf[%d]:%d\r\n", cnt, txbuf[cnt], cnt,
rxbuf[cnt]);
}
status = McASPTxStatusGet(CSL_MPU_MCASP3_CFG_REGS); //0x4846 80c0
System_printf("Txstatus:%x\r\n", status);
status = McASPRxStatusGet(CSL_MPU_MCASP3_CFG_REGS); //0x4846 8080
System_printf("Rxstatus:%x\r\n", status);
//
// status = mcaspControlChan(hMcaspRxChan, Mcasp_IOCTL_CHAN_PARAMS_WORD_WIDTH,
// &mcasp_chanparam[0]);
status = mcaspDeleteChan(hMcaspRxChan);
System_printf("Deleting Rx channel %d\r\n", status);
status = mcaspDeleteChan(hMcaspTxChan);
System_printf("Deleting Tx channel %d\r\n", status);
status = mcaspUnBindDev(hMcaspDev);
System_printf("UnBinding Mcasp %d\r\n", status);
}
void McASP3_Enable(void)
{
//uint32_t regVal = 0U;
// Choose SYS_CLK2 (22.5792 MHZ) as source for ABE_PLL REF CLK
HW_WR_FIELD32(CSL_DSP_CKGEN_PRM_REGS+CSL_CKGEN_PRM_CM_CLKSEL_ABE_PLL_SYS_REG, \
CSL_CKGEN_PRM_CM_CLKSEL_ABE_PLL_SYS_REG_CLKSEL, \
CSL_CKGEN_PRM_CM_CLKSEL_ABE_PLL_SYS_REG_CLKSEL_SEL_SYS_CLK1);
/* Reprogram ABE DPLL for 451.584 MHz output on PER_ABE_X1_GFCLK line */
// step 1: disable the PLL, if enabled (ex: via GEL)
while(HW_RD_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN) == CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN_DPLL_LOCK_MODE)
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN_DPLL_FR_BYP_MODE);
// step 2: modify Synthesized Clock Parameters - DPLL MULT & DIV
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKSEL_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKSEL_DPLL_ABE_REG_DPLL_MULT, \
0xC8);
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKSEL_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKSEL_DPLL_ABE_REG_DPLL_DIV, \
0x09);
// step 3: Configure output clocks parameters - M2 = 1 M3 = 1
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_DIV_M2_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_DIV_M2_DPLL_ABE_REG_DIVHS, \
0x1);
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_DIV_M3_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_DIV_M3_DPLL_ABE_REG_DIVHS, \
0x1);
// step 4: Confirm that the PLL has locked
while(HW_RD_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN) != CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN_DPLL_LOCK_MODE)
HW_WR_FIELD32(CSL_DSP_CKGEN_CM_CORE_AON_REGS+CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN, \
CSL_CKGEN_CM_CORE_AON_CM_CLKMODE_DPLL_ABE_REG_DPLL_EN_DPLL_LOCK_MODE);
/* McASP3 Module Control */
HW_WR_FIELD32(CSL_DSP_L4PER_CM_CORE_REGS+CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_MCASP3_CLKCTRL_REG, \
CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_MCASP3_CLKCTRL_REG_MODULEMODE, \
CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_MCASP3_CLKCTRL_REG_MODULEMODE_ENABLE);
while ((HW_RD_REG32(CSL_DSP_L4PER_CM_CORE_REGS+CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_MCASP3_CLKCTRL_REG) & CM_L4PER2_MCASP3_CLKCTRL_MODULEMODE_MASK) != \
CSL_L4PER_CM_CORE_COMPONENT_CM_L4PER2_MCASP3_CLKCTRL_REG_MODULEMODE_ENABLE) ;
/* PAD IO Config for McASP3 pins - ACLKX, AFSX, AXR0, AXR1*/
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_ACLKX, \
CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_ACLKX_MCASP3_ACLKX_MUXMODE, \
0xc0000);//0x4a00 3724
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_FSX, \
CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_FSX_MCASP3_FSX_MUXMODE, \
0xc0000);//0x4a00 3728
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_AXR0, \
CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_AXR0_MCASP3_AXR0_MUXMODE, \
0xc0000);//0x4a00 372c
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_AXR1, \
CSL_CONTROL_CORE_PAD_IO_PAD_MCASP3_AXR1_MCASP3_AXR1_MUXMODE, \
0xc0000);//0x4a00 3730
//HW_WR_REG32(0x4AE06160, 0x1); // CM_CLKSEL_CLKOUT2: 0x1: Selects SYS_CLK2
HW_WR_FIELD32(CSL_DSP_CKGEN_PRM_REGS+CSL_CKGEN_PRM_CM_CLKSEL_CLKOUTMUX2_REG, \
CSL_CKGEN_PRM_CM_CLKSEL_CLKOUTMUX2_REG_CLKSEL, \
CSL_CKGEN_PRM_CM_CLKSEL_CLKOUTMUX2_REG_CLKSEL_SEL_SYS_CLK2);//0x4ae0 6160
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_XREF_CLK0, \
CSL_CONTROL_CORE_PAD_IO_PAD_XREF_CLK0_XREF_CLK0_INPUTENABLE, \
0x0); // 0x0: Receive mode is disabled
HW_WR_FIELD32(CSL_DSP_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_XREF_CLK0, \
CSL_CONTROL_CORE_PAD_IO_PAD_XREF_CLK0_XREF_CLK0_MUXMODE, \
0x9); //0x9: clkout2 //0x4a00 3694
HW_WR_FIELD32(CSL_DSP_COREAON_CM_CORE_REGS+CSL_COREAON_CM_CORE_CM_COREAON_DUMMY_MODULE2_CLKCTRL_REG, \
CSL_COREAON_CM_CORE_CM_COREAON_DUMMY_MODULE2_CLKCTRL_REG_OPTFCLKEN_CLKOUTMUX2_CLK, \
CSL_COREAON_CM_CORE_CM_COREAON_DUMMY_MODULE2_CLKCTRL_REG_OPTFCLKEN_CLKOUTMUX2_CLK_FCLK_EN);//0x4a00 86b0
}
/***************************** End Of File ***********************************/
Below is test log:
1.021] Error waiting for packets!
[ 1.021]
[ 1.021] Total frames sent: 0
[ 1.021] Total frames received: 0
[ 1.021]
[ 1.021] ******************* Transmit Watch dog stats ****************
[ 1.021] ------------ Error stats --------------
[ 1.021] ***** isClkFailErr : 0
[ 1.021] ***** isDMAErr : 0
[ 1.021] ***** isSyncErr : 0
[ 1.021] ***** retVal : -1
[ 1.021] ***** isRcvOvrRunOrTxUndRunErr : 1
[ 1.021]
[ 1.021]
[ 1.021] ******************* Receive Watch dog stats ****************
[ 1.021] ------------ Error stats --------------
[ 1.021] ***** isClkFailErr : 1
[ 1.021] ***** isDMAErr : 0
[ 1.021] ***** isSyncErr : 0
[ 1.021] ***** retVal : -1
[ 1.021] ***** isRcvOvrRunOrTxUndRunErr : 0
[ 1.021]
[ 1.021] Deleting Rx channel
[ 1.021] Deleting Tx channel
[ 1.021] UnBinding Mcasp
[ 1.021] TEST FAIL: Test quit after sending 0 frames and receiving 0 frames.
[ 1.021]
[ 1.021] TEST FAIL: Ramp test never found sync on rx for Serializer=0, timeslot=0
[ 1.021]
[ 1.021] TEST FAIL: Ramp test never found sync on rx for Serializer=0, timeslot=1
[ 1.021]
[ 1.021] TEST FAIL:Some tests have failed