Hello,
1. We are having a device which uses TI's Sitara-am335x processor (Part No: AM3356BZCZD60).
2. We are Currently trying to upgrade to new 512MB (4Gb)-256Mx16 ISSI SDRAM (part no:IS43TR16256B-125KBLI). Previously We were using 256MB (2Gb)-128Mx16 ISSI SDRAM (part no:512MBIS43TR16128B-125KBLI)
2. We transferred the uboot-spl.bin file over X-Modem protocol, but when we tried to transfer the uboot-img.bin over Y-Modem, the operation gets failed. I assume this is because the required support for 512MB RAMSIZE is not present in the uboot-spl.bin image.
3. Kindly advise what are the changes required in U-boot & kernel source to integrate the new RAM support for am335x.
4. Below is the Uboot version taken from a working device (with 256MB/2Gb RAM). We are using the same u-boot-spL and u-boot.img images in the new proto as well.
U-Boot 2018.01-00444-g96cdbef-dirty (Dec 01 2021 - 23:25:16 +0530)