This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3505: Clarification of am35X Technical Reference manual

Part Number: AM3505


We are using the ccdc interface on an am3505 processor.  

The control register:  Control_Devconf2 bit vpfe_pclk_invert_en  has the following description:

0 Do not invert the pclk

1 Invert the pclk

 

My question is with a setting of 0   is the ccdc data sampled on the rising edge of pclk or the falling edge?

  • Paul

    The data will be sample on the opposite edge. However, I am checking to see on which edge the data is captured when not inverted. 

    --Paul 

  • Sorry to be dense but I could use a clarification of what sample on the opposite edge means.

    PaulM thanks for you attention to this item

  • If the VPFE uses the falling edge of PLCLK to capture the data, then setting  vpfe_pclk_invert_en would mean that the VPFE would then using the rising edge of PCLK to capture the data, ie the opposite edge.  What I don't know yet is which edge of PCLK the VPFE natively uses to capture the data.

    --Paul

  • Paul

    I was unable to find a definitive answer. However, I did find the following statement relating to the vpfe_pclk_invert_en bit:

    "There is an option of inverting this clock internally to support sensors which launches data on negative clock edge"

    This implies that when vpfe_pclk_invert_en is "0", the IP expects the sensor to launch data on the rising clock edge and be captured, by the IP, using the falling clock edge. Therefore, setting vpfe_pclk_invert_en = "1", to invert PCLK (internally),  would then mean that the data is captured on the rising edge of the external PCLK.

    --Paul 

  • Thanks so much for your help.   Where was this statement found.   Did I miss it in the technical reference manual or datasheet?  Would it be possible to get the document that it was found in?

    Again thanks for your help.

  • Paul

    The statement was in an internal design spec..

      Paul