Hi,
I am using C6745 (BIOS_5_33_05) and I have the PLLEN set to 1 for "PLL mode, not bypassed". The DSP has an external oscillator and external watchdog. The firmware toggling the watchdog from the highest priority task every 400msec. During ESD testing, we used the spectrum analyzer to sniff the system clock at 300MHz. After ESD shots, the system clock disappeared from the spectrum analyzer. However, the watchdog still got kicked but at a weird interval 1.66 second low and 1.77milli-second high from the oscilloscope. My thought was the firmware couldn't be running without the system clock. Is it possible that the DSP got zapped and the PLL switch to a bypass clock even that I set PLLEN to 1? Any suggestion for this scenario to reset the DSP?
Thanks,
Dennis Nguyen