Part Number: TDA2EG-17
Dear all,
I create a new static lib , name is file.a , and I use some function from file.a
And I see VisionSDK_UserGuide_BuildSystem.pdf Chapter 8 Adding new library to appliation
Then I add my new library in MAKEFILE.MK
like this => LIBS += file.a
But happend error : undefined reference to" "some function"
but it seems to have no effect
I would like to ask where to add the .a lib under LINUX to be included (VSDK 0307)
Thanks a lot!!
David.