This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: U-Boot execute "rproc init"

Part Number: TDA4VM

Hi Sir :

If I execute "rproc init" in the U-boot, I will get a failure message. What is the problem?

NOTICE:  BL31: v2.4(release):07.03.00.005-dirty
NOTICE:  BL31: Built : 00:15:40, Apr 10 2021
ERROR:   GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader

U-Boot SPL 2020.01-00007-g5108984-dirty (Mar 25 2022 - 09:37:27 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
ti_i2c_eeprom_am6_parse_record: Ignoring record id 17
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2


U-Boot 2020.01-00007-g5108984-dirty (Mar 25 2022 - 09:37:27 +0800)

SoC:   J721E SR1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM:  4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:   K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000

Warning: ethernet@46000000 using MAC address from ROM
eth0: ethernet@46000000
Hit any key to stop autoboot:  0 
=> 
=> 
=> rproc init
Core 1 is already in use. No rproc commands work
Core 2 is already in use. No rproc commands work
ti-sci processor request failed: -19
rproc configure failed -19
Few Remote Processors failed to be initialized
=>