hi all:
I am using uart boot to flash the UBL and Uboot to Nand, type is K9F1G08U0B, I have another board ,which is based on DM355, and it works fine.
But it seems that K9F1G08U0B cannot work on DM365, From the console I saw sfh_DM36x.exe successfully wrote data to flash, but when I change the boot mode pin to NAND Boot, it has nothing from console.
Any advice?