Part Number: AM5728
Other Parts Discussed in Thread: BEAGLEBOARD-X15,
Hii,
i am using am57xx evm lcd module and i am using ti-processor-sdk-android-am57xx-evm-06.03.00.106.bin to bring up my board.
it generates different folder like bin,prebuilt images,u boot etc,
inside bin folder one script is available which is /create-sdcard.sh after running script it creates only one partition that is boot and copies u boot.img , uenv.txt, MLO into boot partition. no filesystem partition is available.

after creating partition i plugged in sd card into the board and try to run setup.sh it says ***Board could not be detected. Please connect the board to the PC.***
on minicom output is below says ***Wrong Image Format for bootm command ERROR: can't get kernel image!***
U-Boot SPL 2019.01-g333c3e72d3 (Apr 19 2020 - 06:06:00 +0000)
DRA752-GP ES2.0
no pinctrl state for default mode
** Unable to read file dra7-ipu1-fw.xem4 **
Firmware loading failed
Trying to boot from MMC1
no pinctrl state for default mode
Loading Environment from FAT... *** Warning - bad CRC, using default environment
Loading Environment from MMC... OK
U-Boot 2019.01-g333c3e72d3 (Apr 19 2020 - 06:06:00 +0000)
CPU : DRA752-GP ES2.0
Model: TI AM5728 BeagleBoard-X15
Board: AM572x EVM REV A.30
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment
Loading Environment from MMC... OK
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
1394 bytes read in 2 ms (680.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
1 bytes read in 2 ms (0 Bytes/s)
Already setup.
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file /zImage **
Trying to boot Linux from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** File not found /zImage **
Trying to boot Android from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
mmc - MMC sub system
Usage:
mmc info - display info of the current MMC device
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt
mmc rescan
mmc part - lists available partition on current mmc device
mmc dev [dev] [part] - show or set current mmc device [partition]
mmc list - lists available devices
mmc hwpartition [args...] - does hardware partitioning
arguments (sizes in 512-byte blocks):
[user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
[gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
[check|set|complete] - mode, complete set partitioning completed
WARNING: Partitioning is a write-once setting once it is set to complete.
Power cycling is required to initialize partitions after set to complete.
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
mmc rst-function dev value
- Change the RST_n_FUNCTION field of the specified device
WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
mmc setdsr <value> - set DSR register value
Wrong Image Format for bootm command
ERROR: can't get kernel image!
=>
U-Boot SPL 2019.01-g333c3e72d3 (Apr 19 2020 - 06:06:00 +0000)
DRA752-GP ES2.0
no pinctrl state for default mode
** Unable to read file dra7-ipu1-fw.xem4 **
Firmware loading failed
Trying to boot from MMC1
no pinctrl state for default mode
Loading Environment from FAT... *** Warning - bad CRC, using default environment
Loading Environment from MMC... OK
U-Boot 2019.01-g333c3e72d3 (Apr 19 2020 - 06:06:00 +0000)
CPU : DRA752-GP ES2.0
Model: TI AM5728 BeagleBoard-X15
Board: AM572x EVM REV A.30
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment
Loading Environment from MMC... OK
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
1394 bytes read in 2 ms (680.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
1 bytes read in 2 ms (0 Bytes/s)
Already setup.
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file /zImage **
Trying to boot Linux from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
** File not found /zImage **
Trying to boot Android from eMMC ...
switch to partitions #0, OK
mmc1(part 0) is current device
mmc - MMC sub system
Usage:
mmc info - display info of the current MMC device
mmc read addr blk# cnt
mmc write addr blk# cnt
mmc erase blk# cnt
mmc rescan
mmc part - lists available partition on current mmc device
mmc dev [dev] [part] - show or set current mmc device [partition]
mmc list - lists available devices
mmc hwpartition [args...] - does hardware partitioning
arguments (sizes in 512-byte blocks):
[user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
[gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
[check|set|complete] - mode, complete set partitioning completed
WARNING: Partitioning is a write-once setting once it is set to complete.
Power cycling is required to initialize partitions after set to complete.
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
mmc rst-function dev value
- Change the RST_n_FUNCTION field of the specified device
WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
mmc setdsr <value> - set DSR register value
Wrong Image Format for bootm command
ERROR: can't get kernel image!