Part Number: TDA4VM
What is the difference between SBL and SPL, and what scenarios are they used for?
Which SDK is used to make MMCSD for SBL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
What is the difference between SBL and SPL, and what scenarios are they used for?
Which SDK is used to make MMCSD for SBL
Hi,
Following are the differences between SBL & SPL:
| SBL | SPL |
| This is RTOS based custom boot loader. | This is standard U-Boot based boot loader. |
| This is to be built specifically for each boot media like OSPI, MMC, eMMC etc | Single Image caters to all the boot media. |
| The images are typically smaller in size. | The image size is large |
| The boot time is faster | The boot time is slower |
| This is applicable to scenario where the boot media is fixed and boot time is of utmost concern. | It has lot more features to offer. U-Boot gives command line interface. Very flexible for development scenarios |
Which SDK is used to make MMCSD for SBL
RTOS SDK should be used to build SBL for MMCSD
Best Regards,
Keerthy