This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Error message displayed when installing eSDK (Extensible SDK).

Part Number: AM3352

I posted this page https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1088892/error-message-displayed-when-installing-esdk-extensible-sdk#, but something problem was happened. I can't see this page correctly,  so I'll post this again.

I added the below modification to local.conf in tisdk (using SDK7.3), and SDK building was finished without any problem.

Then I created eSDK (Extensible SDK) which was explained in this page https://docs.yoctoproject.org/3.1.15/sdk-manual/sdk-manual.html# .
( I used this command  "MACHINE=am335x-evm bitbake tisdk-base-image -c populate_sdk_ext" )
After that, eSDK was created without any problem.
But, when installing eSDK, the error message "ERROR: Task pseudo-native.do_fetch attempted to execute unexpectedly" was displayed (see the attached log file in detail).

Do you have any solution to solve this issue ?

modification of build/local.conf

uegaki@admine330-Precision-3520:~/ex1/rmu/tisdk/build/conf$ diff local.conf.20211021_1758 local.conf
103c103,105
< EXTRA_IMAGE_FEATURES = "debug-tweaks"
---
> EXTRA_IMAGE_FEATURES = "debug-tweaks tools-debug read-only-rootfs ssh-server-openssh"
> IMAGE_INSTALL_append = " gdbserver openssh-sftp-server net-snmp-server nodejs mmc-utils rsyslog sqlite3 ntp ntpdate tree python3-flask python3-django python3-djangorestframework tzdata"
> VOLATILE_LOG_DIR = "no"

log file
51006.log.txt

  • Part Number: AM3352

    I added the below modification to local.conf in tisdk, and SDK building was finished without any problem.

    Then I created eSDK (Extensible SDK) which was explained in this page https://docs.yoctoproject.org/3.1.15/sdk-manual/sdk-manual.html# .
    ( I used this command  "MACHINE=am335x-evm bitbake tisdk-base-image -c populate_sdk_ext" )
    After that, eSDK was created without any problem.
    But, when installing eSDK, the error message "ERROR: Task pseudo-native.do_fetch attempted to execute unexpectedly" was displayed (the attached log file).

    Do you have any solution to solve this issue ?

    build/local.conf 

    uegaki@admine330-Precision-3520:~/ex1/rmu/tisdk/build/conf$ diff local.conf.20211021_1758 local.conf
    103c103,105
    < EXTRA_IMAGE_FEATURES = "debug-tweaks"
    ---
    > EXTRA_IMAGE_FEATURES = "debug-tweaks tools-debug read-only-rootfs ssh-server-openssh"
    > IMAGE_INSTALL_append = " gdbserver openssh-sftp-server net-snmp-server nodejs mmc-utils rsyslog sqlite3 ntp ntpdate tree python3-flask python3-django python3-djangorestframework tzdata"
    > VOLATILE_LOG_DIR = "no"
    

    log.txt

    0068.log.txt

  • Hello,

    I merged both of your inquiries together. Our Yocto expert will get back to you.

    Regards,

    Jianzhong