Hi,
I've been trying for a while now (first with NAND) to boot a kernel and filesystem from flash. I recently received a IO daughter card Rev. B and that is attached to my C6A816x-EVM DDR2 Rev. C board.
This morning I flashed u-boot to the NOR flash with JTAG & CCS5 which went OK and allowed me to flash kernel and rootfs to NOR via TFTP.
I see the same kind of behavior from the kerenl no matter if I am booting from NAND or NOR, both die and give a divide by zero about the time the rootfs should be mounted. I've been monitoring the commit messages in git and I think I might need to step up to the kernel in PSP 04.00.00.10 but I don't see a tag laid down on the Arago trees yet ... I only see the tag in the "people" git trees which I know is for staging.
Having said all that, I've tried using mtdblock3 & mtdblock7 as the rootfs and don't see much difference between the two. One way it appears to be trying to do NFS although I didn't tell it the rootfs was NFS which is kind of strange.
Below I'll post the kernel output messages from the 2.6.36+2.6.37-rc3 kernel that was bitbaked from the Arago git trees. Please let me know what I am missing:
Kernel output using mtdblock3:
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37-rc3 (hutch@localhost.localdomain) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #3 Wed May 4 14:35:53 EDT 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
bootconsole [earlycon0] enabled
reserved size = 0 at 0
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 25400
Kernel command line: console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 mem=100M earlyprintk
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 100MB = 100MB total
Memory: 96624k/96624k available, 5776k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xc6800000 - 0xf8000000 ( 792 MB)
lowmem : 0xc0000000 - 0xc6400000 ( 100 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0035000 ( 180 kB)
.text : 0xc0035000 - 0xc0447000 (4168 kB)
.data : 0xc0448000 - 0xc0483280 ( 237 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:400
GPMC revision 6.0
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_init_signal: Could not set signal i2c2_scl.i2c2_scl
_omap_mux_init_signal: Could not set signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_vpss device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
ti816x_pcie: Invoking PCI BIOS...
ti816x_pcie: Setting up Host Controller...
ti816x_pcie: Register base mapped @0xc6820000
ti816x_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c_omap i2c_omap.1: bus 1 rev4.0 at 100 kHz
i2c_omap i2c_omap.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Switched to NOHz mode on CPU #0
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb_hdrc: kernel must blacklist external hubs
musb_hdrc musb_hdrc.0: MUSB HDRC host driver
musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb_hdrc musb_hdrc.0: USB Host mode controller at c680c000 using DMA, IRQ 18
musb_hdrc: kernel must blacklist external hubs
musb_hdrc musb_hdrc.1: MUSB HDRC host driver
musb_hdrc musb_hdrc.1: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb_hdrc musb_hdrc.1: USB Host mode controller at c681e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
squashfs: version 4.0 (2009/01/31) Phillip Lougher
Registering mini_fo version $Id$
JFFS2 version 2.2. (NAND) .. 2001-2006 Red Hat, Inc.
msgmni has been set to 188
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap-hsuart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap-hsuart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap-hsuart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled, bootconsole disabled
console [ttyO2] enabled, bootconsole disabled
brd: module loaded
loop: module loaded
ahci ahci: forcing port_map 0x0 -> 0x3
ahci ahci: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci
scsi1 : ahci
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: found m25p05-nonjedec, expected w25x32
m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000012000 : "U-Boot Env"
mtd: partition "U-Boot Env" is out of reach -- disabled
0x000000000000-0x000000280000 : "Kernel"
mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000010000 : "File System"
mtd: partition "File System" is out of reach -- disabled
omap2-nand driver initializing
No NAND device found.
No NAND device found.
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
PSTATE 1f20000
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
1-0018 supply IOVDD not found, using dummy regulator
1-0018 supply DVDD not found, using dummy regulator
1-0018 supply AVDD not found, using dummy regulator
1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
emac-mii: probed
mdio_bus 1:01: DaVinci EMAC: mii bus found 31
ata1: SATA link down (SStatus 0 SControl 300)
ata2: SATA link down (SStatus 0 SControl 300)
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5e51600 r6:c5e51800 r5:00000000 r4:00000000
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5e51600 r6:c5e51800 r5:00000000 r4:00000000
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015db30>] (jffs2_do_mount_fs+0x0/0x648) from [<c015f7cc>] (jffs2_do_fill_super+0x15c/0x238)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5c22000 r6:00000080 r5:00000000 r4:00000080
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015db30>] (jffs2_do_mount_fs+0x0/0x648) from [<c015f7cc>] (jffs2_do_fill_super+0x15c/0x238)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
VFS: Mounted root (jffs2 filesystem) on device 31:3.
devtmpfs: error mounting -2
Freeing init memory: 180K
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:00000013 r6:c005e5c4 r5:c0008670 r4:c0483910
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0330824>] (panic+0x60/0x17c)
[<c03307c4>] (panic+0x0/0x17c) from [<c0035574>] (init_post+0xa4/0xc4)
r3:c5e49d00 r2:00000000 r1:c0576920 r0:c03ddb3d
[<c00354d0>] (init_post+0x0/0xc4) from [<c0008788>] (kernel_init+0x118/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Kernel output from using mtdblock7:
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37-rc3 (hutch@localhost.localdomain) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #3 Wed May 4 14:35:53 EDT 2011
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168evm
bootconsole [earlycon0] enabled
reserved size = 0 at 0
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 25400
Kernel command line: console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 mem=100M earlyprintk
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 100MB = 100MB total
Memory: 96624k/96624k available, 5776k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xc6800000 - 0xf8000000 ( 792 MB)
lowmem : 0xc0000000 - 0xc6400000 ( 100 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0035000 ( 180 kB)
.text : 0xc0035000 - 0xc0447000 (4168 kB)
.data : 0xc0448000 - 0xc0483280 ( 237 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:400
GPMC revision 6.0
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
omap_mux_init: Add partition: #1: core, flags: 0
_omap_mux_init_signal: Could not set signal i2c2_scl.i2c2_scl
_omap_mux_init_signal: Could not set signal i2c2_sda.i2c2_sda
NOR: Can't request GPMC CS
registered ti816x_vpss device
pm_dbg_init: only OMAP3 supported
Registered ti81xx_fb device
ti816x_pcie: Invoking PCI BIOS...
ti816x_pcie: Setting up Host Controller...
ti816x_pcie: Register base mapped @0xc6820000
ti816x_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c_omap i2c_omap.1: bus 1 rev4.0 at 100 kHz
i2c_omap i2c_omap.2: bus 2 rev4.0 at 100 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0
Switched to NOHz mode on CPU #0
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb_hdrc: kernel must blacklist external hubs
musb_hdrc musb_hdrc.0: MUSB HDRC host driver
musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb_hdrc musb_hdrc.0: USB Host mode controller at c680c000 using DMA, IRQ 18
musb_hdrc: kernel must blacklist external hubs
musb_hdrc musb_hdrc.1: MUSB HDRC host driver
musb_hdrc musb_hdrc.1: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb_hdrc musb_hdrc.1: USB Host mode controller at c681e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
squashfs: version 4.0 (2009/01/31) Phillip Lougher
Registering mini_fo version $Id$
JFFS2 version 2.2. (NAND) .. 2001-2006 Red Hat, Inc.
msgmni has been set to 188
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap-hsuart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap-hsuart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap-hsuart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled, bootconsole disabled
console [ttyO2] enabled, bootconsole disabled
brd: module loaded
loop: module loaded
ahci ahci: forcing port_map 0x0 -> 0x3
ahci ahci: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci
scsi1 : ahci
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
m25p80 spi1.0: found m25p05-nonjedec, expected w25x32
m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)
Creating 4 MTD partitions on "spi_flash":
0x000000000000-0x000000040000 : "U-Boot"
mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000012000 : "U-Boot Env"
mtd: partition "U-Boot Env" is out of reach -- disabled
0x000000000000-0x000000280000 : "Kernel"
mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
0x000000010000-0x000000010000 : "File System"
mtd: partition "File System" is out of reach -- disabled
omap2-nand driver initializing
No NAND device found.
No NAND device found.
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
i2c /dev entries driver
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
PSTATE 1f20000
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
1-0018 supply IOVDD not found, using dummy regulator
1-0018 supply DVDD not found, using dummy regulator
1-0018 supply AVDD not found, using dummy regulator
1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
ALSA device list:
#0: TI81XX EVM
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
emac-mii: probed
mdio_bus 1:01: DaVinci EMAC: mii bus found 31
ata1: SATA link down (SStatus 0 SControl 300)
ata2: SATA link down (SStatus 0 SControl 300)
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5e51600 r6:c5e51800 r5:00000000 r4:00000000
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5e51600 r6:c5e51800 r5:00000000 r4:00000000
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015db30>] (jffs2_do_mount_fs+0x0/0x648) from [<c015f7cc>] (jffs2_do_fill_super+0x15c/0x238)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Division by zero in kernel.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:c5c22000 r6:00000080 r5:00000000 r4:00000080
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0044328>] (__div0+0x18/0x20)
[<c0044310>] (__div0+0x0/0x20) from [<c018501c>] (Ldiv0+0x8/0x10)
[<c015db30>] (jffs2_do_mount_fs+0x0/0x648) from [<c015f7cc>] (jffs2_do_fill_super+0x15c/0x238)
[<c015f670>] (jffs2_do_fill_super+0x0/0x238) from [<c0160550>] (jffs2_fill_super+0xbc/0xd4)
r7:00000001 r6:00000000 r5:c5e51600 r4:c5e51800
[<c0160494>] (jffs2_fill_super+0x0/0xd4) from [<c020bd90>] (mount_mtd_aux+0x54/0xe8)
r7:00000000 r6:00008000 r5:c5df9200 r4:c5e51600
[<c020bd3c>] (mount_mtd_aux+0x0/0xe8) from [<c020be80>] (mount_mtd_nr+0x5c/0x64)
r7:00008000 r6:c0468580 r5:00000000 r4:c5e50c80
[<c020be24>] (mount_mtd_nr+0x0/0x64) from [<c020bfc8>] (mount_mtd+0x140/0x170)
r7:c0468580 r6:00008000 r5:01f00003 r4:c5e50c80
[<c020be88>] (mount_mtd+0x0/0x170) from [<c0160228>] (jffs2_mount+0x1c/0x28)
[<c016020c>] (jffs2_mount+0x0/0x28) from [<c00b4054>] (vfs_kern_mount+0xac/0x1d8)
[<c00b3fa8>] (vfs_kern_mount+0x0/0x1d8) from [<c00b41dc>] (do_kern_mount+0x3c/0xe0)
[<c00b41a0>] (do_kern_mount+0x0/0xe0) from [<c00c9c48>] (do_mount+0x68c/0x6ec)
r9:00000000 r8:c5e50c80 r7:00000020 r6:00000000 r5:00000000
r4:00008000
[<c00c95bc>] (do_mount+0x0/0x6ec) from [<c00c9d34>] (sys_mount+0x8c/0xcc)
[<c00c9ca8>] (sys_mount+0x0/0xcc) from [<c0008ef0>] (do_mount_root+0x28/0xc0)
r7:c5c12000 r6:c005e5c4 r5:c002bd7c r4:c5c12000
[<c0008ec8>] (do_mount_root+0x0/0xc0) from [<c0009174>] (mount_block_root+0x100/0x220)
r4:c5c12000
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xcc)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x1d4)
r4:c04832e4
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
VFS: Mounted root (jffs2 filesystem) on device 31:3.
devtmpfs: error mounting -2
Freeing init memory: 180K
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c03307c0>] (dump_stack+0x18/0x1c)
r7:00000013 r6:c005e5c4 r5:c0008670 r4:c0483910
[<c03307a8>] (dump_stack+0x0/0x1c) from [<c0330824>] (panic+0x60/0x17c)
[<c03307c4>] (panic+0x0/0x17c) from [<c0035574>] (init_post+0xa4/0xc4)
r3:c5e49d00 r2:00000000 r1:c0576920 r0:c03ddb3d
[<c00354d0>] (init_post+0x0/0xc4) from [<c0008788>] (kernel_init+0x118/0x154)
r5:c0008670 r4:c0483280
[<c0008670>] (kernel_init+0x0/0x154) from [<c005e5c4>] (do_exit+0x0/0x5b8)
r5:c0008670 r4:00000000
Here is my .config:
#
# Automatically generated make config: don't edit
# Linux/arm 2.6.37-rc3 Kernel Configuration
# Wed May 4 14:28:30 2011
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_GENERIC_GPIO=y
# CONFIG_ARCH_USES_GETTIMEOFFSET is not set
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_HAVE_PROC_CPU=y
CONFIG_GENERIC_HARDIRQS=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_NEED_DMA_MAP_STATE=y
CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
CONFIG_ARM_L1_CACHE_SHIFT_6=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_CONSTRUCTORS=y
CONFIG_HAVE_IRQ_WORK=y
#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_CROSS_COMPILE=""
CONFIG_LOCALVERSION=""
CONFIG_LOCALVERSION_AUTO=y
CONFIG_HAVE_KERNEL_GZIP=y
CONFIG_HAVE_KERNEL_LZMA=y
CONFIG_HAVE_KERNEL_LZO=y
CONFIG_KERNEL_GZIP=y
# CONFIG_KERNEL_LZMA is not set
# CONFIG_KERNEL_LZO is not set
# CONFIG_SWAP is not set
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
CONFIG_POSIX_MQUEUE=y
CONFIG_POSIX_MQUEUE_SYSCTL=y
CONFIG_BSD_PROCESS_ACCT=y
# CONFIG_BSD_PROCESS_ACCT_V3 is not set
# CONFIG_TASKSTATS is not set
# CONFIG_AUDIT is not set
# CONFIG_HAVE_GENERIC_HARDIRQS is not set
# CONFIG_SPARSE_IRQ is not set
#
# RCU Subsystem
#
CONFIG_TINY_RCU=y
# CONFIG_PREEMPT_RCU is not set
# CONFIG_TREE_RCU_TRACE is not set
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=17
# CONFIG_CGROUPS is not set
CONFIG_NAMESPACES=y
# CONFIG_UTS_NS is not set
# CONFIG_IPC_NS is not set
# CONFIG_USER_NS is not set
# CONFIG_PID_NS is not set
# CONFIG_NET_NS is not set
# CONFIG_SYSFS_DEPRECATED is not set
# CONFIG_RELAY is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE=""
CONFIG_RD_GZIP=y
CONFIG_RD_BZIP2=y
CONFIG_RD_LZMA=y
CONFIG_RD_LZO=y
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
# CONFIG_EMBEDDED is not set
CONFIG_UID16=y
CONFIG_SYSCTL_SYSCALL=y
CONFIG_KALLSYMS=y
# CONFIG_KALLSYMS_ALL is not set
CONFIG_KALLSYMS_EXTRA_PASS=y
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y
CONFIG_HAVE_PERF_EVENTS=y
CONFIG_PERF_USE_VMALLOC=y
#
# Kernel Performance Events And Counters
#
# CONFIG_PERF_EVENTS is not set
# CONFIG_PERF_COUNTERS is not set
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_PCI_QUIRKS=y
CONFIG_SLUB_DEBUG=y
CONFIG_COMPAT_BRK=y
# CONFIG_SLAB is not set
CONFIG_SLUB=y
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
CONFIG_KPROBES=y
CONFIG_KRETPROBES=y
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
CONFIG_HAVE_CLK=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
CONFIG_MODULES=y
# CONFIG_MODULE_FORCE_LOAD is not set
CONFIG_MODULE_UNLOAD=y
# CONFIG_MODULE_FORCE_UNLOAD is not set
CONFIG_MODVERSIONS=y
# CONFIG_MODULE_SRCVERSION_ALL is not set
CONFIG_BLOCK=y
# CONFIG_LBDAF is not set
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_INTEGRITY is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
# CONFIG_INLINE_SPIN_TRYLOCK is not set
# CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK is not set
# CONFIG_INLINE_SPIN_LOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK_IRQ is not set
# CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
CONFIG_INLINE_SPIN_UNLOCK=y
# CONFIG_INLINE_SPIN_UNLOCK_BH is not set
CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
# CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_READ_TRYLOCK is not set
# CONFIG_INLINE_READ_LOCK is not set
# CONFIG_INLINE_READ_LOCK_BH is not set
# CONFIG_INLINE_READ_LOCK_IRQ is not set
# CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
CONFIG_INLINE_READ_UNLOCK=y
# CONFIG_INLINE_READ_UNLOCK_BH is not set
CONFIG_INLINE_READ_UNLOCK_IRQ=y
# CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_WRITE_TRYLOCK is not set
# CONFIG_INLINE_WRITE_LOCK is not set
# CONFIG_INLINE_WRITE_LOCK_BH is not set
# CONFIG_INLINE_WRITE_LOCK_IRQ is not set
# CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
CONFIG_INLINE_WRITE_UNLOCK=y
# CONFIG_INLINE_WRITE_UNLOCK_BH is not set
CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
# CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
# CONFIG_MUTEX_SPIN_ON_OWNER is not set
# CONFIG_FREEZER is not set
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_AAEC2000 is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_VEXPRESS is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_BCMRING is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_CNS3XXX is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_MXC is not set
# CONFIG_ARCH_STMP3XXX is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP23XX is not set
# CONFIG_ARCH_IXP2000 is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_LOKI is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_NS9XXX is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_NUC93X is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_ARCH_PNX4008 is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C2410 is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5P6442 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_S5PV310 is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_TCC_926 is not set
# CONFIG_ARCH_LH7A40X is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_NOMADIK is not set
# CONFIG_ARCH_DAVINCI is not set
CONFIG_ARCH_OMAP=y
# CONFIG_PLAT_SPEAR is not set
#
# TI OMAP Common Features
#
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# OMAP Feature Selections
#
# CONFIG_OMAP_RESET_CLOCKS is not set
CONFIG_OMAP_MUX=y
# CONFIG_OMAP_MUX_DEBUG is not set
CONFIG_OMAP_MUX_WARNINGS=y
# CONFIG_OMAP_MCBSP is not set
# CONFIG_OMAP_MBOX_FWK is not set
CONFIG_OMAP_MPU_TIMER=y
# CONFIG_OMAP_32K_TIMER is not set
CONFIG_OMAP_DM_TIMER=y
# CONFIG_OMAP_PM_NONE is not set
CONFIG_OMAP_PM_NOOP=y
#
# TI OMAP2/3/4 Specific Features
#
CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
# CONFIG_ARCH_OMAP2 is not set
# CONFIG_ARCH_OMAP3 is not set
# CONFIG_ARCH_OMAP4 is not set
CONFIG_ARCH_TI81XX=y
CONFIG_ARCH_TI816X=y
# CONFIG_ARCH_TI814X is not set
#
# OMAP Board Type
#
#
# TI81XX Board Type
#
CONFIG_MACH_TI8168EVM=y
#
# Processor Type
#
CONFIG_CPU_32v6K=y
CONFIG_CPU_V7=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
CONFIG_ARM_THUMB=y
# CONFIG_ARM_THUMBEE is not set
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_DMA_MEM_BUFFERABLE=y
CONFIG_CPU_HAS_PMU=y
# CONFIG_ARM_ERRATA_430973 is not set
# CONFIG_ARM_ERRATA_458693 is not set
# CONFIG_ARM_ERRATA_460075 is not set
# CONFIG_ARM_ERRATA_743622 is not set
CONFIG_COMMON_CLKDEV=y
#
# Bus support
#
CONFIG_PCI=y
CONFIG_PCI_SYSCALL=y
CONFIG_ARCH_SUPPORTS_MSI=y
CONFIG_PCI_MSI=y
# CONFIG_PCI_DEBUG is not set
# CONFIG_PCI_STUB is not set
# CONFIG_PCI_IOV is not set
# CONFIG_PCCARD is not set
#
# Kernel Features
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
# CONFIG_HIGH_RES_TIMERS is not set
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_PREEMPT_NONE=y
# CONFIG_PREEMPT_VOLUNTARY is not set
# CONFIG_PREEMPT is not set
CONFIG_HZ=100
# CONFIG_THUMB2_KERNEL is not set
CONFIG_AEABI=y
CONFIG_OABI_COMPAT=y
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
# CONFIG_HIGHMEM is not set
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_HAVE_MEMBLOCK=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_VIRT_TO_BUS=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
CONFIG_NEED_PER_CPU_KM=y
CONFIG_FORCE_MAX_ZONEORDER=11
# CONFIG_LEDS is not set
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
# CONFIG_SECCOMP is not set
# CONFIG_CC_STACKPROTECTOR is not set
# CONFIG_DEPRECATED_PARAM_STRUCT is not set
#
# Boot options
#
CONFIG_ZBOOT_ROM_TEXT=0
CONFIG_ZBOOT_ROM_BSS=0
CONFIG_CMDLINE=""
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
# CONFIG_AUTO_ZRELADDR is not set
#
# CPU Power Management
#
# CONFIG_CPU_FREQ is not set
# CONFIG_CPU_IDLE is not set
#
# Floating point emulation
#
#
# At least one emulation must be selected
#
CONFIG_FPE_NWFPE=y
# CONFIG_FPE_NWFPE_XP is not set
# CONFIG_FPE_FASTFPE is not set
CONFIG_VFP=y
CONFIG_VFPv3=y
CONFIG_NEON=y
#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
# CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
CONFIG_HAVE_AOUT=y
# CONFIG_BINFMT_AOUT is not set
CONFIG_BINFMT_MISC=y
#
# Power management options
#
CONFIG_PM=y
CONFIG_PM_DEBUG=y
# CONFIG_PM_ADVANCED_DEBUG is not set
CONFIG_PM_VERBOSE=y
# CONFIG_SUSPEND is not set
# CONFIG_APM_EMULATION is not set
CONFIG_PM_RUNTIME=y
CONFIG_PM_OPS=y
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_NET=y
#
# Networking options
#
CONFIG_PACKET=y
CONFIG_UNIX=y
CONFIG_XFRM=y
# CONFIG_XFRM_USER is not set
# CONFIG_XFRM_SUB_POLICY is not set
# CONFIG_XFRM_MIGRATE is not set
# CONFIG_XFRM_STATISTICS is not set
# CONFIG_NET_KEY is not set
CONFIG_INET=y
# CONFIG_IP_MULTICAST is not set
# CONFIG_IP_ADVANCED_ROUTER is not set
CONFIG_IP_FIB_HASH=y
CONFIG_IP_PNP=y
CONFIG_IP_PNP_DHCP=y
CONFIG_IP_PNP_BOOTP=y
CONFIG_IP_PNP_RARP=y
# CONFIG_NET_IPIP is not set
# CONFIG_NET_IPGRE_DEMUX is not set
# CONFIG_ARPD is not set
# CONFIG_SYN_COOKIES is not set
# CONFIG_INET_AH is not set
# CONFIG_INET_ESP is not set
# CONFIG_INET_IPCOMP is not set
# CONFIG_INET_XFRM_TUNNEL is not set
CONFIG_INET_TUNNEL=m
CONFIG_INET_XFRM_MODE_TRANSPORT=y
CONFIG_INET_XFRM_MODE_TUNNEL=y
CONFIG_INET_XFRM_MODE_BEET=y
CONFIG_INET_LRO=y
CONFIG_INET_DIAG=y
CONFIG_INET_TCP_DIAG=y
# CONFIG_TCP_CONG_ADVANCED is not set
CONFIG_TCP_CONG_CUBIC=y
CONFIG_DEFAULT_TCP_CONG="cubic"
# CONFIG_TCP_MD5SIG is not set
CONFIG_IPV6=m
# CONFIG_IPV6_PRIVACY is not set
# CONFIG_IPV6_ROUTER_PREF is not set
# CONFIG_IPV6_OPTIMISTIC_DAD is not set
# CONFIG_INET6_AH is not set
# CONFIG_INET6_ESP is not set
# CONFIG_INET6_IPCOMP is not set
# CONFIG_IPV6_MIP6 is not set
# CONFIG_INET6_XFRM_TUNNEL is not set
# CONFIG_INET6_TUNNEL is not set
CONFIG_INET6_XFRM_MODE_TRANSPORT=m
CONFIG_INET6_XFRM_MODE_TUNNEL=m
CONFIG_INET6_XFRM_MODE_BEET=m
# CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set
CONFIG_IPV6_SIT=m
# CONFIG_IPV6_SIT_6RD is not set
CONFIG_IPV6_NDISC_NODETYPE=y
# CONFIG_IPV6_TUNNEL is not set
# CONFIG_IPV6_MULTIPLE_TABLES is not set
# CONFIG_IPV6_MROUTE is not set
# CONFIG_NETLABEL is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
# CONFIG_NETFILTER is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IP_SCTP is not set
# CONFIG_RDS is not set
# CONFIG_TIPC is not set
# CONFIG_ATM is not set
# CONFIG_L2TP is not set
# CONFIG_BRIDGE is not set
# CONFIG_NET_DSA is not set
# CONFIG_VLAN_8021Q is not set
# CONFIG_DECNET is not set
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_ECONET is not set
# CONFIG_WAN_ROUTER is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set
# CONFIG_DNS_RESOLVER is not set
#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
# CONFIG_NET_TCPPROBE is not set
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
CONFIG_WIRELESS=y
# CONFIG_CFG80211 is not set
# CONFIG_LIB80211 is not set
#
# CFG80211 needs to be enabled for MAC80211
#
#
# Some wireless drivers require a rate control algorithm
#
# CONFIG_WIMAX is not set
# CONFIG_RFKILL is not set
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH=""
CONFIG_DEVTMPFS=y
CONFIG_DEVTMPFS_MOUNT=y
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
CONFIG_FIRMWARE_IN_KERNEL=y
CONFIG_EXTRA_FIRMWARE=""
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_DEBUG is not set
# CONFIG_MTD_TESTS is not set
CONFIG_MTD_CONCAT=y
CONFIG_MTD_PARTITIONS=y
# CONFIG_MTD_REDBOOT_PARTS is not set
CONFIG_MTD_CMDLINE_PARTS=y
# CONFIG_MTD_AFS_PARTS is not set
# CONFIG_MTD_AR7_PARTS is not set
#
# User Modules And Translation Layers
#
CONFIG_MTD_CHAR=y
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_SM_FTL is not set
# CONFIG_MTD_OOPS is not set
#
# RAM/ROM/Flash chip drivers
#
CONFIG_MTD_CFI=y
CONFIG_MTD_JEDECPROBE=y
CONFIG_MTD_GEN_PROBE=y
# CONFIG_MTD_CFI_ADV_OPTIONS is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
# CONFIG_MTD_CFI_INTELEXT is not set
CONFIG_MTD_CFI_AMDSTD=y
# CONFIG_MTD_CFI_STAA is not set
CONFIG_MTD_CFI_UTIL=y
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set
#
# Mapping drivers for chip access
#
# CONFIG_MTD_COMPLEX_MAPPINGS is not set
CONFIG_MTD_PHYSMAP=y
# CONFIG_MTD_PHYSMAP_COMPAT is not set
# CONFIG_MTD_ARM_INTEGRATOR is not set
# CONFIG_MTD_IMPA7 is not set
# CONFIG_MTD_INTEL_VR_NOR is not set
# CONFIG_MTD_PLATRAM is not set
#
# Self-contained MTD device drivers
#
# CONFIG_MTD_PMC551 is not set
# CONFIG_MTD_DATAFLASH is not set
CONFIG_MTD_M25P80=y
CONFIG_M25PXX_USE_FAST_READ=y
# CONFIG_MTD_SST25L is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set
#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOC2000 is not set
# CONFIG_MTD_DOC2001 is not set
# CONFIG_MTD_DOC2001PLUS is not set
CONFIG_MTD_NAND_ECC=y
# CONFIG_MTD_NAND_ECC_SMC is not set
CONFIG_MTD_NAND=y
CONFIG_MTD_NAND_VERIFY_WRITE=y
# CONFIG_MTD_SM_COMMON is not set
# CONFIG_MTD_NAND_MUSEUM_IDS is not set
# CONFIG_MTD_NAND_DENALI is not set
# CONFIG_MTD_NAND_GPIO is not set
CONFIG_MTD_NAND_OMAP2=y
# CONFIG_MTD_NAND_OMAP_PREFETCH is not set
CONFIG_MTD_NAND_IDS=y
# CONFIG_MTD_NAND_RICOH is not set
# CONFIG_MTD_NAND_DISKONCHIP is not set
# CONFIG_MTD_NAND_CAFE is not set
# CONFIG_MTD_NAND_NANDSIM is not set
# CONFIG_MTD_NAND_PLATFORM is not set
# CONFIG_MTD_ALAUDA is not set
# CONFIG_MTD_ONENAND is not set
#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set
# CONFIG_MTD_UBI is not set
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_CPQ_DA is not set
# CONFIG_BLK_CPQ_CISS_DA is not set
# CONFIG_BLK_DEV_DAC960 is not set
# CONFIG_BLK_DEV_UMEM is not set
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
#
# DRBD disabled because PROC_FS, INET or CONNECTOR not selected
#
# CONFIG_BLK_DEV_NBD is not set
# CONFIG_BLK_DEV_SX8 is not set
# CONFIG_BLK_DEV_UB is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=32768
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
# CONFIG_BLK_DEV_RBD is not set
CONFIG_MISC_DEVICES=y
# CONFIG_AD525X_DPOT is not set
# CONFIG_PHANTOM is not set
# CONFIG_SGI_IOC4 is not set
# CONFIG_TIFM_CORE is not set
# CONFIG_ICS932S401 is not set
# CONFIG_ENCLOSURE_SERVICES is not set
# CONFIG_HP_ILO is not set
# CONFIG_APDS9802ALS is not set
# CONFIG_ISL29003 is not set
# CONFIG_ISL29020 is not set
# CONFIG_SENSORS_TSL2550 is not set
# CONFIG_SENSORS_BH1780 is not set
# CONFIG_SENSORS_BH1770 is not set
# CONFIG_SENSORS_APDS990X is not set
# CONFIG_HMC6352 is not set
# CONFIG_DS1682 is not set
# CONFIG_TI_DAC7512 is not set
# CONFIG_BMP085 is not set
# CONFIG_PCH_PHUB is not set
# CONFIG_C2PORT is not set
#
# EEPROM support
#
CONFIG_EEPROM_AT24=y
# CONFIG_EEPROM_AT25 is not set
# CONFIG_EEPROM_LEGACY is not set
# CONFIG_EEPROM_MAX6875 is not set
# CONFIG_EEPROM_93CX6 is not set
# CONFIG_CB710_CORE is not set
# CONFIG_IWMC3200TOP is not set
#
# Texas Instruments shared transport line discipline
#
CONFIG_HAVE_IDE=y
# CONFIG_IDE is not set
#
# SCSI device support
#
CONFIG_SCSI_MOD=y
# CONFIG_RAID_ATTRS is not set
CONFIG_SCSI=y
CONFIG_SCSI_DMA=y
# CONFIG_SCSI_TGT is not set
# CONFIG_SCSI_NETLINK is not set
CONFIG_SCSI_PROC_FS=y
#
# SCSI support type (disk, tape, CD-ROM)
#
CONFIG_BLK_DEV_SD=y
# CONFIG_CHR_DEV_ST is not set
# CONFIG_CHR_DEV_OSST is not set
CONFIG_BLK_DEV_SR=y
CONFIG_BLK_DEV_SR_VENDOR=y
CONFIG_CHR_DEV_SG=y
# CONFIG_CHR_DEV_SCH is not set
# CONFIG_SCSI_MULTI_LUN is not set
# CONFIG_SCSI_CONSTANTS is not set
# CONFIG_SCSI_LOGGING is not set
# CONFIG_SCSI_SCAN_ASYNC is not set
CONFIG_SCSI_WAIT_SCAN=m
#
# SCSI Transports
#
# CONFIG_SCSI_SPI_ATTRS is not set
# CONFIG_SCSI_FC_ATTRS is not set
# CONFIG_SCSI_ISCSI_ATTRS is not set
# CONFIG_SCSI_SAS_ATTRS is not set
# CONFIG_SCSI_SAS_LIBSAS is not set
# CONFIG_SCSI_SRP_ATTRS is not set
# CONFIG_SCSI_LOWLEVEL is not set
# CONFIG_SCSI_DH is not set
# CONFIG_SCSI_OSD_INITIATOR is not set
CONFIG_ATA=y
# CONFIG_ATA_NONSTANDARD is not set
CONFIG_ATA_VERBOSE_ERROR=y
CONFIG_SATA_PMP=y
#
# Controllers with non-SFF native interface
#
CONFIG_SATA_AHCI=y
CONFIG_SATA_AHCI_PCI=y
CONFIG_SATA_AHCI_PLATFORM=y
# CONFIG_SATA_INIC162X is not set
# CONFIG_SATA_SIL24 is not set
# CONFIG_ATA_SFF is not set
# CONFIG_MD is not set
# CONFIG_FUSION is not set
#
# IEEE 1394 (FireWire) support
#
# CONFIG_FIREWIRE is not set
# CONFIG_FIREWIRE_NOSY is not set
# CONFIG_I2O is not set
CONFIG_NETDEVICES=y
# CONFIG_DUMMY is not set
# CONFIG_BONDING is not set
# CONFIG_MACVLAN is not set
# CONFIG_EQUALIZER is not set
# CONFIG_TUN is not set
# CONFIG_VETH is not set
# CONFIG_ARCNET is not set
# CONFIG_MII is not set
CONFIG_PHYLIB=y
#
# MII PHY device drivers
#
# CONFIG_MARVELL_PHY is not set
# CONFIG_DAVICOM_PHY is not set
# CONFIG_QSEMI_PHY is not set
# CONFIG_LXT_PHY is not set
# CONFIG_CICADA_PHY is not set
# CONFIG_VITESSE_PHY is not set
# CONFIG_SMSC_PHY is not set
# CONFIG_BROADCOM_PHY is not set
# CONFIG_BCM63XX_PHY is not set
# CONFIG_ICPLUS_PHY is not set
# CONFIG_REALTEK_PHY is not set
# CONFIG_NATIONAL_PHY is not set
# CONFIG_STE10XP is not set
# CONFIG_LSI_ET1011C_PHY is not set
# CONFIG_MICREL_PHY is not set
# CONFIG_FIXED_PHY is not set
# CONFIG_MDIO_BITBANG is not set
# CONFIG_NET_ETHERNET is not set
CONFIG_NETDEV_1000=y
# CONFIG_ACENIC is not set
# CONFIG_DL2K is not set
CONFIG_TI_DAVINCI_EMAC=y
# CONFIG_E1000 is not set
# CONFIG_E1000E is not set
# CONFIG_IP1000 is not set
# CONFIG_IGB is not set
# CONFIG_IGBVF is not set
# CONFIG_NS83820 is not set
# CONFIG_HAMACHI is not set
# CONFIG_YELLOWFIN is not set
# CONFIG_R8169 is not set
# CONFIG_SIS190 is not set
# CONFIG_SKGE is not set
# CONFIG_SKY2 is not set
# CONFIG_VIA_VELOCITY is not set
# CONFIG_TIGON3 is not set
# CONFIG_BNX2 is not set
# CONFIG_CNIC is not set
# CONFIG_QLA3XXX is not set
# CONFIG_ATL1 is not set
# CONFIG_ATL1E is not set
# CONFIG_ATL1C is not set
# CONFIG_JME is not set
# CONFIG_STMMAC_ETH is not set
# CONFIG_PCH_GBE is not set
# CONFIG_NETDEV_10000 is not set
# CONFIG_TR is not set
# CONFIG_WLAN is not set
#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
#
# USB Network Adapters
#
# CONFIG_USB_CATC is not set
# CONFIG_USB_KAWETH is not set
# CONFIG_USB_PEGASUS is not set
# CONFIG_USB_RTL8150 is not set
# CONFIG_USB_USBNET is not set
# CONFIG_USB_IPHETH is not set
# CONFIG_WAN is not set
#
# CAIF transport drivers
#
# CONFIG_FDDI is not set
# CONFIG_HIPPI is not set
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
# CONFIG_NET_FC is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
# CONFIG_VMXNET3 is not set
# CONFIG_ISDN is not set
# CONFIG_PHONE is not set
#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
# CONFIG_INPUT_POLLDEV is not set
# CONFIG_INPUT_SPARSEKMAP is not set
#
# Userland interfaces
#
CONFIG_INPUT_MOUSEDEV=y
# CONFIG_INPUT_MOUSEDEV_PSAUX is not set
CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
# CONFIG_INPUT_JOYDEV is not set
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set
#
# Input Device Drivers
#
# CONFIG_INPUT_KEYBOARD is not set
# CONFIG_INPUT_MOUSE is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
# CONFIG_INPUT_TOUCHSCREEN is not set
# CONFIG_INPUT_MISC is not set
#
# Hardware I/O ports
#
CONFIG_SERIO=y
CONFIG_SERIO_SERPORT=y
# CONFIG_SERIO_PCIPS2 is not set
# CONFIG_SERIO_RAW is not set
# CONFIG_SERIO_ALTERA_PS2 is not set
# CONFIG_SERIO_PS2MULT is not set
# CONFIG_GAMEPORT is not set
#
# Character devices
#
CONFIG_VT=y
CONFIG_CONSOLE_TRANSLATIONS=y
CONFIG_VT_CONSOLE=y
CONFIG_HW_CONSOLE=y
# CONFIG_VT_HW_CONSOLE_BINDING is not set
CONFIG_DEVKMEM=y
CONFIG_SERIAL_NONSTANDARD=y
# CONFIG_COMPUTONE is not set
# CONFIG_ROCKETPORT is not set
# CONFIG_CYCLADES is not set
# CONFIG_DIGIEPCA is not set
# CONFIG_MOXA_INTELLIO is not set
# CONFIG_MOXA_SMARTIO is not set
# CONFIG_ISI is not set
# CONFIG_SYNCLINKMP is not set
# CONFIG_SYNCLINK_GT is not set
# CONFIG_N_HDLC is not set
# CONFIG_N_GSM is not set
# CONFIG_RISCOM8 is not set
# CONFIG_SPECIALIX is not set
# CONFIG_STALDRV is not set
# CONFIG_NOZOMI is not set
#
# Serial drivers
#
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_PCI=y
CONFIG_SERIAL_8250_NR_UARTS=64
CONFIG_SERIAL_8250_RUNTIME_UARTS=4
CONFIG_SERIAL_8250_EXTENDED=y
# CONFIG_SERIAL_8250_MANY_PORTS is not set
CONFIG_SERIAL_8250_SHARE_IRQ=y
CONFIG_SERIAL_8250_DETECT_IRQ=y
CONFIG_SERIAL_8250_RSA=y
#
# Non-8250 serial port support
#
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_MAX3107 is not set
# CONFIG_SERIAL_MFD_HSU is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
# CONFIG_SERIAL_JSM is not set
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
# CONFIG_SERIAL_TIMBERDALE is not set
# CONFIG_SERIAL_ALTERA_JTAGUART is not set
# CONFIG_SERIAL_ALTERA_UART is not set
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
# CONFIG_LEGACY_PTYS is not set
# CONFIG_IPMI_HANDLER is not set
# CONFIG_HW_RANDOM is not set
# CONFIG_R3964 is not set
# CONFIG_APPLICOM is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
CONFIG_DEVPORT=y
# CONFIG_TI81XX_HDMI is not set
# CONFIG_TI816X_PCIE_BOOTDRV is not set
# CONFIG_RAMOOPS is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
CONFIG_I2C_COMPAT=y
CONFIG_I2C_CHARDEV=y
# CONFIG_I2C_MUX is not set
CONFIG_I2C_HELPER_AUTO=y
#
# I2C Hardware Bus support
#
#
# PC SMBus host controller drivers
#
# CONFIG_I2C_ALI1535 is not set
# CONFIG_I2C_ALI1563 is not set
# CONFIG_I2C_ALI15X3 is not set
# CONFIG_I2C_AMD756 is not set
# CONFIG_I2C_AMD8111 is not set
# CONFIG_I2C_I801 is not set
# CONFIG_I2C_ISCH is not set
# CONFIG_I2C_PIIX4 is not set
# CONFIG_I2C_NFORCE2 is not set
# CONFIG_I2C_SIS5595 is not set
# CONFIG_I2C_SIS630 is not set
# CONFIG_I2C_SIS96X is not set
# CONFIG_I2C_VIA is not set
# CONFIG_I2C_VIAPRO is not set
#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_DESIGNWARE is not set
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_INTEL_MID is not set
# CONFIG_I2C_OCORES is not set
CONFIG_I2C_OMAP=y
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_SIMTEC is not set
# CONFIG_I2C_XILINX is not set
#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set
# CONFIG_I2C_TINY_USB is not set
#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_STUB is not set
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
#
# SPI Master Controller Drivers
#
# CONFIG_SPI_BITBANG is not set
# CONFIG_SPI_GPIO is not set
CONFIG_SPI_OMAP24XX=y
# CONFIG_SPI_TOPCLIFF_PCH is not set
# CONFIG_SPI_XILINX is not set
# CONFIG_SPI_DESIGNWARE is not set
#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
#
# PPS support
#
# CONFIG_PPS is not set
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIOLIB=y
# CONFIG_DEBUG_GPIO is not set
# CONFIG_GPIO_SYSFS is not set
#
# Memory mapped GPIO expanders:
#
# CONFIG_GPIO_BASIC_MMIO is not set
# CONFIG_GPIO_IT8761E is not set
# CONFIG_GPIO_SCH is not set
# CONFIG_GPIO_VX855 is not set
#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX7300 is not set
# CONFIG_GPIO_MAX732X is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_GPIO_PCF857X is not set
# CONFIG_GPIO_SX150X is not set
# CONFIG_GPIO_ADP5588 is not set
#
# PCI GPIO expanders:
#
# CONFIG_GPIO_CS5535 is not set
# CONFIG_GPIO_BT8XX is not set
# CONFIG_GPIO_LANGWELL is not set
# CONFIG_GPIO_PCH is not set
# CONFIG_GPIO_RDC321X is not set
#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_GPIO_MC33880 is not set
# CONFIG_GPIO_74X164 is not set
#
# AC97 GPIO expanders:
#
#
# MODULbus GPIO expanders:
#
# CONFIG_W1 is not set
# CONFIG_POWER_SUPPLY is not set
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
CONFIG_WATCHDOG=y
# CONFIG_WATCHDOG_NOWAYOUT is not set
#
# Watchdog Device Drivers
#
# CONFIG_SOFT_WATCHDOG is not set
CONFIG_OMAP_WATCHDOG=y
# CONFIG_MAX63XX_WATCHDOG is not set
# CONFIG_ALIM7101_WDT is not set
#
# PCI-based Watchdog Cards
#
# CONFIG_PCIPCWATCHDOG is not set
# CONFIG_WDTPCI is not set
#
# USB-based Watchdog Cards
#
# CONFIG_USBPCWATCHDOG is not set
CONFIG_SSB_POSSIBLE=y
#
# Sonics Silicon Backplane
#
CONFIG_SSB=m
CONFIG_SSB_SPROM=y
CONFIG_SSB_PCIHOST_POSSIBLE=y
CONFIG_SSB_PCIHOST=y
# CONFIG_SSB_B43_PCI_BRIDGE is not set
CONFIG_SSB_SDIOHOST_POSSIBLE=y
# CONFIG_SSB_SDIOHOST is not set
# CONFIG_SSB_DEBUG is not set
CONFIG_SSB_DRIVER_PCICORE_POSSIBLE=y
# CONFIG_SSB_DRIVER_PCICORE is not set
# CONFIG_MFD_SUPPORT is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
CONFIG_REGULATOR_DUMMY=y
# CONFIG_REGULATOR_FIXED_VOLTAGE is not set
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
# CONFIG_REGULATOR_BQ24022 is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_MAX8649 is not set
# CONFIG_REGULATOR_MAX8660 is not set
# CONFIG_REGULATOR_MAX8952 is not set
# CONFIG_REGULATOR_LP3971 is not set
# CONFIG_REGULATOR_LP3972 is not set
# CONFIG_REGULATOR_TPS65023 is not set
# CONFIG_REGULATOR_TPS6507X is not set
# CONFIG_REGULATOR_ISL6271A is not set
# CONFIG_REGULATOR_AD5398 is not set
# CONFIG_MEDIA_SUPPORT is not set
#
# Graphics support
#
CONFIG_VGA_ARB=y
CONFIG_VGA_ARB_MAX_GPUS=16
# CONFIG_DRM is not set
# CONFIG_STUB_POULSBO is not set
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
CONFIG_FB=y
# CONFIG_FIRMWARE_EDID is not set
# CONFIG_FB_DDC is not set
# CONFIG_FB_BOOT_VESA_SUPPORT is not set
CONFIG_FB_CFB_FILLRECT=y
CONFIG_FB_CFB_COPYAREA=y
CONFIG_FB_CFB_IMAGEBLIT=y
# CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
# CONFIG_FB_SYS_FILLRECT is not set
# CONFIG_FB_SYS_COPYAREA is not set
# CONFIG_FB_SYS_IMAGEBLIT is not set
# CONFIG_FB_FOREIGN_ENDIAN is not set
# CONFIG_FB_SYS_FOPS is not set
# CONFIG_FB_SVGALIB is not set
# CONFIG_FB_MACMODES is not set
# CONFIG_FB_BACKLIGHT is not set
# CONFIG_FB_MODE_HELPERS is not set
# CONFIG_FB_TILEBLITTING is not set
#
# Frame buffer hardware drivers
#
# CONFIG_FB_CIRRUS is not set
# CONFIG_FB_PM2 is not set
# CONFIG_FB_CYBER2000 is not set
# CONFIG_FB_ASILIANT is not set
# CONFIG_FB_IMSTT is not set
# CONFIG_FB_S1D13XXX is not set
# CONFIG_FB_NVIDIA is not set
# CONFIG_FB_RIVA is not set
# CONFIG_FB_MATROX is not set
# CONFIG_FB_RADEON is not set
# CONFIG_FB_ATY128 is not set
# CONFIG_FB_ATY is not set
# CONFIG_FB_S3 is not set
# CONFIG_FB_SAVAGE is not set
# CONFIG_FB_SIS is not set
# CONFIG_FB_NEOMAGIC is not set
# CONFIG_FB_KYRO is not set
# CONFIG_FB_3DFX is not set
# CONFIG_FB_VOODOO1 is not set
# CONFIG_FB_VT8623 is not set
# CONFIG_FB_TRIDENT is not set
# CONFIG_FB_ARK is not set
# CONFIG_FB_PM3 is not set
# CONFIG_FB_CARMINE is not set
# CONFIG_FB_VIRTUAL is not set
# CONFIG_FB_METRONOME is not set
# CONFIG_FB_MB862XX is not set
# CONFIG_FB_BROADSHEET is not set
# CONFIG_FB_OMAP is not set
# CONFIG_TI81XX_VPSS is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set
#
# Display device support
#
# CONFIG_DISPLAY_SUPPORT is not set
#
# Console display driver support
#
CONFIG_DUMMY_CONSOLE=y
# CONFIG_FRAMEBUFFER_CONSOLE is not set
# CONFIG_LOGO is not set
CONFIG_SOUND=y
# CONFIG_SOUND_OSS_CORE is not set
CONFIG_SND=y
CONFIG_SND_TIMER=y
CONFIG_SND_PCM=y
CONFIG_SND_HWDEP=y
CONFIG_SND_RAWMIDI=y
CONFIG_SND_JACK=y
# CONFIG_SND_SEQUENCER is not set
# CONFIG_SND_MIXER_OSS is not set
# CONFIG_SND_PCM_OSS is not set
# CONFIG_SND_DYNAMIC_MINORS is not set
CONFIG_SND_SUPPORT_OLD_API=y
CONFIG_SND_VERBOSE_PROCFS=y
# CONFIG_SND_VERBOSE_PRINTK is not set
# CONFIG_SND_DEBUG is not set
# CONFIG_SND_RAWMIDI_SEQ is not set
# CONFIG_SND_OPL3_LIB_SEQ is not set
# CONFIG_SND_OPL4_LIB_SEQ is not set
# CONFIG_SND_SBAWE_SEQ is not set
# CONFIG_SND_EMU10K1_SEQ is not set
# CONFIG_SND_DRIVERS is not set
CONFIG_SND_PCI=y
# CONFIG_SND_AD1889 is not set
# CONFIG_SND_ALS300 is not set
# CONFIG_SND_ALI5451 is not set
# CONFIG_SND_ATIIXP is not set
# CONFIG_SND_ATIIXP_MODEM is not set
# CONFIG_SND_AU8810 is not set
# CONFIG_SND_AU8820 is not set
# CONFIG_SND_AU8830 is not set
# CONFIG_SND_AW2 is not set
# CONFIG_SND_AZT3328 is not set
# CONFIG_SND_BT87X is not set
# CONFIG_SND_CA0106 is not set
# CONFIG_SND_CMIPCI is not set
# CONFIG_SND_OXYGEN is not set
# CONFIG_SND_CS4281 is not set
# CONFIG_SND_CS46XX is not set
# CONFIG_SND_CS5535AUDIO is not set
# CONFIG_SND_CTXFI is not set
# CONFIG_SND_DARLA20 is not set
# CONFIG_SND_GINA20 is not set
# CONFIG_SND_LAYLA20 is not set
# CONFIG_SND_DARLA24 is not set
# CONFIG_SND_GINA24 is not set
# CONFIG_SND_LAYLA24 is not set
# CONFIG_SND_MONA is not set
# CONFIG_SND_MIA is not set
# CONFIG_SND_ECHO3G is not set
# CONFIG_SND_INDIGO is not set
# CONFIG_SND_INDIGOIO is not set
# CONFIG_SND_INDIGODJ is not set
# CONFIG_SND_INDIGOIOX is not set
# CONFIG_SND_INDIGODJX is not set
# CONFIG_SND_EMU10K1 is not set
# CONFIG_SND_EMU10K1X is not set
# CONFIG_SND_ENS1370 is not set
# CONFIG_SND_ENS1371 is not set
# CONFIG_SND_ES1938 is not set
# CONFIG_SND_ES1968 is not set
# CONFIG_SND_FM801 is not set
# CONFIG_SND_HDA_INTEL is not set
# CONFIG_SND_HDSP is not set
# CONFIG_SND_HDSPM is not set
# CONFIG_SND_HIFIER is not set
# CONFIG_SND_ICE1712 is not set
# CONFIG_SND_ICE1724 is not set
# CONFIG_SND_INTEL8X0 is not set
# CONFIG_SND_INTEL8X0M is not set
# CONFIG_SND_KORG1212 is not set
# CONFIG_SND_LX6464ES is not set
# CONFIG_SND_MAESTRO3 is not set
# CONFIG_SND_MIXART is not set
# CONFIG_SND_NM256 is not set
# CONFIG_SND_PCXHR is not set
# CONFIG_SND_RIPTIDE is not set
# CONFIG_SND_RME32 is not set
# CONFIG_SND_RME96 is not set
# CONFIG_SND_RME9652 is not set
# CONFIG_SND_SONICVIBES is not set
# CONFIG_SND_TRIDENT is not set
# CONFIG_SND_VIA82XX is not set
# CONFIG_SND_VIA82XX_MODEM is not set
# CONFIG_SND_VIRTUOSO is not set
# CONFIG_SND_VX222 is not set
# CONFIG_SND_YMFPCI is not set
# CONFIG_SND_ARM is not set
# CONFIG_SND_SPI is not set
CONFIG_SND_USB=y
CONFIG_SND_USB_AUDIO=y
# CONFIG_SND_USB_UA101 is not set
# CONFIG_SND_USB_CAIAQ is not set
CONFIG_SND_SOC=y
CONFIG_SND_TI81XX_SOC=y
CONFIG_SND_DAVINCI_SOC_MCASP=y
CONFIG_SND_TI81XX_SOC_EVM=y
# CONFIG_SND_OMAP_SOC is not set
CONFIG_SND_SOC_I2C_AND_SPI=y
# CONFIG_SND_SOC_ALL_CODECS is not set
CONFIG_SND_SOC_TLV320AIC3X=y
# CONFIG_SOUND_PRIME is not set
CONFIG_HID_SUPPORT=y
CONFIG_HID=y
# CONFIG_HIDRAW is not set
#
# USB Input Devices
#
CONFIG_USB_HID=y
# CONFIG_HID_PID is not set
# CONFIG_USB_HIDDEV is not set
#
# Special HID drivers
#
# CONFIG_HID_3M_PCT is not set
CONFIG_HID_A4TECH=y
# CONFIG_HID_ACRUX_FF is not set
CONFIG_HID_APPLE=y
CONFIG_HID_BELKIN=y
# CONFIG_HID_CANDO is not set
CONFIG_HID_CHERRY=y
CONFIG_HID_CHICONY=y
# CONFIG_HID_PRODIKEYS is not set
CONFIG_HID_CYPRESS=y
# CONFIG_HID_DRAGONRISE is not set
# CONFIG_HID_EGALAX is not set
CONFIG_HID_EZKEY=y
CONFIG_HID_KYE=y
# CONFIG_HID_UCLOGIC is not set
# CONFIG_HID_WALTOP is not set
# CONFIG_HID_GYRATION is not set
# CONFIG_HID_TWINHAN is not set
CONFIG_HID_KENSINGTON=y
CONFIG_HID_LOGITECH=y
# CONFIG_LOGITECH_FF is not set
# CONFIG_LOGIRUMBLEPAD2_FF is not set
# CONFIG_LOGIG940_FF is not set
# CONFIG_LOGIWII_FF is not set
CONFIG_HID_MICROSOFT=y
# CONFIG_HID_MOSART is not set
CONFIG_HID_MONTEREY=y
# CONFIG_HID_NTRIG is not set
# CONFIG_HID_ORTEK is not set
# CONFIG_HID_PANTHERLORD is not set
# CONFIG_HID_PETALYNX is not set
# CONFIG_HID_PICOLCD is not set
# CONFIG_HID_QUANTA is not set
# CONFIG_HID_ROCCAT is not set
# CONFIG_HID_ROCCAT_KONE is not set
# CONFIG_HID_ROCCAT_PYRA is not set
# CONFIG_HID_SAMSUNG is not set
# CONFIG_HID_SONY is not set
# CONFIG_HID_STANTUM is not set
# CONFIG_HID_SUNPLUS is not set
# CONFIG_HID_GREENASIA is not set
# CONFIG_HID_SMARTJOYPLUS is not set
# CONFIG_HID_TOPSEED is not set
# CONFIG_HID_THRUSTMASTER is not set
# CONFIG_HID_ZEROPLUS is not set
# CONFIG_HID_ZYDACRON is not set
CONFIG_USB_SUPPORT=y
CONFIG_USB_ARCH_HAS_HCD=y
CONFIG_USB_ARCH_HAS_OHCI=y
CONFIG_USB_ARCH_HAS_EHCI=y
CONFIG_USB=y
# CONFIG_USB_DEBUG is not set
# CONFIG_USB_ANNOUNCE_NEW_DEVICES is not set
#
# Miscellaneous USB options
#
# CONFIG_USB_DEVICEFS is not set
# CONFIG_USB_DEVICE_CLASS is not set
# CONFIG_USB_DYNAMIC_MINORS is not set
# CONFIG_USB_SUSPEND is not set
# CONFIG_USB_MON is not set
# CONFIG_USB_WUSB is not set
# CONFIG_USB_WUSB_CBAF is not set
#
# USB Host Controller Drivers
#
# CONFIG_USB_C67X00_HCD is not set
# CONFIG_USB_XHCI_HCD is not set
# CONFIG_USB_EHCI_HCD is not set
# CONFIG_USB_OXU210HP_HCD is not set
# CONFIG_USB_ISP116X_HCD is not set
# CONFIG_USB_ISP1760_HCD is not set
# CONFIG_USB_ISP1362_HCD is not set
# CONFIG_USB_OHCI_HCD is not set
# CONFIG_USB_UHCI_HCD is not set
# CONFIG_USB_SL811_HCD is not set
# CONFIG_USB_R8A66597_HCD is not set
# CONFIG_USB_WHCI_HCD is not set
# CONFIG_USB_HWA_HCD is not set
CONFIG_USB_MUSB_HDRC=y
# CONFIG_USB_MUSB_OMAP2PLUS is not set
# CONFIG_USB_MUSB_AM35X is not set
CONFIG_USB_MUSB_TI81XX=y
# CONFIG_USB_TUSB6010 is not set
CONFIG_USB_MUSB_HOST=y
CONFIG_USB_MUSB_HDRC_HCD=y
# CONFIG_MUSB_PIO_ONLY is not set
# CONFIG_USB_TI_CPPI_DMA is not set
CONFIG_USB_TI_CPPI41_DMA=y
CONFIG_USB_MUSB_DEBUG=y
#
# USB Device Class drivers
#
# CONFIG_USB_ACM is not set
# CONFIG_USB_PRINTER is not set
# CONFIG_USB_WDM is not set
# CONFIG_USB_TMC is not set
#
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
#
#
# also be needed; see USB_STORAGE Help for more info
#
CONFIG_USB_STORAGE=y
# CONFIG_USB_STORAGE_DEBUG is not set
# CONFIG_USB_STORAGE_DATAFAB is not set
# CONFIG_USB_STORAGE_FREECOM is not set
# CONFIG_USB_STORAGE_ISD200 is not set
# CONFIG_USB_STORAGE_USBAT is not set
# CONFIG_USB_STORAGE_SDDR09 is not set
# CONFIG_USB_STORAGE_SDDR55 is not set
# CONFIG_USB_STORAGE_JUMPSHOT is not set
# CONFIG_USB_STORAGE_ALAUDA is not set
# CONFIG_USB_STORAGE_ONETOUCH is not set
# CONFIG_USB_STORAGE_KARMA is not set
# CONFIG_USB_STORAGE_CYPRESS_ATACB is not set
# CONFIG_USB_UAS is not set
# CONFIG_USB_LIBUSUAL is not set
#
# USB Imaging devices
#
# CONFIG_USB_MDC800 is not set
# CONFIG_USB_MICROTEK is not set
#
# USB port drivers
#
# CONFIG_USB_SERIAL is not set
#
# USB Miscellaneous drivers
#
# CONFIG_USB_EMI62 is not set
# CONFIG_USB_EMI26 is not set
# CONFIG_USB_ADUTUX is not set
# CONFIG_USB_SEVSEG is not set
# CONFIG_USB_RIO500 is not set
# CONFIG_USB_LEGOTOWER is not set
# CONFIG_USB_LCD is not set
# CONFIG_USB_LED is not set
# CONFIG_USB_CYPRESS_CY7C63 is not set
# CONFIG_USB_CYTHERM is not set
# CONFIG_USB_IDMOUSE is not set
# CONFIG_USB_FTDI_ELAN is not set
# CONFIG_USB_APPLEDISPLAY is not set
# CONFIG_USB_SISUSBVGA is not set
# CONFIG_USB_LD is not set
# CONFIG_USB_TRANCEVIBRATOR is not set
# CONFIG_USB_IOWARRIOR is not set
# CONFIG_USB_TEST is not set
# CONFIG_USB_ISIGHTFW is not set
# CONFIG_USB_YUREX is not set
# CONFIG_USB_GADGET is not set
#
# OTG and related infrastructure
#
CONFIG_USB_OTG_UTILS=y
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_USB_ULPI is not set
CONFIG_NOP_USB_XCEIV=y
# CONFIG_UWB is not set
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
# CONFIG_MMC_UNSAFE_RESUME is not set
#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_MINORS=8
CONFIG_MMC_BLOCK_BOUNCE=y
# CONFIG_SDIO_UART is not set
# CONFIG_MMC_TEST is not set
#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_OMAP is not set
CONFIG_MMC_OMAP_HS=y
# CONFIG_MMC_TIFM_SD is not set
# CONFIG_MMC_SPI is not set
# CONFIG_MMC_CB710 is not set
# CONFIG_MMC_VIA_SDMMC is not set
# CONFIG_MMC_USHC is not set
# CONFIG_MEMSTICK is not set
# CONFIG_NEW_LEDS is not set
# CONFIG_ACCESSIBILITY is not set
# CONFIG_INFINIBAND is not set
CONFIG_RTC_LIB=y
# CONFIG_RTC_CLASS is not set
# CONFIG_DMADEVICES is not set
# CONFIG_AUXDISPLAY is not set
# CONFIG_UIO is not set
# CONFIG_STAGING is not set
#
# File systems
#
CONFIG_EXT2_FS=y
CONFIG_EXT2_FS_XATTR=y
CONFIG_EXT2_FS_POSIX_ACL=y
CONFIG_EXT2_FS_SECURITY=y
# CONFIG_EXT2_FS_XIP is not set
CONFIG_EXT3_FS=y
# CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
CONFIG_EXT3_FS_XATTR=y
CONFIG_EXT3_FS_POSIX_ACL=y
CONFIG_EXT3_FS_SECURITY=y
# CONFIG_EXT4_FS is not set
CONFIG_JBD=y
# CONFIG_JBD_DEBUG is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
CONFIG_FS_POSIX_ACL=y
# CONFIG_XFS_FS is not set
# CONFIG_OCFS2_FS is not set
# CONFIG_BTRFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_FILE_LOCKING=y
# CONFIG_FSNOTIFY is not set
# CONFIG_DNOTIFY is not set
# CONFIG_INOTIFY_USER is not set
# CONFIG_FANOTIFY is not set
# CONFIG_QUOTA is not set
# CONFIG_QUOTACTL is not set
# CONFIG_AUTOFS4_FS is not set
# CONFIG_FUSE_FS is not set
#
# Caches
#
# CONFIG_FSCACHE is not set
#
# CD-ROM/DVD Filesystems
#
# CONFIG_ISO9660_FS is not set
# CONFIG_UDF_FS is not set
#
# DOS/FAT/NT Filesystems
#
CONFIG_FAT_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_FAT_DEFAULT_CODEPAGE=437
CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
# CONFIG_NTFS_FS is not set
#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
# CONFIG_TMPFS_POSIX_ACL is not set
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_ECRYPT_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
CONFIG_JFFS2_FS=y
CONFIG_JFFS2_FS_DEBUG=0
CONFIG_JFFS2_FS_WRITEBUFFER=y
CONFIG_JFFS2_FS_WBUF_VERIFY=y
# CONFIG_JFFS2_SUMMARY is not set
# CONFIG_JFFS2_FS_XATTR is not set
# CONFIG_JFFS2_COMPRESSION_OPTIONS is not set
CONFIG_JFFS2_ZLIB=y
# CONFIG_JFFS2_LZO is not set
CONFIG_JFFS2_RTIME=y
# CONFIG_JFFS2_RUBIN is not set
# CONFIG_LOGFS is not set
# CONFIG_CRAMFS is not set
CONFIG_SQUASHFS=y
# CONFIG_SQUASHFS_XATTR is not set
# CONFIG_SQUASHFS_LZO is not set
# CONFIG_SQUASHFS_EMBEDDED is not set
CONFIG_SQUASHFS_FRAGMENT_CACHE_SIZE=3
# CONFIG_VXFS_FS is not set
CONFIG_MINI_FO=y
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
CONFIG_NETWORK_FILESYSTEMS=y
CONFIG_NFS_FS=y
CONFIG_NFS_V3=y
# CONFIG_NFS_V3_ACL is not set
# CONFIG_NFS_V4 is not set
CONFIG_ROOT_NFS=y
# CONFIG_NFSD is not set
CONFIG_LOCKD=y
CONFIG_LOCKD_V4=y
CONFIG_NFS_COMMON=y
CONFIG_SUNRPC=y
# CONFIG_RPCSEC_GSS_KRB5 is not set
# CONFIG_CEPH_FS is not set
# CONFIG_CIFS is not set
# CONFIG_NCP_FS is not set
# CONFIG_CODA_FS is not set
# CONFIG_AFS_FS is not set
#
# Partition Types
#
# CONFIG_PARTITION_ADVANCED is not set
CONFIG_MSDOS_PARTITION=y
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="utf8"
CONFIG_NLS_CODEPAGE_437=y
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
CONFIG_NLS_ASCII=y
CONFIG_NLS_ISO8859_1=y
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
CONFIG_NLS_UTF8=y
# CONFIG_DLM is not set
#
# Kernel hacking
#
# CONFIG_PRINTK_TIME is not set
CONFIG_ENABLE_WARN_DEPRECATED=y
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
# CONFIG_MAGIC_SYSRQ is not set
# CONFIG_STRIP_ASM_SYMS is not set
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
CONFIG_DEBUG_KERNEL=y
# CONFIG_DEBUG_SHIRQ is not set
# CONFIG_LOCKUP_DETECTOR is not set
# CONFIG_HARDLOCKUP_DETECTOR is not set
# CONFIG_DETECT_HUNG_TASK is not set
# CONFIG_SCHED_DEBUG is not set
# CONFIG_SCHEDSTATS is not set
# CONFIG_TIMER_STATS is not set
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_SLUB_DEBUG_ON is not set
# CONFIG_SLUB_STATS is not set
# CONFIG_DEBUG_KMEMLEAK is not set
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
# CONFIG_DEBUG_SPINLOCK is not set
# CONFIG_DEBUG_MUTEXES is not set
CONFIG_BKL=y
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_SPARSE_RCU_POINTER is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_SPINLOCK_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
# CONFIG_DEBUG_KOBJECT is not set
CONFIG_DEBUG_BUGVERBOSE=y
# CONFIG_DEBUG_INFO is not set
# CONFIG_DEBUG_VM is not set
# CONFIG_DEBUG_WRITECOUNT is not set
CONFIG_DEBUG_MEMORY_INIT=y
# CONFIG_DEBUG_LIST is not set
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_DEBUG_CREDENTIALS is not set
CONFIG_FRAME_POINTER=y
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_KPROBES_SANITY_TEST is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# CONFIG_LKDTM is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
# CONFIG_SYSCTL_SYSCALL_CHECK is not set
# CONFIG_PAGE_POISONING is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
# CONFIG_DYNAMIC_DEBUG is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
# CONFIG_STRICT_DEVMEM is not set
# CONFIG_ARM_UNWIND is not set
# CONFIG_DEBUG_USER is not set
# CONFIG_DEBUG_ERRORS is not set
# CONFIG_DEBUG_STACK_USAGE is not set
CONFIG_DEBUG_LL=y
CONFIG_EARLY_PRINTK=y
# CONFIG_DEBUG_ICEDCC is not set
# CONFIG_OC_ETM is not set
#
# Security options
#
CONFIG_KEYS=y
CONFIG_KEYS_DEBUG_PROC_KEYS=y
# CONFIG_SECURITY_DMESG_RESTRICT is not set
CONFIG_SECURITY=y
# CONFIG_SECURITYFS is not set
CONFIG_SECURITY_NETWORK=y
# CONFIG_SECURITY_NETWORK_XFRM is not set
# CONFIG_SECURITY_PATH is not set
# CONFIG_SECURITY_TOMOYO is not set
# CONFIG_SECURITY_APPARMOR is not set
# CONFIG_IMA is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
# CONFIG_CRYPTO_MANAGER is not set
# CONFIG_CRYPTO_MANAGER2 is not set
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
# CONFIG_CRYPTO_TEST is not set
#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set
#
# Block modes
#
# CONFIG_CRYPTO_CBC is not set
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
# CONFIG_CRYPTO_ECB is not set
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set
#
# Hash modes
#
# CONFIG_CRYPTO_HMAC is not set
# CONFIG_CRYPTO_XCBC is not set
# CONFIG_CRYPTO_VMAC is not set
#
# Digest
#
# CONFIG_CRYPTO_CRC32C is not set
# CONFIG_CRYPTO_GHASH is not set
# CONFIG_CRYPTO_MD4 is not set
# CONFIG_CRYPTO_MD5 is not set
# CONFIG_CRYPTO_MICHAEL_MIC is not set
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
# CONFIG_CRYPTO_SHA1 is not set
# CONFIG_CRYPTO_SHA256 is not set
# CONFIG_CRYPTO_SHA512 is not set
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set
#
# Ciphers
#
# CONFIG_CRYPTO_AES is not set
# CONFIG_CRYPTO_ANUBIS is not set
# CONFIG_CRYPTO_ARC4 is not set
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
# CONFIG_CRYPTO_DES is not set
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set
#
# Compression
#
# CONFIG_CRYPTO_DEFLATE is not set
# CONFIG_CRYPTO_ZLIB is not set
# CONFIG_CRYPTO_LZO is not set
#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
# CONFIG_CRYPTO_HW is not set
# CONFIG_BINARY_PRINTF is not set
#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_FIND_LAST_BIT=y
# CONFIG_CRC_CCITT is not set
# CONFIG_CRC16 is not set
# CONFIG_CRC_T10DIF is not set
# CONFIG_CRC_ITU_T is not set
CONFIG_CRC32=y
# CONFIG_CRC7 is not set
# CONFIG_LIBCRC32C is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_ZLIB_DEFLATE=y
CONFIG_LZO_DECOMPRESS=y
CONFIG_DECOMPRESS_GZIP=y
CONFIG_DECOMPRESS_BZIP2=y
CONFIG_DECOMPRESS_LZMA=y
CONFIG_DECOMPRESS_LZO=y
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_NLATTR=y
Here is my u-boot env:
TI8168_EVM#printenv
bootdelay=3
baudrate=115200
verify=yes
bootfile=uImage
ramdisk_file=ramdisk.gz
loadaddr=0x81000000
script_addr=0x80900000
bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${script_addr}
ethact=DaVinci EMAC
machid=af0
autoload=yes
ethaddr=ff:ff:ff:04:24:69
bootcmd=bootm 0x08060000
filesize=1409C40
fileaddr=81000000
netmask=255.255.255.0
ipaddr=192.168.1.1
serverip=192.168.1.5
bootargs=console=ttyO2,115200n8 root=/dev/mtdblock3 rw rootfstype=jffs2 mem=100M earlyprintk
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2010.06 (May 03 2011 - 14:52:47)
Switch settings on the board are:
SW3:
switch 5 & 8 on the rest off
SW4:
all off
SW1 (on daughter card):
switch 1 & 2 on, 3 & 4 off
Regards,
Brian