This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ways to reduce power during cpu idle? OMAP-l138

So we first only had the wait for interupt impletemented but that didn't seem to reduce power usage at, so we lowered the clock and voltage on our platform to 1.0v and 100mhz for the core. Out of 2.5 mA previously being used total, it dropped it a whole .1 to .2 mA. I was wondering if there was anything else that can be done to get better results, this is just while the CPU is idle...

I don't actually know the % of the 2.5mA that the cpu is actually using, I havn't discovered how to test those yet, so I don't actually know how much it was actually reduced,