Part Number: TMS320C6416T
Hello all,
I have dev board with TMS320C6416t, emulator XDS100 v3, jtag connection test is fine, but when I run the debugger I get the error:
Error connecting to the target: (Error -1004 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172)
Here is the schematic jtag which i used

I followed this pattern

I use CCS Version: 11.1.0.00011