Hi expert.
about mcu1_0 domain internal SRAM ECC function,i have follwing 2 questions:
1).after power reset, Is the ECC function enabled automatically by hardware itself or not ?
2). for external DDR,if enable ECC,some cell shall be used as ECC and the usable size shall < DDR physical size.
what about internal SRAM?
the SRAM size is 1M, if ECC enabled, the size isl 1M or some cells are used as ECC area ,then,the usage size < 1M?