Hi,
Good day.
Our customer has the below question regarding the TMS320C6726 with a Blackhawk 560v2USB. Can you please help us?
I am currently trying to connect to a TMS320C6726 with a Blackhawk 560v2USB probe but the version of CCS I'm using doesn't seem to support that combination. Can you tell me what version of CCS I should be using? foreither Linux or Windows
Can't give you a screenshot but I am using CCS v10.3.1.00003 on Linux and also on Windows. The problem is when I try (either automatically or manually) CCS doesn't recognize the TMS chip in conjunction with the Blackhawk probe I'm using but it seems to want an older version of the Blackhawk (510L or 510W I think). So, is the TMS320c6726 no longer supported in CCS10 and should I try an older version? if so, which one?
BTW I think all drivers have been installed but just in case, how do I verify that the necessary drivers are installed?
Regards,
Cedrick