Hi Team
We refer to the Processor SDK Linux for AM64. For better visibility of the boot process, we want to provide a console on our custom board for both, the R5F and the A53 boot core. On the SK-AM64, the boot console of the A53 boot core is connected with UART0. We presume that there is also a default serial interface where the R5F boot core is connected with. Could you please tell us which serial interface this is ?