I have a customer asking the following question. I was not able to find the answer in the TI datasheet.
It appears that I have inadverntantly left GIO81 (OSCCFG) floating in our design. Since this is used at start-up as the oscillator config input, can you tell me what the possible consequences are of leaving this floating instead of pulling up or down? Will it choose one or the other (15-35MHz or 30-40MHz mode) based on the floating value? And if it chooses the wrong state, what happens?