Hello,
Does the TDA3 support processing YUV422 10-bit on Vision SDK 3.06? Only the 8 MSBs are being used. The hardware setup involves an image sensor sending a UB933 parallel data, which is sent to a UB960 on the TDA3 over CSI-2.
Currently, an image is being processed and displayed, but the colors look completely wrong. After manually repacking the bits to conform to YUV422 8-bit, I was able to get a reasonably good image in other image viewers, such as OpenCV. Ideally, we would prefer to do this in realtime.
Thank you,
Stefen Sharkey