This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 CSL - procedure to submit patches?

Hi

 

I am using the C6747 CSL that comes with the BIOSPSP 1.30.01.

I am writing code to program the PLL.  I would like to program the OCSEL regsiter so I can change the default clock output on the OBSCLK pin.  This regsiter is not current supported in the CSL:

typedef struct  {
    volatile Uint32 REVID;
    volatile Uint8 RSVD0[224];
    volatile Uint32 RSTYPE;
    volatile Uint8 RSVD1[24];
    volatile Uint32 PLLCTL;
    volatile Uint8 RSVD2[12]; <--------------------------- OSSEL should be here
    volatile Uint32 PLLM;
    volatile Uint32 PREDIV;
    volatile Uint32 PLLDIV1;
    volatile Uint32 PLLDIV2;
    volatile Uint32 PLLDIV3;
    volatile Uint8 RSVD4[4];
    volatile Uint32 POSTDIV;
    volatile Uint8 RSVD5[12];
    volatile Uint32 PLLCMD;
    volatile Uint32 PLLSTAT;
    volatile Uint32 ALNCTL;
    volatile Uint32 DCHANGE;
    volatile Uint32 CKEN;
    volatile Uint32 CKSTAT;
    volatile Uint32 SYSTAT;
    volatile Uint8 RSVD6[12];
    volatile Uint32 PLLDIV4;
    volatile Uint32 PLLDIV5;
    volatile Uint32 PLLDIV6;
    volatile Uint32 PLLDIV7;
} CSL_PllcRegs;

I can add it myself, but really want the official TI PSP patched and a new version released.  Can this be done?.

thanks

seteve