I have a HS-FS device instead of HS-SE-TIDK now. How can I program OTP on it to convert it to a HS-SE-TIDK device? According to the <Jacinto7 High Security Device Development>, I need to use the TI dummy keys to complete the key programming.
Please provide instructions for building and booting for HS-FS devices on QNX SDK 8.0
And please help to confirm that if secure boot is disabled on a HS-FS device (which means that a signed SBL is unnecessary), or I have to program TI dummy key into HS-FS device via JTAG?