This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: I'm asking for someone's help regarding the ddr3 pin swap of the 66AK2G12 custom board.

Part Number: 66AK2G12


Hello~

I designed a custom board based on EVMK2G.

Most DDR3 configurations are the same as EVM. Only 32-bit data has been pin swapped in bytes.

From now on, I would like to modify the "evmk2g.gel" file to proceed with debugging, and rebuild "sdk_rtos_k2g" to create an MLO file.

I'd like someone to help me with which part of the gel file I need to modify and what I need to change to create the MLO.

  • THere should be no need to change the gel file.  The swap is just at a hardware level, the software does not need to be adjusted since the processor is the only device reading/writing the memory.

    James