Part Number: DRA746
Have an inquiry regarding which version of JEDEC / MMC the following kernel version is compliant with:
Android Version: Lollipop 5.1.1
Kernel Version: 3.8.13-g57be5b6
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA746
Have an inquiry regarding which version of JEDEC / MMC the following kernel version is compliant with:
Android Version: Lollipop 5.1.1
Kernel Version: 3.8.13-g57be5b6
John
Per internal discussions here, answer from the team:
Please note that features-based support that gets added to kernel and not something like "adding support for JEDEC version x".
For instance, JEDEC 5.0 introduces support for HS400 and is supported in kernel. However, that does not mean the kernel would have added all the features introduced in 5.0 (just for example).