This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPS with DM365 microprocessor

Hi:

I have on my board, a GPS chip, and microprocessor DM365. When themicroprocessor is operating, the signal received by the GPs of its satellites is 0. I need to run the 2 together, DM365 and GPS.

I be trying to change the frequency because II think that 300 MHz is 5 harmonic of 1.5 GHz, which is the frequency at which the GPS works. or by the electromagnetic field

With this we have problems to get GPS satellite signal, because when the microprocessor operates at full capacity, the noise can take the GPS satellite signal.

Any suggestions? Could solve this in some way from software?

Thanks