Part Number: TDA4VM
Hi,
Customer wants to run MCU domain application on DDR, Is this possible? If yes, will the crash of the main domain in this case affect the running of RTOS applications on the MCU domain?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi,
Customer wants to run MCU domain application on DDR, Is this possible? If yes, will the crash of the main domain in this case affect the running of RTOS applications on the MCU domain?
Hello,
Yes, an application can run from DDR for the MCU domain, such as running on MCU1_0 or MCU1_1.
Since the DDR is in the main domain, a failure can result in the DDR become inaccessible. The behavior after the crash can vary depending on the nature of the crash.
The linker files in the PDK show how an application could be linked to run from DDR.
ti/build/j721e/linker_r5.lds:
63 .intvecs : {} palign(8) > VECTORS
64 .intc_text : {} palign(8) > VECTORS
65 .rstvectors : {} palign(8) > RESET_VECTORS
66 .bootCode : {} palign(8) > MSMC3
67 .startupCode : {} palign(8) > MSMC3
68 .startupData : {} palign(8) > MSMC3, type = NOINIT
69 .text : {} palign(8) > DDR0
70 .const : {} palign(8) > DDR0
71 .rodata : {} palign(8) > DDR0
72 .cinit : {} palign(8) > DDR0
73 .pinit : {} palign(8) > DDR0
74 .bss : {} align(4) > DDR0
75 .far : {} align(4) > DDR0
76 .data : {} palign(128) > DDR0
77 .sysmem : {} > DDR0
78 .data_buffer : {} palign(128) > DDR0
79 .bss.devgroup* : {} align(4) > DDR0
80 .const.devgroup*: {} align(4) > DDR0
81 .boardcfg_data : {} align(4) > DDR0
Please let me know if you have further questions.
Regards,
Erick