Hello,
The SBL I made by this https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/07_03_00_07/exports/docs/pdk_jacinto_07_03_00_29/docs/userguide/jacinto/boot/boot_k3.html#building-the-sbl-and-its-components
The system can be successfully started
The following is the boot/sbl/tools/combined_appimage/config.mk used to make SBl
root@j7-evm:~# [MCU2_0] 1.802800 s: CIO: Init ... Done !!!
[MCU2_0] 1.802852 s: ### CPU Frequency = 1000000000 Hz
[MCU2_0] 1.802884 s: APP: Init ... !!!
[MCU2_0] 1.802900 s: SCICLIENT: Init ... !!!
[MCU2_0] 1.803106 s: SCICLIENT: DMSC FW version [21.5.0--v2021.05 (Terrific Llam]
[MCU2_0] 1.803142 s: SCICLIENT: DMSC FW revision 0x15
[MCU2_0] 1.803166 s: SCICLIENT: DMSC FW ABI revision 3.1
[MCU2_0] 1.803190 s: SCICLIENT: Init ... Done !!!
[MCU2_0] 1.803209 s: UDMA: Init ... !!!
[MCU2_0] 1.804240 s: UDMA: Init ... Done !!!
[MCU2_0] 1.804284 s: MEM: Init ... !!!
[MCU2_0] 1.804315 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ e1000000 of size 16777216 bytes !!!
[MCU2_0] 1.804365 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!!
[MCU2_0] 1.804408 s: MEM: Created heap (DDR_NON_CACHE_ME, id=5, flags=0x00000000) @ d8000000 of size 16777216 bytes !!!
[MCU2_0] 1.804449 s: MEM: Init ... Done !!!
[MCU2_0] 1.804467 s: IPC: Init ... !!!
[MCU2_0] 1.804513 s: IPC: 6 CPUs participating in IPC !!!
[MCU2_0] 1.804559 s: IPC: Waiting for HLOS to be ready ... !!!