Part Number: AM5728
Hi,
I am following the instructions from -https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Overview_Building_the_SDK.html to build processor SDK.
My environment is
Window 10
Virtual Box - Ubuntu 18.04 LTS
ti-processor-sdk-linux-am57xx-evm-06.03.00.106
and trying to build arago base image
$ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
I have ended up in this state when I have rebooted my PC due to windows crash. I assume the SDK build was running in the background at the time of windows crash.
I tried to start a clean build but no success.
$MACHINE=am57xx-evm bitbake arago-base-tisdk-image -c cleansstate
sri@sri-VirtualBox:~/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/build$ export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf
sri@sri-VirtualBox:~/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/build$ export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu
sri@sri-VirtualBox:~/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/build$ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
Loading cache: 100% |############################################| Time: 0:00:01
Loaded 4658 entries from dependency cache.
WARNING: No recipes available for:
/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/meta-arago/meta-arago-distro/recipes-browser/chromium/chromium-wayland_%.bbappend
/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
ERROR: Execution of event handler 'sstate_eventhandler2' failed
Traceback (most recent call last):
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/oe-core/meta/classes/sstate.bbclass", line 1090, in sstate_eventhandler2(e=<bb.event.ReachableStamps object at 0x7f9648923cf8>):
for l in lines:
> (stamp, manifest, workdir) = l.split()
if stamp not in stamps and stamp not in preservestamps and stamp in machineindex:
ValueError: not enough values to unpack (expected 3, got 1)
ERROR: Command execution failed: Traceback (most recent call last):
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/bitbake/lib/bb/command.py", line 113, in runAsyncCommand
self.cooker.updateCache()
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/bitbake/lib/bb/cooker.py", line 1588, in updateCache
bb.event.fire(event, self.databuilder.mcdata[mc])
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/bitbake/lib/bb/event.py", line 225, in fire
fire_class_handlers(event, d)
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/bitbake/lib/bb/event.py", line 134, in fire_class_handlers
execute_handler(name, handler, event, d)
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/bitbake/lib/bb/event.py", line 106, in execute_handler
ret = handler(event)
File "/home/sri/ti-processor-sdk-linux-am57xx-evm-06.03.00.106/armtoolchain/tisdk/sources/oe-core/meta/classes/sstate.bbclass", line 1090, in sstate_eventhandler2
(stamp, manifest, workdir) = l.split()
ValueError: not enough values to unpack (expected 3, got 1)
Summary: There were 3 WARNING messages shown.
I assume some kind of corruption during the build process due to the windows crash which I could not recover.
can you please help ?
thanks
Sri