This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Slave timing of Video I/O with DM8165/8 Family of DaVinci Processors

Hello:

 

Cannot get answer on this from TI yet.  Can the Video input and video output timing on the DM8168 be syncronized from the video input timing?  We are trying insert the video outputs into the live video feed that is running at its own VD and HD rates.  We would encode these into the DaVinci Video input and then the output would be locked. 

 

The DM365 would allow the part to be slaved in this way