Hi,
Here are a few questions :
1) We noticed a difference between TMDS64GPEVM & SK-AM64 : that there are pull-up resistors at the SD card interface of the SK-AM64 and not for the TMDS64GPEVM, why and could it cause integrity signal issues if they are not present ?
2) When using the PRU-ICSSG in parallel input mode, page 3441 of the TRM, GPI0->16 are used and GPI17-> 19 are greyed out. Does it mean GPI17-> 19 can't be used as Direct Input ? If not, how can I use the PRU to receive other type if signal such as ChipSelect signal?
3) Can you confirm that they instruction wbs in assembly with the PRU is active on the rising edge and not on the state 1 ?
Regards,
Geoffrey