Part Number: TDA4VM
We are attempting to get our image sensor running with our TDA4EVM. Our setup includes a Sony image sensor, a TI UB933 serializer, and a TI UB960 deserializer. We had previously had this sensor streaming video to a display via the single cam app demo with the 7.02 PSDKR. We have now updated to the 8.02 release and have lost the ability to stream video. Beforehand, we changed the following files to enable video streaming: iss_sensor_gw_ar0233.c and ub9xx_gw_ar0233_serdes_config.h. Our ser-des scripts were as follows:
#define GW_AR0233_DES_CFG_SIZE (15U)
I2cParams ub9xxDesCfg_GW_AR0233[GW_AR0233_DES_CFG_SIZE] = {
// {0xB3, 0x00, 0x1},
{0x4C, 0x01, 0x1},
{0x5c, 0x58, 0x01}, //ser addr
{0x58, 0xd8, 0x1}, //2.5Mbps
{0x6d, 0x6f, 0x01}, //raw 10
{0x70, 0x1e, 0x01},
{0x71, 0x2c, 0x01},
{0x7c, 0xe0, 0x1}, // send 8 bit over csi
{0x21, 0x03, 0x0},
{0x0F, 0x7F, 0x1},
{0x6E, 0x10, 0x1},
{0x6F, 0x32, 0x1},
{0x32, 0x01, 0x1},
{0x33, 0x02, 0x1},
{0x20, 0x00, 0x1},
{0xFFFF, 0x00, 0x0} /*End of script */
};
#define GW_AR0233_SER_CFG_SIZE (4U)
I2cParams ub9xxSerCfg_GW_AR0233[GW_AR0233_SER_CFG_SIZE] = {
// {0x0E, 0xF0, 0xF0},
{0x0d, 0x99, 0x60},
{0x0d, 0x91, 0x60},
{0x0d, 0x99, 0x60},
{0xFFFF, 0x00, 0x0} /*End of script */
};
I2cParams ub9xxGW_AR0233DesCSI2Enable[10u] = {
{0x33, 0x03, 0x1},
{0xFFFF, 0x00, 0x0} //End of script
};
I2cParams ub9xxGW_AR0233DesCSI2Disable[2u] = {
{0x33, 0x02, 0x10},
{0xFFFF, 0x00, 0x0} /*End of script */
};
To add support for our sensor, we modified the GW AR0233 sensor files as follows:
static IssSensor_CreateParams gw_ar0233CreatePrms = {
GW_AR0233_UYVY, /*sensor name*/
0x6, /*i2cInstId*/
{0x1b, 0, 0, 0, 0, 0, 0, 0}, /*i2cAddrSensor*/
{0x58, 0, 0, 0, 0, 0, 0, 0}, /*i2cAddrSer*/
/*IssSensor_Info*/
{
{
GW_AR0233_OUT_WIDTH, /*width*/
GW_AR0233_OUT_HEIGHT, /*height*/
1, /*num_exposures*/
vx_false_e, /*line_interleaved*/
{
{VX_DF_IMAGE_UYVY, 7}, /*dataFormat and MSB [0]*/
},
0, /*meta_height_before*/
0, /*meta_height_after*/
},
ISS_SENSOR_GW_AR0233_FEATURES, /*features*/
ALGORITHMS_ISS_AEWB_MODE_NONE, /*aewbMode*/
30, /*fps*/
4, /*numDataLanes*/
{1, 2, 3, 4}, /*dataLanesMap*/
{0, 0, 0, 0}, /*dataLanesPolarity*/
800, /*CSI Clock*/
},
1, /*numChan*/
5233, /*dccId*/
};
static IssSensorIntfParams gw_ar0233SensorIntfPrms = {
0, /*isMultiChannel*/
4, /*numCSI2Lanes*/
1, /*inCsi2VirtualChanNum*/
1, /* isCplxCfgValid */
{
{0, 1}, /* Clock Lane */
{0, 2}, /* data1Lane */
{0, 3}, /* data2Lane */
{0, 4}, /* data3Lane*/
{0, 5}, /* data4Lane */
},
800, /* csi2PhyClk */
0, /*sensorBroadcast*/
0, /*enableFsin*/
};
IssSensorConfig gw_ar0233SensorRegConfig = {
ub9xxDesCfg_GW_AR0233, /*desCfgPreScript*/
ub9xxSerCfg_GW_AR0233, /*serCfgPreScript*/
NULL, /*sensorCfgPreScript*/
ub9xxGW_AR0233DesCSI2Enable, /*desCfgPostScript*/
NULL, /*serCfgPostScript*/
NULL, /*sensorCfgPostScript*/
};
Per advice from another forum post, we have also tried using the macro CSIRX_LANE_BAND_SPEED_720_TO_800_MBPS for the CSI clock to no avail.
There were also some changes that we noticed in the iss_sensors.c file, namely the inclusion of the ub960DesCfg_Common struct. After viewing the I2C communication, we do not think that the deserializer and serializer are properly linking. Are these settings interfering with our previous configuration? Is there anything else that we have to do differently on 8.02? I have attached logs of our boot-up, vision app initialization, and single cam app.
cd /opt/vision_apps/ root@j7-evm:/opt/vision_apps# source ./vision_apps_init.sh root@j7-evm:/opt/vision_apps# [MCU2_0] 4.214755 s: CIO: Init ... Done !!! [MCU2_0] 4.214827 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 4.214869 s: APP: Init ... !!! [MCU2_0] 4.214893 s: SCICLIENT: Init ... !!! [MCU2_0] 4.215163 s: SCICLIENT: DMSC FW version [22.1.1--v2022.01 (Terrific Llam] [MCU2_0] 4.215211 s: SCICLIENT: DMSC FW revision 0x16 [MCU2_0] 4.215243 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_0] 4.215278 s: SCICLIENT: Init ... Done !!! [MCU2_0] 4.215305 s: UDMA: Init ... !!! [MCU2_0] 4.216643 s: UDMA: Init ... Done !!! [MCU2_0] 4.216710 s: MEM: Init ... !!! [MCU2_0] 4.216756 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!! [MCU2_0] 4.216831 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!! [MCU2_0] 4.216892 s: MEM: Init ... Done !!! [MCU2_0] 4.216918 s: IPC: Init ... !!! [MCU2_0] 4.216982 s: IPC: 6 CPUs participating in IPC !!! [MCU2_0] 4.217036 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_0] 17.190128 s: IPC: HLOS is ready !!! [MCU2_0] 17.205628 s: IPC: Init ... Done !!! [MCU2_0] 17.205697 s: APP: Syncing with 5 CPUs ... !!! [MCU2_0] 17.443053 s: APP: Syncing with 5 CPUs ... Done !!! [MCU2_0] 17.443306 s: REMOTE_SERVICE: Init ... !!! [MCU2_0] 17.444913 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_0] 17.444980 s: ETHFW: Init ... !!! [MCU2_0] 17.464236 s: ETHFW: Shared multicasts (software fanout): [MCU2_0] 17.464318 s: 01:00:5e:00:00:01 [MCU2_0] 17.464380 s: 01:00:5e:00:00:fb [MCU2_0] 17.464428 s: 01:00:5e:00:00:fc [MCU2_0] 17.464492 s: 33:33:00:00:00:01 [MCU2_0] 17.464540 s: 33:33:ff:1d:92:c2 [MCU2_0] 17.464584 s: 01:80:c2:00:00:00 [MCU2_0] 17.464629 s: 01:80:c2:00:00:03 [MCU2_0] 17.464675 s: ETHFW: Reserved multicasts: [MCU2_0] 17.464705 s: 01:80:c2:00:00:0e [MCU2_0] 17.464752 s: 01:1b:19:00:00:00 [MCU2_0] 17.465024 s: EnetMcm: CPSW_9G on MAIN NAVSS [MCU2_0] 17.474441 s: PHY 16 is alive [MCU2_0] 17.474552 s: PHY 17 is alive [MCU2_0] 17.474594 s: PHY 18 is alive [MCU2_0] 17.474626 s: PHY 19 is alive [MCU2_0] 17.475491 s: EnetPhy_bindDriver: PHY 16: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK [MCU2_0] 17.475875 s: EnetPhy_bindDriver: PHY 17: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK [MCU2_0] 17.476232 s: EnetPhy_bindDriver: PHY 18: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK [MCU2_0] 17.476587 s: EnetPhy_bindDriver: PHY 19: OUI:0001c1 Model:27 Ver:00 <-> 'vsc8514' : OK [MCU2_0] 17.478320 s: [MCU2_0] ETHFW Version : 0.02.00 [MCU2_0] 17.478393 s: ETHFW Build Date: Apr 14, 2022 [MCU2_0] 17.478424 s: ETHFW Build Time: 11:53:27 [MCU2_0] 17.478453 s: ETHFW Commit SHA: [MCU2_0] 17.478533 s: ETHFW: Init ... DONE !!! [MCU2_0] 17.478566 s: ETHFW: Remove server Init ... !!! [MCU2_0] 17.478764 s: CpswProxyServer: Virtual port configuration: [MCU2_0] 17.478823 s: mpu_1_0 <-> Switch port 0: mpu_1_0_ethswitch-device-0 [MCU2_0] 17.478870 s: mcu_2_1 <-> Switch port 1: mcu_2_1_ethswitch-device-1 [MCU2_0] 17.478913 s: mpu_1_0 <-> MAC port 1: mpu_1_0_ethmac-device-1 [MCU2_0] 17.478955 s: mcu_2_1 <-> MAC port 4: mcu_2_1_ethmac-device-4 [MCU2_0] 17.480031 s: CpswProxyServer: initialization completed (core: mcu2_0) [MCU2_0] 17.480095 s: ETHFW: Remove server Init ... DONE !!! [MCU2_0] 17.481229 s: Starting lwIP, local interface IP is dhcp-enabled [MCU2_0] 17.487884 s: Host MAC address: 70:ff:76:1d:92:c3 [MCU2_0] 17.491851 s: [LWIPIF_LWIP] Enet LLD netif initialized successfully [MCU2_0] 17.522035 s: [LWIPIF_LWIP_IC] Interface started successfully [MCU2_0] 17.522112 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS [MCU2_0] 17.532480 s: FVID2: Init ... !!! [MCU2_0] 17.532580 s: FVID2: Init ... Done !!! [MCU2_0] 17.532629 s: DSS: Init ... !!! [MCU2_0] 17.532656 s: DSS: Display type is eDP !!! [MCU2_0] 17.532683 s: DSS: M2M Path is enabled !!! [MCU2_0] 17.532711 s: DSS: SoC init ... !!! [MCU2_0] 17.532736 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2 [MCU2_0] 17.532961 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.533000 s: SCICLIENT: Sciclient_pmSetModuleState module=297 state=2 [MCU2_0] 17.533200 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.533233 s: SCICLIENT: Sciclient_pmSetModuleState module=151 state=2 [MCU2_0] 17.533382 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.533414 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11 [MCU2_0] 17.533680 s: SCICLIENT: Sciclient_pmSetModuleClkParent success [MCU2_0] 17.533735 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=13 parent=18 [MCU2_0] 17.533859 s: SCICLIENT: Sciclient_pmSetModuleClkParent success [MCU2_0] 17.533895 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=1 parent=2 [MCU2_0] 17.533993 s: SCICLIENT: Sciclient_pmSetModuleClkParent success [MCU2_0] 17.534028 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=1 freq=148500000 [MCU2_0] 17.535084 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success [MCU2_0] 17.535136 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=1 state=2 flag=0 [MCU2_0] 17.535307 s: SCICLIENT: Sciclient_pmModuleClkRequest success [MCU2_0] 17.535345 s: DSS: SoC init ... Done !!! [MCU2_0] 17.535371 s: DSS: Board init ... !!! [MCU2_0] 17.535397 s: DSS: Board init ... Done !!! [MCU2_0] 17.580362 s: DSS: Init ... Done !!! [MCU2_0] 17.580430 s: VHWA: VPAC Init ... !!! [MCU2_0] 17.580601 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2 [MCU2_0] 17.580832 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.580874 s: VHWA: LDC Init ... !!! [MCU2_0] 17.584628 s: VHWA: LDC Init ... Done !!! [MCU2_0] 17.584696 s: VHWA: MSC Init ... !!! [MCU2_0] 17.597099 s: VHWA: MSC Init ... Done !!! [MCU2_0] 17.597169 s: VHWA: NF Init ... !!! [MCU2_0] 17.599178 s: VHWA: NF Init ... Done !!! [MCU2_0] 17.599246 s: VHWA: VISS Init ... !!! [MCU2_0] 17.611027 s: VHWA: VISS Init ... Done !!! [MCU2_0] 17.611093 s: VHWA: VPAC Init ... Done !!! [MCU2_0] 17.611138 s: VX_ZONE_INIT:Enabled [MCU2_0] 17.611171 s: VX_ZONE_ERROR:Enabled [MCU2_0] 17.611197 s: VX_ZONE_WARNING:Enabled [MCU2_0] 17.612694 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-0 [MCU2_0] 17.613057 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_NF [MCU2_0] 17.613325 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_LDC1 [MCU2_0] 17.613767 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC1 [MCU2_0] 17.614044 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC2 [MCU2_0] 17.614333 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_VISS1 [MCU2_0] 17.614787 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE1 [MCU2_0] 17.615083 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE2 [MCU2_0] 17.615343 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY1 [MCU2_0] 17.615763 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY2 [MCU2_0] 17.616025 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CSITX [MCU2_0] 17.616297 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE3 [MCU2_0] 17.616717 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE4 [MCU2_0] 17.617009 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE5 [MCU2_0] 17.617271 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE6 [MCU2_0] 17.617685 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE7 [MCU2_0] 17.617991 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE8 [MCU2_0] 17.618217 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M1 [MCU2_0] 17.618430 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M2 [MCU2_0] 17.618850 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M3 [MCU2_0] 17.619091 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M4 [MCU2_0] 17.619150 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_0] 17.619187 s: APP: OpenVX Target kernel init ... !!! [MCU2_0] 17.625279 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6 [MCU2_0] 17.641014 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_0] 17.641081 s: CSI2RX: Init ... !!! [MCU2_0] 17.641112 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2 [MCU2_0] 17.641242 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.641280 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2 [MCU2_0] 17.641422 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.641589 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2 [MCU2_0] 17.641753 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.641793 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2 [MCU2_0] 17.641901 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.641934 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2 [MCU2_0] 17.642025 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.642948 s: CSI2RX: Init ... Done !!! [MCU2_0] 17.643018 s: CSI2TX: Init ... !!! [MCU2_0] 17.643047 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2 [MCU2_0] 17.643165 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.643201 s: SCICLIENT: Sciclient_pmSetModuleState module=28 state=2 [MCU2_0] 17.643359 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.643393 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2 [MCU2_0] 17.643592 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 17.644274 s: CSI2TX: Init ... Done !!! [MCU2_0] 17.644337 s: ISS: Init ... !!! [MCU2_0] 17.644380 s: IssSensor_Init ... Done !!! [MCU2_0] 17.644634 s: vissRemoteServer_Init ... Done !!! [MCU2_0] 17.644728 s: IttRemoteServer_Init ... Done !!! [MCU2_0] 17.644768 s: UDMA Copy: Init ... !!! [MCU2_0] 17.646904 s: UDMA Copy: Init ... Done !!! [MCU2_0] 17.647013 s: APP: Init ... Done !!! [MCU2_0] 17.647055 s: APP: Run ... !!! [MCU2_0] 17.647080 s: IPC: Starting echo test ... [MCU2_0] 17.650069 s: APP: Run ... Done !!! [MCU2_0] 17.657146 s: [LWIPIF_LWIP_IC] Interface started successfully [MCU2_0] 17.657220 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS [MCU2_0] 17.657335 s: Added interface 'br4', IP is 0.0.0.0 [MCU2_0] 17.659306 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C66X_1[P] C66X_2[x] C7X_1[.] [MCU2_0] 17.659847 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[.] C7X_1[.] [MCU2_0] 17.659965 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[.] C7X_1[P] [MCU2_0] 17.660065 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[P] [MCU2_0] 17.760532 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6 [MCU2_0] 20.525962 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c2, FlowIdx:173, FlowIdxOffset:1 [MCU2_0] 20.539045 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_0] 20.539381 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_0] 20.547530 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_0] 20.555026 s: Function:CpswProxyServer_registerMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:70:ff:76:1d:92:c1, FlowIdx:172, FlowIdxOffset:0 [MCU2_0] 20.558203 s: Cpsw_ioctlInternal: CPSW: Registered MAC address. ALE entry:7, Policer Entry:2 [MCU2_0] 20.613617 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.615618 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:1:0:5e:0:0:1, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.617611 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:33:33:ff:1d:92:c1, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.745083 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_0] 20.756744 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:0, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.758815 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.760799 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:1:80:c2:0:0:e, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 20.760951 s: CpswProxyServer_isRsvdMcast: Reserved mcast cannot be added to filter [MCU2_0] 20.896123 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_0] 20.896381 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:33:33:0:0:0:fb, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 21.762392 s: Function:CpswProxyServer_filterAddMacHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6, MacAddress:33:33:0:1:0:3, vlanId:0, FlowIdx:172, FlowIdOffset:0 [MCU2_0] 22.209165 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a38f00b4,CoreKey:38acb7e6,mode:disable [MCU2_1] 4.166897 s: CIO: Init ... Done !!! [MCU2_1] 4.166969 s: ### CPU Frequency = 1000000000 Hz [MCU2_1] 4.167010 s: APP: Init ... !!! [MCU2_1] 4.167038 s: SCICLIENT: Init ... !!! [MCU2_1] 4.167304 s: SCICLIENT: DMSC FW version [22.1.1--v2022.01 (Terrific Llam] [MCU2_1] 4.167356 s: SCICLIENT: DMSC FW revision 0x16 [MCU2_1] 4.167390 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_1] 4.167443 s: SCICLIENT: Init ... Done !!! [MCU2_1] 4.167473 s: UDMA: Init ... !!! [MCU2_1] 4.168927 s: UDMA: Init ... Done !!! [MCU2_1] 4.168994 s: MEM: Init ... !!! [MCU2_1] 4.169038 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!! [MCU2_1] 4.169116 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!! [MCU2_1] 4.169175 s: MEM: Init ... Done !!! [MCU2_1] 4.169202 s: IPC: Init ... !!! [MCU2_1] 4.169264 s: IPC: 6 CPUs participating in IPC !!! [MCU2_1] 4.169314 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_1] 17.427559 s: IPC: HLOS is ready !!! [MCU2_1] 17.442928 s: IPC: Init ... Done !!! [MCU2_1] 17.443004 s: APP: Syncing with 5 CPUs ... !!! [MCU2_1] 17.443052 s: APP: Syncing with 5 CPUs ... Done !!! [MCU2_1] 17.443089 s: REMOTE_SERVICE: Init ... !!! [MCU2_1] 17.444934 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_1] 17.445003 s: FVID2: Init ... !!! [MCU2_1] 17.445081 s: FVID2: Init ... Done !!! [MCU2_1] 17.445118 s: VHWA: DMPAC: Init ... !!! [MCU2_1] 17.445146 s: SCICLIENT: Sciclient_pmSetModuleState module=48 state=2 [MCU2_1] 17.445322 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 17.445367 s: SCICLIENT: Sciclient_pmSetModuleState module=305 state=2 [MCU2_1] 17.445907 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 17.445949 s: VHWA: DOF Init ... !!! [MCU2_1] 17.454308 s: VHWA: DOF Init ... Done !!! [MCU2_1] 17.454375 s: VHWA: SDE Init ... !!! [MCU2_1] 17.456955 s: VHWA: SDE Init ... Done !!! [MCU2_1] 17.457021 s: VHWA: DMPAC: Init ... Done !!! [MCU2_1] 17.457074 s: VX_ZONE_INIT:Enabled [MCU2_1] 17.457107 s: VX_ZONE_ERROR:Enabled [MCU2_1] 17.457137 s: VX_ZONE_WARNING:Enabled [MCU2_1] 17.458304 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_SDE [MCU2_1] 17.458552 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_DOF [MCU2_1] 17.458787 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-1 [MCU2_1] 17.458843 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_1] 17.458881 s: APP: OpenVX Target kernel init ... !!! [MCU2_1] 17.459158 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_1] 17.459206 s: UDMA Copy: Init ... !!! [MCU2_1] 17.461042 s: UDMA Copy: Init ... Done !!! [MCU2_1] 17.461116 s: APP: Init ... Done !!! [MCU2_1] 17.461153 s: APP: Run ... !!! [MCU2_1] 17.461181 s: IPC: Starting echo test ... [MCU2_1] 17.463723 s: APP: Run ... Done !!! [MCU2_1] 17.465087 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[.] C7X_1[.] [MCU2_1] 17.465204 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[.] [MCU2_1] 17.465304 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P] [MCU2_1] 17.659262 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P] [C6x_1 ] 4.230762 s: CIO: Init ... Done !!! [C6x_1 ] 4.230788 s: ### CPU Frequency = 1350000000 Hz [C6x_1 ] 4.230800 s: APP: Init ... !!! [C6x_1 ] 4.230808 s: SCICLIENT: Init ... !!! [C6x_1 ] 4.231051 s: SCICLIENT: DMSC FW version [22.1.1--v2022.01 (Terrific Llam] [C6x_1 ] 4.231068 s: SCICLIENT: DMSC FW revision 0x16 [C6x_1 ] 4.231078 s: SCICLIENT: DMSC FW ABI revision 3.1 [C6x_1 ] 4.231089 s: SCICLIENT: Init ... Done !!! [C6x_1 ] 4.231099 s: UDMA: Init ... !!! [C6x_1 ] 4.232809 s: UDMA: Init ... Done !!! [C6x_1 ] 4.232834 s: MEM: Init ... !!! [C6x_1 ] 4.232849 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ dc000000 of size 16777216 bytes !!! [C6x_1 ] 4.232870 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!! [C6x_1 ] 4.232887 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ dd000000 of size 50331648 bytes !!! [C6x_1 ] 4.232905 s: MEM: Init ... Done !!! [C6x_1 ] 4.232914 s: IPC: Init ... !!! [C6x_1 ] 4.232938 s: IPC: 6 CPUs participating in IPC !!! [C6x_1 ] 4.232954 s: IPC: Waiting for HLOS to be ready ... !!! [C6x_1 ] 15.618645 s: IPC: HLOS is ready !!! [C6x_1 ] 15.623285 s: IPC: Init ... Done !!! [C6x_1 ] 15.623315 s: APP: Syncing with 5 CPUs ... !!! [C6x_1 ] 17.443051 s: APP: Syncing with 5 CPUs ... Done !!! [C6x_1 ] 17.443071 s: REMOTE_SERVICE: Init ... !!! [C6x_1 ] 17.443876 s: REMOTE_SERVICE: Init ... Done !!! [C6x_1 ] 17.443918 s: VX_ZONE_INIT:Enabled [C6x_1 ] 17.443930 s: VX_ZONE_ERROR:Enabled [C6x_1 ] 17.443940 s: VX_ZONE_WARNING:Enabled [C6x_1 ] 17.444853 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C6x_1 ] 17.444871 s: APP: OpenVX Target kernel init ... !!! [C6x_1 ] 17.445318 s: APP: OpenVX Target kernel init ... Done !!! [C6x_1 ] 17.445339 s: UDMA Copy: Init ... !!! [C6x_1 ] 17.448630 s: UDMA Copy: Init ... Done !!! [C6x_1 ] 17.448658 s: APP: Init ... Done !!! [C6x_1 ] 17.449408 s: APP: Run ... !!! [C6x_1 ] 17.449423 s: IPC: Starting echo test ... [C6x_1 ] 17.450517 s: APP: Run ... Done !!! [C6x_1 ] 17.450926 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[x] C7X_1[P] [C6x_1 ] 17.451428 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[s] C66X_2[P] C7X_1[P] [C6x_1 ] 17.464825 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P] [C6x_1 ] 17.659090 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P] [C6x_2 ] 4.318577 s: CIO: Init ... Done !!! [C6x_2 ] 4.318604 s: ### CPU Frequency = 1350000000 Hz [C6x_2 ] 4.318616 s: APP: Init ... !!! [C6x_2 ] 4.318625 s: SCICLIENT: Init ... !!! [C6x_2 ] 4.318876 s: SCICLIENT: DMSC FW version [22.1.1--v2022.01 (Terrific Llam] [C6x_2 ] 4.318894 s: SCICLIENT: DMSC FW revision 0x16 [C6x_2 ] 4.318904 s: SCICLIENT: DMSC FW ABI revision 3.1 [C6x_2 ] 4.318916 s: SCICLIENT: Init ... Done !!! [C6x_2 ] 4.318925 s: UDMA: Init ... !!! [C6x_2 ] 4.320685 s: UDMA: Init ... Done !!! [C6x_2 ] 4.320710 s: MEM: Init ... !!! [C6x_2 ] 4.320724 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ e0000000 of size 16777216 bytes !!! [C6x_2 ] 4.320745 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!! [C6x_2 ] 4.320763 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e1000000 of size 50331648 bytes !!! [C6x_2 ] 4.320781 s: MEM: Init ... Done !!! [C6x_2 ] 4.320790 s: IPC: Init ... !!! [C6x_2 ] 4.320815 s: IPC: 6 CPUs participating in IPC !!! [C6x_2 ] 4.320831 s: IPC: Waiting for HLOS to be ready ... !!! [C6x_2 ] 16.179899 s: IPC: HLOS is ready !!! [C6x_2 ] 16.184557 s: IPC: Init ... Done !!! [C6x_2 ] 16.184586 s: APP: Syncing with 5 CPUs ... !!! [C6x_2 ] 17.443051 s: APP: Syncing with 5 CPUs ... Done !!! [C6x_2 ] 17.443071 s: REMOTE_SERVICE: Init ... !!! [C6x_2 ] 17.443884 s: REMOTE_SERVICE: Init ... Done !!! [C6x_2 ] 17.443927 s: VX_ZONE_INIT:Enabled [C6x_2 ] 17.443938 s: VX_ZONE_ERROR:Enabled [C6x_2 ] 17.443949 s: VX_ZONE_WARNING:Enabled [C6x_2 ] 17.444860 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C6x_2 ] 17.444878 s: APP: OpenVX Target kernel init ... !!! [C6x_2 ] 17.445326 s: APP: OpenVX Target kernel init ... Done !!! [C6x_2 ] 17.445347 s: UDMA Copy: Init ... !!! [C6x_2 ] 17.448928 s: UDMA Copy: Init ... Done !!! [C6x_2 ] 17.448953 s: APP: Init ... Done !!! [C6x_2 ] 17.449727 s: APP: Run ... !!! [C6x_2 ] 17.449747 s: IPC: Starting echo test ... [C6x_2 ] 17.450917 s: APP: Run ... Done !!! [C6x_2 ] 17.451425 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[.] [C6x_2 ] 17.451470 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[P] [C6x_2 ] 17.464852 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P] [C6x_2 ] 17.659117 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P] [C7x_1 ] 4.544409 s: CIO: Init ... Done !!! [C7x_1 ] 4.544424 s: ### CPU Frequency = 1000000000 Hz [C7x_1 ] 4.544436 s: APP: Init ... !!! [C7x_1 ] 4.544444 s: SCICLIENT: Init ... !!! [C7x_1 ] 4.544657 s: SCICLIENT: DMSC FW version [22.1.1--v2022.01 (Terrific Llam] [C7x_1 ] 4.544671 s: SCICLIENT: DMSC FW revision 0x16 [C7x_1 ] 4.544681 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 4.544692 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 4.544701 s: UDMA: Init ... !!! [C7x_1 ] 4.545855 s: UDMA: Init ... Done !!! [C7x_1 ] 4.545868 s: MEM: Init ... !!! [C7x_1 ] 4.545880 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ 100000000 of size 268435456 bytes !!! [C7x_1 ] 4.545902 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!! [C7x_1 ] 4.545919 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!! [C7x_1 ] 4.545937 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!! [C7x_1 ] 4.545954 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ e4000000 of size 385875968 bytes !!! [C7x_1 ] 4.545974 s: MEM: Init ... Done !!! [C7x_1 ] 4.545982 s: IPC: Init ... !!! [C7x_1 ] 4.545997 s: IPC: 6 CPUs participating in IPC !!! [C7x_1 ] 4.546012 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 16.703116 s: IPC: HLOS is ready !!! [C7x_1 ] 16.705356 s: IPC: Init ... Done !!! [C7x_1 ] 16.705371 s: APP: Syncing with 5 CPUs ... !!! [C7x_1 ] 17.443053 s: APP: Syncing with 5 CPUs ... Done !!! [C7x_1 ] 17.443070 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 17.443204 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 17.443274 s: VX_ZONE_INIT:Enabled [C7x_1 ] 17.443286 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 17.443296 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 17.443477 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 [C7x_1 ] 17.443565 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 [C7x_1 ] 17.443700 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 [C7x_1 ] 17.443781 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 [C7x_1 ] 17.443855 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 [C7x_1 ] 17.443923 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 [C7x_1 ] 17.444002 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 [C7x_1 ] 17.444109 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 [C7x_1 ] 17.444133 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_1 ] 17.444147 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 17.444394 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 17.444409 s: APP: Init ... Done !!! [C7x_1 ] 17.444420 s: APP: Run ... !!! [C7x_1 ] 17.444431 s: IPC: Starting echo test ... [C7x_1 ] 17.444591 s: APP: Run ... Done !!! [C7x_1 ] 17.450912 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[x] C7X_1[s] [C7x_1 ] 17.451411 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C66X_1[P] C66X_2[P] C7X_1[s] [C7x_1 ] 17.464868 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s] [C7x_1 ] 17.659166 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s] root@j7-evm:/opt/vision_apps# ./
[ 134.627628] Initializing XFRM netlink socket [ 137.267498] process 'docker/tmp/qemu-check515055542/check' started with executable stack root@j7-evm:/opt/vision_apps# ./run_app_single_cam.sh APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 172.343015 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 172.349670 s: VX_ZONE_INIT:Enabled 172.349699 s: VX_ZONE_ERROR:Enabled 172.349705 s: VX_ZONE_WARNING:Enabled 172.357014 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! 172.357209 s: VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!! sensor_selection = [0] ldc_enable = [0] num_frames_to_run = [1000000000] is_interactive = [1] IttCtrl_registerHandler: command echo registered at location 0 IttCtrl_registerHandler: command iss_read_2a_params registered at location 1 IttCtrl_registerHandler: command iss_write_2a_params registered at location 2 IttCtrl_registerHandler: command iss_raw_save registered at location 3 IttCtrl_registerHandler: command iss_yuv_save registered at location 4 IttCtrl_registerHandler: command iss_read_sensor_reg registered at location 5 IttCtrl_registerHandler: command iss_write_sensor_reg registered at location 6 IttCtrl_registerHandler: command dev_ctrl registered at location 7 IttCtrl_registerHandler: command iss_send_dcc_file registered at location 8 NETWORK: Opened at IP Addr = 0.0.16.0, socket port=5000!!! 172.366951 s: ISS: Enumerating sensors ... !!! [MCU2_0] 172.682694 s: BPD: address = 0x3d reg = 0x35 value = 0x0 [MCU2_0] 172.682919 s: BPD: address = 0x3d reg = 0x73 value = 0x0 [MCU2_0] 172.683121 s: BPD: address = 0x3d reg = 0x74 value = 0x0 [MCU2_0] 172.683317 s: BPD: address = 0x3d reg = 0x75 value = 0x0 [MCU2_0] 172.683552 s: BPD: address = 0x3d reg = 0x76 value = 0x0 [MCU2_0] 172.683757 s: BPD: address = 0x3d reg = 0x90 value = 0x0 [MCU2_0] 172.683957 s: BPD: address = 0x3d reg = 0x91 value = 0x0 172.883941 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3 172.883956 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS 172.883976 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI 172.883981 s: ISS: Enumerating sensors ... found 3 : UB9xxx_RAW12_TESTPATTERN 172.883986 s: ISS: Enumerating sensors ... found 4 : UB96x_UYVY_TESTPATTERN 172.883991 s: ISS: Enumerating sensors ... found 5 : GW_AR0233_UYVY Select camera port index 0-7 : 0 6 registered sensor drivers a : IMX390-UB953_D3 b : AR0233-UB953_MARS c : AR0820-UB953_LI d : UB9xxx_RAW12_TESTPATTERN e : UB96x_UYVY_TESTPATTERN f : GW_AR0233_UYVY Select a sensor above or press '0' to autodetect the sensor : Invalid selection . Try again 6 registered sensor drivers a : IMX390-UB953_D3 b : AR0233-UB953_MARS c : AR0820-UB953_LI d : UB9xxx_RAW12_TESTPATTERN e : UB96x_UYVY_TESTPATTERN f : GW_AR0233_UYVY Select a sensor above or press '0' to autodetect the sensor : f Sensor selected : GW_AR0233_UYVY LDC Selection Yes(1)/No(0) : LDC Selection Yes(1)/No(0) : 0 Querying GW_AR0233_UYVY 182.024346 s: ISS: Querying sensor [GW_AR0233_UYVY] ... !!! 182.024737 s: ISS: Querying sensor [GW_AR0233_UYVY] ... Done !!! YUV Input selected. VISS and AEWB nodes will be bypassed. 182.024754 s: ISS: Initializing sensor [GW_AR0233_UYVY], doing IM_SENSOR_CMD_PWRON ... !!! 182.025061 s: ISS: Initializing sensor [GW_AR0233_UYVY], doing IM_SENSOR_CMD_CONFIG ... !!! [MCU2_0] 182.296701 s: BPD: address = 0x3d reg = 0x35 value = 0x0 [MCU2_0] 182.296929 s: BPD: address = 0x3d reg = 0x73 value = 0x0 [MCU2_0] 182.297128 s: BPD: address = 0x3d reg = 0x74 value = 0x0 [MCU2_0] 182.297321 s: BPD: address = 0x3d reg = 0x75 value = 0x0 [MCU2_0] 182.297554 s: BPD: address = 0x3d reg = 0x76 value = 0x0 [MCU2_0] 182.297763 s: BPD: address = 0x3d reg = 0x90 value = 0x0 [MCU2_0] 182.297958 s: BPD: address = 0x3d reg = 0x91 value = 0x0 182.553842 s: ISS: ERROR: Initializing sensor [GW_AR0233_UYVY] failed !!! 182.553889 s: ISS: Initializing sensor [GW_AR0233_UYVY] ... Done !!! Error initializing sensor GW_AR0233_UYVY [MCU2_0] 182.553635 s: Error : sensor probe failed for channel 0 Scaler is disabled 182.564785 s: ISS: Starting sensor [GW_AR0233_UYVY] ... !!! [MCU2_0] 182.836693 s: BPD: address = 0x3d reg = 0x35 value = 0x0 [MCU2_0] 182.836922 s: BPD: address = 0x3d reg = 0x73 value = 0x0 [MCU2_0] 182.837126 s: BPD: address = 0x3d reg = 0x74 value = 0x0 [MCU2_0] 182.837319 s: BPD: address = 0x3d reg = 0x75 value = 0x0 [MCU2_0] 182.837555 s: BPD: address = 0x3d reg = 0x76 value = 0x0 [MCU2_0] 182.837759 s: BPD: address = 0x3d reg = 0x90 value = 0x0 [MCU2_0] 182.837958 s: BPD: address = 0x3d reg = 0x91 value = 0x0 [MCU2_0] 183.110689 s: BPD: address = 0x3d reg = 0x35 value = 0x1 [MCU2_0] 183.110908 s: BPD: address = 0x3d reg = 0x73 value = 0x0 183.112172 s: ISS: Starting sensor [GW_AR0233_UYVY] ... !!! get_dcc_dir_size : Could not open directory or directory is empty /opt/vision_apps/dcc/GW_AR0233_UYVY/wdr [MCU2_0] 183.111109 s: BPD: address = 0x3d reg = 0x74 value = 0x0 [MCU2_0] 183.111306 s: BPD: address = 0x3d reg = 0x75 value = 0x0 [MCU2_0] 183.111554 s: BPD: address = 0x3d reg = 0x76 value = 0x0 [MCU2_0] 183.111760 s: BPD: address = 0x3d reg = 0x90 value = 0x0 [MCU2_0] 183.111956 s: BPD: address = 0x3d reg = 0x91 value = 0x0 [MCU2_0] 183.112776 s: VX_ZONE_WARNING:[tivxCaptureSetTimeout:774] CAPTURE: WARNING: Error frame not provided using tivxCaptureRegisterErrorFrame, defaulting to waiting forever !!! Unsupported command ========================== Demo : Single Camera w/ 2A ========================== p: Print performance statistics s: Save Sensor RAW, VISS Output and H3A output images to File System e: Export performance statistics u: Update DCC from File System x: Exit Enter Choice: