Hello,
I have a problem with a J7 CP board J721EXCPXEVM, suddenly the SoM power is down and when I tried the SoM on another CP board, it worked.
So it seems that the DC-DC conversion circuit on the CP board is off for some reason as it appears in the following photo:
The 12V LED is ON when I flip the power switch, but other LEDs are OFF. (I tried a different brand new board and at least LD7 was ON)
Any idea what might be the problem?
Thanks in advance.