This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Would you tell me in which position voice codec HW module dirver source code of dm365 is in the psp3.01, and any explanation or use doc(for example:audio user guide etc )regarding this driver source code.

Dear all,

                          I'm using  dvsdk4.02(include psp3.01)  for a product development , this product need to be used voice codec HW module of dm365 for talking applicaton(not use McBSP HW interface of dm365),but i do not find voice codec HW module driver source code form psp3.1 linux kernal,would you tell me in which position this HW dirver source is  in the psp3.01, any explanation or use doc(for example:audio user guide etc ) regarding this driver source code as well ?

                        I  have get  a doc named SPRUG98 LSP 2.10 DaVinci Linux Audio Driver User's Guide  form ti carlisle ,but i find this doc be explained for  McBSP HW interface of dm365 and OSS standard,not for voice codec HW module of dm365 and ALSA standard .

                        Best regard