Part Number: TDA4VM
Hi TI,
I configure wkup_gpio0_7 as the wakeup source from “mem” power state, but it always fail, could you please help? I'm using SDK8.0, thanks
dts:
gpio_keys: gpio-keys {
compatible = "gpio-keys";
autorepeat;
pinctrl-names = "default";
pinctrl-0 = <&sw11_button_pins_default>;
sw11: sw11 {
label = "GPIO Key USER2";
linux,code = <KEY_WAKEUP>;
gpios = <&wkup_gpio0 7 GPIO_ACTIVE_LOW>;
interrupt-parent = <&wkup_gpio0>;
interrupts = <7 IRQ_TYPE_EDGE_BOTH>;
debounce-interval = <10>;
wakeup-source;
};
};
&wkup_pmx0 {
sw11_button_pins_default: sw11-button-pins-default {
pinctrl-single,pins = <
J721E_WKUP_IOPAD(0xcc, PIN_INPUT, 7) /* (G28) WKUP_GPIO0_7 */
>;
};
};
fail log:
root@j7-evm:~# echo mem > /sys/power/state [ 74.238387] PM: suspend entry (s2idle) [ 74.245362] Filesystems sync: 0.003 seconds [ 74.253256] Freezing user space processes ... (elapsed 0.000 seconds) done. [ 74.261184] OOM killer disabled. [ 74.264407] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 74.273073] printk: Suspending console(s) (use no_console_suspend to debug) [ 74.301035] gpio-keys gpio-keys: failed to configure IRQ 216 as wakeup source: -6 [ 74.301055] PM: dpm_run_callback(): platform_pm_suspend+0x0/0x78 returns -6 [ 74.301060] PM: Device gpio-keys failed to suspend: error -6 [ 74.301064] PM: Some devices failed to suspend, or early wake event detected [ 74.329772] OOM killer enabled. [ 74.332907] Restarting tasks ... done. [ 74.339576] PM: suspend exit